Power Save Deep Sleep#
1. Purpose / Scope#
This application demonstrates how to enable power save deep sleep profile with RS9116W EVK. This application enables power save profile mode 8 and then wait in a scheduler for some time. Once it will come out of delay, it will connect to the configured AP and open udp client socket. It sends some packets to the udp server, disconnects from AP and goes back to deep sleep.
2. Prerequisites / Setup Requirements#
Before running the application, the user will need the following things to setup.
2.1 Hardware Requirements#
Windows PC with Host interface (UART / SPI/ SDIO).
Silicon Labs RS9116 Wi-Fi Evaluation Kit
Host MCU Eval Kit. This example has been tested with:
Silicon Labs WSTK + EFR32MG21
Silicon Labs WSTK + EFM32GG11
Wireless Access point
Windows PC2 (Remote PC) with UDP server application (Iperf Application)
2 wire connectors for GPIO pins
Agilent power analyzer


2.2 Software Requirements#
Embedded Development Environment
For STM32, use licensed Keil IDE
For Silicon Labs EFx32, use the latest version of Simplicity Studio
Iperf Application in the remote PC.
3. Application Build Environment#
3.1 Platform#
The Application can be built and executed on below Host platforms
3.2 Host Interface#
By default, the application is configured to use the SPI bus for interfacing between Host platforms(STM32F411 Nucleo / EFR32MG21) and the RS9116W EVK.
This application is also configured to use the SDIO bus for interfacing between Host platforms(EFM32GG11) and the RS9116W EVK.
3.3 Project Configuration#
The Application is provided with the project folder containing Keil and Simplicity Studio project files.
Keil Project
The Keil project is used to evaluate the application on STM32.
Project path:
<SDK>/examples/snippets/wlan/power_save_deep_sleep/projects/power_save_deep_sleep-nucleo-f411re.uvprojx
Simplicity Studio
The Simplicity Studio project is used to evaluate the application on EFR32MG21.
Project path:
If the Radio Board is BRD4180A or BRD4181A, then access the path
<SDK>/examples/snippets/wlan/power_save_deep_sleep/projects/power_save_deep_sleep-brd4180a-mg21.slsprojIf the Radio Board is BRD4180B or BRD4181B, then access the path
<SDK>/examples/snippets/wlan/power_save_deep_sleep/projects/power_save_deep_sleep-brd4180b-mg21.slsprojUser can find the Radio Board version as given below


EFM32GG11 platform
The Simplicity Studio project is used to evaluate the application on EFM32GG11.
Project path:
<SDK>/examples/snippets/wlan/power_save_deep_sleep/projects/power_save_deep_sleep-brd2204a-gg11.slsproj
3.4 Bare Metal/RTOS Support#
This application supports bare metal and RTOS environment. By default, the application project files (Keil and Simplicity studio) are provided with bare metal configuration in the SDK.
4. Application Configuration Parameters#
The application can be configured to suit user requirements and development environment. Read through the following sections and make any changes needed.
4.1 Open rsi_wlan_power_save_profile.c file#
4.1.1 User must update the below parameters#
SSID refers to the name of the Access point.
#define SSID "SILABS_AP" SECURITY_TYPE refers to the type of security. In this application STA supports Open, WPA-PSK, WPA2-PSK securities.
Valid configuration is:
RSI_OPEN - For OPEN security mode
RSI_WPA - For WPA security mode
RSI_WPA2 - For WPA2 security mode
#define SECURITY_TYPE RSI_WPA2PSK refers to the secret key if the Access point configured in WPA-PSK/WPA2-PSK security modes.
#define PSK "1234567890" SERVER_PORT port refers remote UDP server port number which is opened in Windows PC2.
#define SERVER_PORT 5001SERVER_IP_ADDRESS refers remote peer IP address to connect with TCP server socket. IP address should be in long format and in little endian byte order.
Example: To configure “192.168.10.100” as IP address, update the macro DEVICE_IP as 0x640AA8C0.
#define SERVER_IP_ADDRESS 0x640AA8C0NUMBER_OF_PACKETS refers how many packets to send from device to remote UDP server.
#define NUMBER_OF_PACKETS <no of packets>4.1.2 The desired parameter are provided below. User can also modify the parameters as per their needs and requirements#
The following parameters are configured if OS is used. WLAN task should be of low priority
#define RSI_WLAN_TASK_PRIORITY 1Driver task should have the highest priority among all threads
#define RSI_DRIVER_TASK_PRIORITY 2WLAN Task stack size is configured by this macro
#define RSI_WLAN_TASK_STACK_SIZE 500Driver Task stack size is configured by this macro
#define RSI_DRIVER_TASK_STACK_SIZE 500Application memory length which is required by the driver.
#define GLOBAL_BUFF_LEN 15000To configure IP address DHCP_MODE refers whether IP address configured through DHCP or STATIC
#define DHCP_MODE 1 Note: If user wants to configure STA IP address through DHCP then set DHCP_MODE to "1" and skip configuring the following DEVICE_IP, GATEWAY and NETMASK macros. (Or) If user wants to configure STA IP address through STATIC then set DHCP_MODE macro to “0” and configure following DEVICE_IP, GATEWAY and NETMASK macros.
IP address to be configured to the device in STA mode should be in long format and in little endian byte order.
Example: To configure “192.168.10.10” as IP address, update the macro DEVICE_IP as 0x0A0AA8C0.
#define DEVICE_IP 0X0A0AA8C0IP address of the gateway should also be in long format and in little endian byte order
Example: To configure “192.168.10.1” as Gateway, update the macro GATEWAY as 0x010AA8C0
#define GATEWAY 0x010AA8C0IP address of the network mask should also be in long format and in little endian byte order.
Example: To configure “255.255.255.0” as network mask, update the macro NETMASK as 0x00FFFFFF
#define NETMASK 0x00FFFFFFIn this application, default power save mode configuration is set to low power mode 8 (RSI_SLEEP_MODE_8) with maximum power save (RSI_MAX_PSP) with message based hand shake.
#define PSP_MODE RSI_SLEEP_MODE_8
#define PSP_TYPE RSI_MAX_PSP 4.1.3 If the user wants different power save modes, update/modify the below macros#
PSP_MODE refers to the power save profile mode. RS9116W EVK supports the following power modes:
RSI_ACTIVE (0) : In this mode, module is active and power save is disabled.
RSI_SLEEP_MODE_1 (1): In this power mode, module goes to power save after association with the Access Point. In this sleep mode, SoC will never turn off, therefore no handshake is required before sending data to the module.
RSI_SLEEP_MODE_2 (2): In this power mode, module goes to power save after association with the Access Point. In this sleep mode, SoC will go to sleep based on GPIO hand shake or Message exchange, therefore handshake is required before sending data to the module.
RSI_SLEEP_MODE_8 (8): In this power mode, module goes to power save when it is in unassociated state with the Access Point. In this sleep mode, SoC will go to sleep based on GPIO hand shake or Message exchange, therefore handshake is required before sending the command to the module.
#define PSP_MODE RSI_SLEEP_MODE_8WiSeConnect device supports following power save modes:
RSI_CONNECTED_GPIO_BASED_PS = 2
RSI_CONNECTED_MSG_BASED_PS = 3
RSI_GPIO_BASED_DEEP_SLEEP = 8
RSI_MSG_BASED_DEEP_SLEEP = 9
Among the above mentioned four power save modes, which power save mode must be selected will depend upon the two macros i.e., PSP_MODE and RSI_HAND_SHAKE_TYPE selection.
RSI_HAND_SHAKE_TYPE | PSP_MODE | |
|---|---|---|
RSI_SLEEP_MODE_2 (Connected_SLEEP) | RSI_SLEEP_MODE_8 (Deep_SLEEP) | |
GPIO_BASED | RSI_CONNECTED_GPIO_BASED_PS = 2 | RSI_GPIO_BASED_DEEP_SLEEP = 8 |
MSG_BASED | RSI_CONNECTED_MSG_BASED_PS = 3 | RSI_MSG_BASED_DEEP_SLEEP = 9 |
Note: For RSI_SLEEP_MODE_2 and RSI_SLEEP_MODE_8 modes, GPIO or Message based hand shake can be selected using RSI_HAND_SHAKE_TYPE macro which is define in rsi_wlan_config.h In this example user can verify RSI_SLEEP_MODE_2 with Message based hand shake. If user wants to verify other power modes, user has to change the application as well as GPIO hand shake signals.
PSP_TYPE refers power save profile type. WiSeConnect device supports following power save profile types :
RSI_MAX_PSP (0) : In this mode, WiSeConnect device will be in Maximum power save mode. i.e Device will wake up for every DTIM beacon and do data Tx and Rx.
RSI_FAST_PSP (1): In this mode, WiSeConnect device will disable power save for any Tx/Rx packet for monitor interval of time (monitor interval can be set through macro in release/examples/snippets/wlan/power_save_deep_sleep/rsi_wlan_config.h file, default value is 50 ms).If there is no data for monitor interval of time then module will again enable power save.
RSI_UAPSD (2) : This PSP_TYPE is used to enable WMM power save.
#define PSP_TYPE RSI_MAX_PSPNote: PSP_TYPE is valid only when PSP_MODE set to RSI_SLEEP_MODE_1 or RSI_SLEEP_MODE_2 mode. RSI_UAPSD power profile type in PSP_TYPE is valid only when RSI_WMM_PS_ENABLE is enabled in rsi_wlan_config.h file.
4.2 Open rsi_wlan_config.h file#
4.2.1 The desired parameters are provided below. User can also modify the parameters as per their needs and requirements#
#define CONCURRENT_MODE RSI_DISABLE
#define RSI_FEATURE_BIT_MAP (FEAT_SECURITY_OPEN | FEAT_ULP_GPIO_BASED_HANDSHAKE)
#define RSI_TCP_IP_BYPASS RSI_DISABLE
#define RSI_TCP_IP_FEATURE_BIT_MAP TCP_IP_FEAT_DHCPV4_CLIENT
#define RSI_CUSTOM_FEATURE_BIT_MAP FEAT_CUSTOM_FEAT_EXTENTION_VALID
#define RSI_EXT_CUSTOM_FEATURE_BIT_MAP (EXT_FEAT_LOW_POWER_MODE | EXT_FEAT_XTAL_CLK_ENABLE)
#define RSI_BAND RSI_BAND_2P4GHZDefault configuration of low power save mode 2
#define RSI_HAND_SHAKE_TYPE GPIO_BASED
#define RSI_SELECT_LP_OR_ULP_MODE RSI_LP_MODE
#define RSI_DTIM_ALIGNED_TYPE 0
#define RSI_MONITOR_INTERVAL 50
#define RSI_WMM_PS_ENABLE RSI_DISABLE
#define RSI_WMM_PS_TYPE 0
#define RSI_WMM_PS_WAKE_INTERVAL 20
#define RSI_WMM_PS_UAPSD_BITMAP 154.2.2 The application is provided with RSI_SLEEP_MODE_8 configurtion. If the user wants to modify different power save modes, update/modify the below macros#
RSI_HAND_SHAKE_TYPE is used to select GPIO or Message based hand shake in RSI_SLEEP_MODE_2 and RSI_SLEEP_MODE_8 modes.
#define RSI_HAND_SHAKE_TYPE GPIO_BASED RSI_SELECT_LP_OR_ULP_MODE is used to select low power mode or ultra low power mode.
Valid configurations are:
RSI_LP_MODE : In this module will be in Low power mode.
RSI_ULP_WITH_RAM_RET : In this module will be in Ultra low power mode and it will remember the previous state after issuing power save mode command.
RSI_ULP_WITHOUT_RAM_RET : In this module will be in Ultra low power mode and it will not remember the previous state after issuing power save mode command. In order to wake the module up, the user needs to call wake up API (rsi_req_wakeup). Once the module wakes up, it gives CARD READY indication to the host and the user has to issue commands from wireless Initialization API (rsi_wireless_init).
#define RSI_SELECT_LP_OR_ULP_MODE RSI_LP_MODE RSI_DTIM_ALIGNED_TYPE refers whether module has to wake up at normal beacon or DTIM beacon which is just before listen interval.
If RSI_DTIM_ALIGNED_TYPE is set to 0 i.e module will wake up at normal beacon which is just before listen interval
If RSI_DTIM_ALIGNED_TYPE is set to 1 i.e module will wake up at DTIM beacon which is just before listen interval
#define RSI_DTIM_ALIGNED_TYPE 0 RSI_MONITOR_INTERVAL refers amount of time (in ms) to wait for Tx or Rx before giving power save indication to connected Access Point.
#define RSI_MONITOR_INTERVAL 50Note: RSI_MONITOR_INTERVAL is applicable only when PSP_TYPE selected as RSI_FAST_PSP
RSI_WMM_PS_ENABLE is used to enable or disable WMM power save.
#define RSI_WMM_PS_ENABLE 0 RSI_WMM_PS_TYPE is used to set Tx based or Periodic based WMM power save.Update RSI_WMM_PS_TYPE macro with 0 for Tx Based or 1 for periodic based WMM power save.
#define RSI_WMM_PS_TYPE 0 RSI_WMM_PS_WAKE_INTERVAL refers at periodic time (in ms) module has to wake up module when RSI_WMM_PS_TYPE selected as Periodic.
#define RSI_WMM_PS_WAKE_INTERVAL 20RSI_WMM_PS_UAPSD_BITMAP refers UAPSD bitmap
#define RSI_WMM_PS_UAPSD_BITMAP 15 Note: If RSI_WMM_PS_ENABLE is enabled then user has to set PSP_TYPE to RSI_UAPSD in order to work with WMM power save mode.
5. Testing the Application#
User has to follow the below steps for the successful execution of the application.
5.1 Loading the RS9116W Firmware#
Refer Getting started with a PC to load the firmware into RS9116W EVK. The firmware file is located in <SDK>/firmware/
5.2 Building the Application on the Host Platform#
5.2.1 Using STM32#
Refer Getting started with STM32
Configure STM32 CN10 header pin-4 should connect to UULP_GPIO_0 and CN10 header pin-2 should connect to UULP_GPIO_2.
Open the project
<SDK>/examples/snippets/wlan/power_save_deep_sleep/projects/power_save_deep_sleep-nucleo-f411re.uvprojxBuild and Debug the project
Check for the RESET pin:
If RESET pin is connected from STM32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before Free run.
If RESET pin is not connected from STM32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before free run.
Free run the project.
Then continue the common steps from 5.3
5.2.2 Using EFX32#
Refer Getting started with EFX32, for settin-up EFR & EFM host platforms
Configure EFX32 J4 pin-9 should connect to UULP_GPIO_0 and EVFX32 J4 pin-7 should connect to UULP_GPIO_2.
Open Simplicity Studio and import the EFR32/EFM32 project from
<SDK>/examples/snippets/wlan/power_save_deep_sleep/projectsSelect the appropriate .slsproj as per Radio Board type mentioned in Section 3.3 for EFR32 board. (or)
Select the *.brd2204a-gg11.slsproj for EFM32GG11 board.
Compile and flash the project in to Host MCU.
Debug the project.
Check for the RESET pin:
If RESET pin is connected from EFX32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before Free run.
If RESET pin is not connected from EFX32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before the Free run.
Free run the project.
Then continue the common steps from 5.3
5.3 Common Steps#
Configure the Access point in OPEN / WPA-PSK / WPA2-PSK mode to connect RS9116W EVK in STA mode.
Open UDP server application using iperf application in Windows PC2 (Remote PC) which is connected to access point.
iperf_demo.exe –s -u -p <SERVER_PORT> -i 1


After program gets executed, RS9116W EVK will go to sleep based on the selected power mode and wakes up after deep sleep timeout (Default deep sleep time is 3sec in RSI_SLEEP_MODE_8 with message based hand shake). Refer the given below image for power save cycle for default deep sleep time.


After successful wake up from deep sleep, RS9116W EVK connects to AP and sends configured number of (NUMBER_OF_PACKETS) UDP packets to remote peer which is connected to Access point. Refer the given below image for reception of UDP data on UDP server.


After sending configured number of packets, RS9116W EVK disconnects from connected AP and again repeat the above steps (It will again go to sleep and wakes up after time out, connects to AP and sends configured number of packets). Find below image for power save profile cycle.


Compressed Debug Logging#
To enable the compressed debug logging feature please refer to Logging User Guide