Public Attributes#

rsi_mutex_handle_t
rsi_mutex_handle_t
rsi_mutex_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
rsi_semaphore_handle_t
int32_t
uint32_t

timer flag

rsi_device_state_t

Public Attribute Documentation#

rom_version_info#

uint32_t rom_version_info

Definition at line 877 of file include/rsi_common.h

tx_mask_event#

uint32_t tx_mask_event

Definition at line 878 of file include/rsi_common.h

tx_mutex#

rsi_mutex_handle_t tx_mutex

Definition at line 879 of file include/rsi_common.h

logging_mutex#

rsi_mutex_handle_t logging_mutex

Definition at line 881 of file include/rsi_common.h

debug_prints_mutex#

rsi_mutex_handle_t debug_prints_mutex

Definition at line 884 of file include/rsi_common.h

nwk_sem#

rsi_semaphore_handle_t nwk_sem

Definition at line 886 of file include/rsi_common.h

wlan_cmd_sem#

rsi_semaphore_handle_t wlan_cmd_sem

Definition at line 887 of file include/rsi_common.h

common_cmd_sem#

rsi_semaphore_handle_t common_cmd_sem

Definition at line 888 of file include/rsi_common.h

common_cmd_send_sem#

rsi_semaphore_handle_t common_cmd_send_sem

Definition at line 889 of file include/rsi_common.h

wlan_cmd_send_sem#

rsi_semaphore_handle_t wlan_cmd_send_sem

Definition at line 890 of file include/rsi_common.h

nwk_cmd_send_sem#

rsi_semaphore_handle_t nwk_cmd_send_sem

Definition at line 891 of file include/rsi_common.h

send_data_sem#

rsi_semaphore_handle_t send_data_sem

Definition at line 892 of file include/rsi_common.h

nwk_wait_bitmap#

uint8_t nwk_wait_bitmap

Definition at line 893 of file include/rsi_common.h

wlan_wait_bitmap#

uint8_t wlan_wait_bitmap

Definition at line 894 of file include/rsi_common.h

send_wait_bitmap#

uint8_t send_wait_bitmap

Definition at line 895 of file include/rsi_common.h

common_wait_bitmap#

uint8_t common_wait_bitmap

Definition at line 896 of file include/rsi_common.h

zigb_wait_bitmap#

uint8_t zigb_wait_bitmap

Definition at line 897 of file include/rsi_common.h

bt_wait_bitmap#

uint8_t bt_wait_bitmap

Definition at line 898 of file include/rsi_common.h

bt_cmd_wait_bitmap#

uint8_t bt_cmd_wait_bitmap

Definition at line 899 of file include/rsi_common.h

nwk_cmd_state#

volatile uint8_t nwk_cmd_state

Definition at line 900 of file include/rsi_common.h

nwk_status#

volatile int32_t nwk_status

Definition at line 901 of file include/rsi_common.h

socket_state#

volatile uint8_t socket_state

Definition at line 902 of file include/rsi_common.h

socket_status#

volatile int32_t socket_status

Definition at line 903 of file include/rsi_common.h

wlan_cmd_state#

volatile uint8_t wlan_cmd_state

Definition at line 904 of file include/rsi_common.h

common_cmd_state#

volatile uint8_t common_cmd_state

Definition at line 905 of file include/rsi_common.h

timer_counter#

volatile uint32_t timer_counter

Definition at line 906 of file include/rsi_common.h

driver_timer_start#

volatile uint32_t driver_timer_start

Definition at line 908 of file include/rsi_common.h

timer_start#

rsi_timer_instance_t timer_start

Definition at line 909 of file include/rsi_common.h

driver_rx_timer_start#

volatile uint32_t driver_rx_timer_start

Definition at line 912 of file include/rsi_common.h

rx_timer_start#

rsi_timer_instance_t rx_timer_start

Definition at line 913 of file include/rsi_common.h

rsi_spiTimer1#

uint32_t rsi_spiTimer1

Definition at line 917 of file include/rsi_common.h

rsi_spiTimer2#

uint32_t rsi_spiTimer2

Definition at line 918 of file include/rsi_common.h

rsi_spiTimer3#

uint32_t rsi_spiTimer3

Definition at line 919 of file include/rsi_common.h

rsi_spiTimer4#

uint32_t rsi_spiTimer4

Definition at line 920 of file include/rsi_common.h

rsi_sdioTimer#

uint32_t rsi_sdioTimer

Definition at line 923 of file include/rsi_common.h

sdio_read_buff#

uint8_t sdio_read_buff[SDIO_BUFFER_LENGTH]

Definition at line 926 of file include/rsi_common.h

non_pref_chan_read_buff#

char non_pref_chan_read_buff[RSI_SINGLE_NON_PREF_CHAN_PARAMS_LEN *RSI_MAX_POSSIBLE_SINGLE_BAND_CHANNEL]

Definition at line 929 of file include/rsi_common.h

rx_driver_flag#

uint32_t rx_driver_flag

timer flag


Definition at line 932 of file include/rsi_common.h

device_state#

volatile rsi_device_state_t device_state

Definition at line 933 of file include/rsi_common.h

rsi_wait_timeout_handler_error_cb#

void(* rsi_wait_timeout_handler_error_cb) (int32_t status, uint32_t cmd_type)

Definition at line 936 of file include/rsi_common.h

nwk_app_buffer#

uint8_t* nwk_app_buffer

Definition at line 939 of file include/rsi_common.h

nwk_app_buffer_length#

uint32_t nwk_app_buffer_length

Definition at line 942 of file include/rsi_common.h

module_type_valid#

uint8_t module_type_valid

Definition at line 943 of file include/rsi_common.h

module_type_id#

uint8_t module_type_id

Definition at line 944 of file include/rsi_common.h