Public Attributes#

uint8_t
uint8_t
struct rsi_m4ta_desc_s *
struct rsi_m4ta_desc_s *
struct rsi_m4ta_desc_s *

Public Attribute Documentation#

rom_apis_p#

rom_apis_t* rom_apis_p

no_of_sockets#

uint8_t no_of_sockets

endian#

uint8_t endian

rx_buffer_mem_copy#

uint8_t rx_buffer_mem_copy

rsi_tcp_listen_min_backlog#

uint8_t rsi_tcp_listen_min_backlog

os_enabled#

uint8_t os_enabled

rsi_max_num_events#

uint8_t rsi_max_num_events

tx_desc#

struct rsi_m4ta_desc_s* tx_desc

rx_desc#

struct rsi_m4ta_desc_s* rx_desc

crypto_desc#

struct rsi_m4ta_desc_s* crypto_desc

submit_rx_pkt_to_ta#

volatile uint8_t submit_rx_pkt_to_ta