Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

dev_addr_type#

uint8_t dev_addr_type

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

le_scan_interval#

uint16_t le_scan_interval

le_scan_window#

uint16_t le_scan_window

conn_interval_min#

uint16_t conn_interval_min

conn_interval_max#

uint16_t conn_interval_max

conn_latency#

uint16_t conn_latency

supervision_tout#

uint16_t supervision_tout