Public Attributes#

uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

remote device address


max_tx_latency#

uint16_t max_tx_latency

Maximum latency for data being transmitted from the local device to the remote device


min_remote_timeout#

uint16_t min_remote_timeout

Base sniff subrate timeout in baseband slots that the remote device use


min_local_timeout#

uint16_t min_local_timeout

Base sniff subrate timeout in baseband slots that the local device use