You are viewing documentation for version:2.9.2Public Attributes#uint16_tcrc_fail_cntuint16_tcrc_pass_cntuint16_ttx_abort_cntuint16_trx_drop_cntuint16_trx_cca_idle_cntuint16_trx_start_idle_cntuint16_trx_abrt_cntuint16_ttx_donesint8_trssiuint16_tid_pkts_rcvduint16_tdummyPublic Attribute Documentation#crc_fail_cnt#uint16_t crc_fail_cntPacket count of CRC fails (Cyclic Redundancy Check (CRC)) crc_pass_cnt#uint16_t crc_pass_cntPacket count of CRC fails (Cyclic Redundancy Check (CRC)) tx_abort_cnt#uint16_t tx_abort_cntPacket count of aborted Tx rx_drop_cnt#uint16_t rx_drop_cntPacket count of dropped Rx rx_cca_idle_cnt#uint16_t rx_cca_idle_cntPacket count of CCA Idle (Clear Channel Assessment (CCA)) rx_start_idle_cnt#uint16_t rx_start_idle_cntPacket count of Rx start rx_abrt_cnt#uint16_t rx_abrt_cntPacket count of aborted Rx tx_dones#uint16_t tx_donesPacket count of successful transmissions rssi#int8_t rssiReceived Signal Strength Indicator of the packet id_pkts_rcvd#uint16_t id_pkts_rcvdPacket count of ID packets received dummy#uint16_t dummy[5]Dummy array of length 5