RS9116 n-Link™ OSD Release Notes
Release notes are provided with each version of RS9116 n-Link OSD drivers .
Versions
Reference Documents
n-Link OSD 2.5.1 Release Notes
Last updated: March 25, 2022
Index
- Highlights
- Release Details
- New Features
- Changes and Issues Fixed
- Known Issues
- Limitations and Unsupported Features
- Terminology
Highlights
- Added support to update gain tables to help with regulatory certification
- Added fast PSP support in power save profile
- Fixed transmit power issue in AA0/CC0 Modules
- Added fixes for Wi-Fi FragAttack vulnerability
Release Details
| Item | Details |
|---|---|
| Release date | 25th March, 2022 |
| Firmware Version | 1610.2.5.1.0.11 |
| Package Name | RS9116.NB0.NL.GNU.LNX.OSD.2.5.1.11 |
| Hardware Modules | QMS, B00, C00, CC1, AB0, AB1, AA0, AA1 |
| Hardware Chipsets | Chip Revision 1.3, 1.4, 1.5 |
| Linux Kernel Version support | From v3.18 to v5.15 |
| Host interfaces supported | USB, SDIO |
New Features
Wi-Fi
- Provision to update Gain Table for certification
- Fast PSP support in power save profile
Bluetooth - Common
- None
Bluetooth – Classic
- None
Bluetooth – LE
- None
Changes and Fixes
Wi-Fi
- Fixed transmit power issue in AA0/CC0 Modules.
- Added minimum supported rate for EAPOL packet transmission.
- Added a fix for SDIO suspend/resume.
- Added fixes for Wi-Fi FragAttack vulnerability.
- RS9116X-DB00-CCX-BXX certified TELEC gain tables included.
Bluetooth – Common
- Added a fix to initiate AFH periodically to resolve a BT and Wi-Fi hang issue.
- Resolved a Wi-Fi ICMP ping issue that used to occur while connecting to BT in co-ex mode in CC0/AA0 modules based on chip version 1.3.
Bluetooth – Classic
- None
Bluetooth – LE
- None
Known Issues
- BT-HID might not inter-operate with Apple devices.
- In Wi-Fi + BT/BLE co-ex mode, high Wi-Fi broadcast traffic, might cause BT/BLE disconnections.
- Set rate can not be used for setting non MCS and non basic rates in kernels above 4.13.16.
- Enterprise security with WPA3 is not supported.
- Tx Rate information is not being updated in WLAN interfaces stats reported by iwconfig tool.
- Auto Channel Selection in AP with WORLD region will not work.
Limitations and Unsupported Features
Wi-Fi
- Tx AMSDU is not supported.
- Fragmentation is not supported.
- AMSDU's within an AMPDU is not supported.
- Wi-Fi performance may be reduced in dense environments.
- 802.11j is not supported.
- In AP mode, more than 16 clients are not supported; AP + BT + BLE mode supports 4 clients.
- USB ULP is not supported.
- External 3-wire co-existence is not supported.
- LP powersave using GPIO handshake is not supported.
- DFS Master is not supported.
- Radar detection in STA mode is not supported.
BT/BLE
-
In BLE, the recommended range for the Connection Interval in
- Power Save: 100 ms to 1.28 seconds.
- BT Classic + BLE Dual Mode: >= 200 ms.
- Wi-Fi + BLE co-ex: 30 ms to 4 seconds
- In BLE, during connection, using the same value for Scan Interval and Scan Window is not recommended.
- In BT Classic, the recommended value of Sniff Interval during Power Save is limited to 100 ms (<= 100).
- In Wi-Fi + BT Classic co-ex, for normal BT file transfer operation, the recommended value of Wi-Fi protocol DTIM is > 3, and that of Beacon Interval is > 200ms.
- In Wi-Fi + BLE, during Wi-Fi connection, using a lower BLE Scan Window and larger BLE Scan Interval is recommended.
- In CC0/CC1 dual-band modules, power consumption during transmission in 2.4 GHz is sometimes higher by up to 30% to 40%
- Power consumption in BLE connected sleep is higher by ~40%
- BT Sniff mode does not work if BT multiple slaves feature is enabled.
- When BT multiple slaves feature is enabled, Master to Slave role switch will not happen.
- In BLE, if Advertising/Scanning is in progress, and the device switches its Slave/Master role, Advertising/Scanning will stop. The command to start Advertising/Scanning must be given again.
- Glitches can be observed in BT audio if Wi-Fi is in connected state.
-
In BLE, if device is acting as Master/Slave, Scan Window (in
set_scan_paramsandcreate_connection command) shall be less than the existing Connection Interval. - In BLE, if BLE Connection is established with small Connection Interval (< 15 ms), simultaneous roles (i.e. Master/Slave + Advertising/Scanning) are not supported.
- BT Classic Simultaneous Slave & Master roles (Scatter-net) is not supported.
Co-existence
- In Wi-Fi + BLE, if the BLE Scan Interval and Scan Window are identical, Wi-Fi connection may be unsuccessful.
- BLE disconnection may be observed with Wi-Fi + BLE configuration with Wi-Fi continuous data transfer for low BLE supervision timeout configured. If the Supervision timeout is configured to >= 16 seconds, no disconnections are observed
- If BT/BLE is connected first with small connection interval, it may be difficult to achieve a Wi-Fi connection. It is recommended to use a longer connection interval and supervision timeout for BLE or a longer supervision timeout and sniff interval for BT.
n-Link OSD 2.3.2 Release Notes
Last updated: July 5, 2021
Index
- Highlights
- Release Details
- New Features
- Changes and Issues Fixed
- Known Issues
- Limitations and Unsupported Features
- Terminology
Highlights
- Added Wi-Fi support for EN 300 328 V2.2.2
-
Fixed STA disconnection issue in co-ex mode while giving
lescancommand
Release Details
| Item | Details |
|---|---|
| Release date | July 5, 2021 |
| Firmware Version | 1610.2.3.2.0003 |
| Package Name | RS9116.NB0.NL.GNU.LNX.OSD.2.3.2.0003 |
| Hardware Modules | QMS, B00, C00, CC1, AB0, AB1, AA0, AA1 |
| Hardware Chipsets | Chip Revision 1.4 |
| Supported Linux Kernel Versions | From v3.18 to v5.7 |
| Host interfaces supported | USB, SDIO |
New Features
Wi-Fi
- Added Support for EN 300 328 V2.2.2.
Bluetooth - Common
- None
Bluetooth – Classic
- None
Bluetooth – LE
- None
Changes/Issues Fixed
Wi-Fi
- None
Bluetooth – Common
-
Fixed STA disconnection issue in co-ex mode while giving
lescancommand.
Bluetooth – Classic
- None
Bluetooth – LE
- None
Known Issues
- BT-HID may not inter-operate with Apple devices
- In Wi-Fi + BT/BLE co-ex mode, high Wi-Fi broadcast traffic may cause BT/BLE disconnections.
- Issues with BT PER continuous mode transmission
- Set rate can not be used for setting non-MCS and non-basic rates in kernels above 4.13.16.
- Enterprise security with WPA3 is not supported.
- Transmit rate update to use (iwconfig) is not supported.
- BT/BLE co-ex modes with WiFi AP are not supported.
- EAP-TLS 1.2 /1.1 are not supported in this release.
- Auto Channel Selection in AP with WORLD region will not work.
Limitations and Unsupported Features
Wi-Fi
- AMSDU TX is not supported
- Fragmentation is not supported.
- AMSDU's within AMPDU is not supported.
- Wi-Fi performance is reduced in dense environments.
- Digital Loopback is not supported.
- PUF is not supported.
- 11j not supported.
- 11p is not supported.
- AP mode more than 16 clients not supported, AP + BT + BLE has 4 clients support.
- CW mode is not supported.
- RF Loopback modes M2, M3 are not supported.
- CCX & 11k not supported.
- USB ULP is not supported.
- iAP Apple Wi-Fi Home kit is not supported.
- PUF IID is not supported.
- WAPI is not supported.
- WDS is not supported.
- WMM-Admission Control is not supported.
- External 3-wire co-existence is not supported.
- LP Power save using GPIO handshake is not supported.
- DFS Master in AP is not supported.
- Radar detection in STA mode is not supported.
- Enterprise security in AP mode is not supported.
BT/BLE
-
In BLE, recommended range of Connection Interval in
- Power Save: 100 ms to 1.28 seconds
- BT Classic + BLE Dual Mode: >= 200 ms.
- Wi-Fi + BLE co-ex: 30 ms to 4 seconds
- In BLE, during Connection, same values of Scan Interval and Scan Window is not recommended.
- In BT Classic, recommended value of Sniff Interval during Power Save is limited to 100ms (<= 100).
- In Wi-Fi + BT Classic co-ex, for BT file transfer to work fine, recommended value of Wi-Fi protocol DTIM is more than 3 and Beacon Interval is more than 200 ms.
- In Wi-Fi + BLE, during Wi-Fi connection, we recommend using a lower BLE Scan Window and higher BLE Scan Interval.
- BT Sniff mode does not work if BT multiple slaves feature is enabled.
- When BT multiple slaves feature is enabled, Master to Slave role switch does not work.
- In BLE, if Advertising/Scanning are in progress, and the device moves to Slave/Master role, Advertising/Scanning will be stopped. Provide respective commands to start Advertising/Scanning while in Slave/Master role.
- In Wi-Fi + BLE co-ex, if BLE Connection is established with small Connection Interval (\< 15ms), simultaneous roles (i.e. Master/Slave + Advertising/Scanning) are not supported.
- Observed glitches in BT audio in co-ex mode when Wi-Fi is connected.
- In BLE, if device is acting as Master/Slave, Scan Window (in set_scan_params and create_connection command) shall be less than the existing Connection Interval.
- In BLE, if BLE Connection is established with small Connection Interval (< 15 ms), simultaneous roles (i.e. Master/Slave + Advertising/Scanning) are not supported.
- Simultaneous Slave & Master roles (Scatter-net) is not supported.
Co-existence
- In Wi-Fi + BLE, if the BLE Scan Interval and Scan Window are identical, Wi-Fi connection may be unsuccessful.
- BLE disconnection might be observed with Wi-Fi + BLE configuration with Wi-Fi continuous data transfer for low BLE supervision timeout configured. For Supervision timeout configured with value 16 seconds no disconnections are observed
- In WiFi+BT/BLE configuration if for some reason Wi-Fi disconnects then it is observed that BT/BLE might not reconnect on a disconnection. Can be recovered through Wireless denint followed by Wireless init.
- In Wi-Fi+BT+BLE mode, if Wi-Fi connects first followed by BT/BLE, there is a high probability that all connections will be successfully established
- If BT/BLE gets connected first with small connection interval, then Wi-Fi tries to connect, it will have a poor chance of connecting. In this scenario, a longer BLE connection interval, supervision timeout or BT with higher supervision timeout and sniff interval will have a higher probability of successfully connecting Wi-Fi
Terminology
| Term | Description |
|---|---|
| New Features | These items are new to this release |
| Changes and Fixes | Changes made to existing features found in previous releases of the software. |
| Enhancements to existing product flow and feature set. | |
| Bug fixes done in the Release | |
| Deprecated Items | Features or functions or APIs that are removed from the distributed release to align with the software roadmap |
| Known Issues | Features or functions that do not work as planned at time of release. Workarounds may be offered to meet short term development goals, but longer-term solutions will be added in future software releases |
| Limitations/Recommendations | Describes the limitations on product usage and recommendations for optimal use cases |