You are viewing documentation for version:
2.5
|
Version History
Revision History
1.0
1.2
-
A note to specify the usage of channel bit map.
-
Added procedure to switch from binary to AT and vice-versa.
1.3
-
Added Broadcast API in the chapter WLAN Commands
1.4
-
Added the broadcast API, added the tcp_rx_window_size_cap parameter in the socket_config command, added the note for the TCP/IP stack and added the antenna command in the chapter WLAN Commands.
1.5
-
Added Error code in Error codes section
-
Added HTTP PUT Response structure
-
Added WLAN keep alive configuration support in request_timeout command
-
Added UART debug prints selection and de selection option in exteded custom feature bitmap in opermode command
-
0 – Selecting single socket is enabled changed as 1 -Selecting single socket is enabled
-
-
Modified the UART debug prints information
1.6
-
Added Setregion command and DFS channels in wireless Configuration
-
Changed the PER Continuous flow and Added the preamble duty cycling bit in the feature frame command
-
Added the TCP ACK division factor changes in ext_tcp_ip_feature_bitmap and socket_config command
-
Added Feature frame command request and response type in Binary Command Mode
-
Added changes for "at+rsi_host_rtc_time" command in WLAN Commands
-
Corrected join security possible values information in WLAN Commands
-
Added ext tcp ip feature bit map in WLAN Commands and certificate valid command in Binary Command Mode
-
Added Bit map in ext_tcp_ip_feature_bit_map[7] for DNS_CLIENT_BYPASS
1.7
-
Added information about RAW socket feature
-
Added rsi_config command and possible error codes in the PRM
-
Added note section in band command related to wifi derect and 11j mode
-
Modified rsi_wireless_antenna api.
-
Added few error codes
-
Added comment in ext_custom_feature_bit_map bit 6, 40mhz not supported in 11j AP
-
Edit note section in at+rsi_snmp_get_rsp, to explain counter64 "data reverse send case"
-
Added gain table user configurable command information
-
Added a Note in opermode for custom feature bit map
-
Added precondition for Antenna selection.
-
Safe upgrade in progress is mentioned for IMAGE_STORED_IN_DUMP in Bootloader for similarity with UART messages
-
Added description of BIT(22) in extended custom feature bitmap as crystal clock selection
1.8
-
Added rsI_get_ram_dump command
1.9
-
Added config feature bitmap in opermode
-
Updated soft reset command description for UART/USB-CDC
-
Added no.of sockets supported in MQTT connection
1.10
-
Added ext_tcp_ip_feature_bit_map[16] description in ext_tcp_ip_feature_bit_map.
-
Added BIT(1) SCAN RESULTS TO HOST description in scan_feature_bitmap in scan command
1.11
-
Added MQTT AT commands
-
Added Error type for MQTT Timeout
-
Added next sequence of commands for MQTT user commands
-
Added Response for MQTT_INIT command and a note for possible opermode for MQTT client usage
-
Removed note which says Antenna selection command is not supported
1.12
-
Modified the parameters of "at+rsi_setregion",command,by adding the third parameter-"module type".
-
Removed the commands,which appeared twice in " Response ID's for Rx operation table",in binary command mode document.
-
Removed the twice appeared error codes,in "WLAN error codes,table".
-
Modified the note which says that UART flow control feature is required only for 926100 baud rate.
1.13
-
Added a Note to run the CW mode
1.14
-
Added UART CTS/RTS pin set selection from host in UART flow control command
-
Updated XTAL clk and Power save GPIOs info according to latest data sheet
-
Removed module_type from setregion command
-
Rephrased description about AP blacklisting feature
1.15
-
Added support for additional memory for SSL connections by configuring BIT(30) in extended TCP/IP feature bitmap.
-
Updated error codes
1.16
1.17
-
Updated MQTT command parameters and MQTT error codes.
Updated MQTT Document
1.18
-
Removed Timeout command.
-
Added Prerequisites for every command.
-
Added MAX length in publish command and few more changes related to MQTT.
1.19
-
Updated HTTP response with additional field for status code
2.0
-
Added the description of BIT(7) for http_client commands, "that bit is used to enable user defined http_content_type".
-
Updated MQTT commands and error codes.
-
Added the weekday parameter and it's description in Set and Get RTC time command.
-
Added NOTE for the configuration of listen_interval in association request related to join command.
-
Added NOTE in 'Open Socket' section, regarding max number of LTCP sockets supported with MQTT connection.
-
Added a note specifying tcp_ip_feature_bit_map[8] has to enabled in oper_mode in "Associate to an Access Point (with WPA2-PSK security) as a client" example and modified the oper_mode accordingly.
-
Modified the description of ht_caps_bit_map[1], "it is used for Channel_Width_Support". Also modified ht_caps_bit_map[8].
-
Merged 'Architecture Overview' and 'Wi-Fi Software Programming' sections.
-
Corrected maximum length of SSID to 32 bytes from 34 bytes.
-
Added description for 'ext_tcp_ip_feature_bit_map[31]'.
-
Removed 'Related Resources' section.
-
Moved 'SPI Interface', 'UART Interface', 'USB Interface' and 'SDIO Interface' sections to - Interfaces'.
-
Moved 'Command Mode Selection' section to 'Bootloader' section.
-
Removed 'PUF Commands'.
-
Renamed 'Using Different Wi-Fi Operation' section to 'Wi-Fi Operation Modes' and moved to Appendix A.
-
Moved 'Wireless Configuration' to Appendix B.
-
Removed 'Wireless Firmware Upgrade', 'Wake on Wireless' sections and 'Power save Modes description from 'Power Mode' section.
-
Renamed 'Appendix A: Sample flow of commands for Wi-Fi over UART' to 'Appendix C: Sample AT command sequences'.
-
Renamed document name from 'Embedded WLAN Software Programming Reference Manual (PRM)' to 'RS9116W Wi-Fi AT Command Programming Reference Manual'.
-
Added the description of WLAN Statistics command.
-
Added a NOTE specifying that the User can configure listen_interval dynamically in Power Mode command.
-
Added a NOTE point in Set Certificate with Indices
saying that the user has to set BIT(31) in tcp_ip_feature_bit_map & BIT(29) in ext_tcp_ip_feature_bit_map to open 3 SSL Client sockets.
-
Provided some information about the support of 3 SSL Client certificates loaded into FLASH in 'Set Certificate with Indices' command.
-
Added the new bit configurations supported in config_feature_bitmap of oper_mode.
-
Added the description of Bit 5 in MODE argument of 'rsi_ipconf' command.
-
Added description for the bit BIT(5) in 'FLAGS' parameter in all the HTTP_CLIENT related commands.
-
Added a NOTE about the port 30000,in Open Socket command
-
Updated Channel Bitmap for 5 GHz
-
Removed all Binary Commands
-
Modified the Username to "redpine" in 'Http Server Credentials From Host' command.
-
Modified open 3 SSL socket information in WLAN PRM
-
Added SNMP GET response in WLAN PRM
-
Renamed the username 'ap_ssid' to 'redpine' in http section.
-
Added note - 'maximum data that can be sent over TCP-SSL/LTCP-SSL is 1370 Bytes only'.
-
Removed SDIO, USB, SPI from Host Interfaces section.
-
Added 'Wireless Features and Mechanisms' section with sub sections 'Connect Application', 'Firmware Upgrade Mechanisms', 'Power Save Modes' and 'Wake on Wireless'.
-
Added 'Changes/Enhancements in WLAN AT Commands, Configurations and Mechanisms' section.
-
Added a note in Opermode section in WLAN AT Commands section.
-
Added/modified description for 'WLAN Statistics' command in 'WLAN Commands' section.
-
Added length for each AT CMD (parameters and responses.)
-
Added bitmap for TLSv1.0 and TLSv1.2 in config_feature_bitmap.
-
Added note for Wifi stats command(only support wifi client mode).
-
Added supported Curve IDs for Ciphers in section ‘Open Socket’.
-
Added HTTP OTAF AT command.
-
Changed HTTP OTAF response format
2.1
-
at+rsi_gain_table Region based user Gain values in 2g has to be doubled before loading Master WLAN Commands
-
Modified the Power save mode 9 figure Master WLAN Commands and Master Power Save Modes
-
Removed the information about "Power save modes" under section Wireless Features and Mechanisms as it is redundant.
-
Corrected Section 5.97 by removing Band command description as it is already described in Section 5.2 .
-
Added a column specifying the bit_info in join_feature_bitmap.
-
Removed "Generate MFI Authentication Signature" command as that command is not validated with the current release.
-
Removed SPI and USB host interaction and Bypass Mode in SPI / USB details from section 2 Bootloader.
2.3
-
Updated config_feature_bitmap[25:24] . Refer WLAN Commands section 5.1.
-
Removed draw.io Watermark from the Power Save Mode figures under section 5.16.
-
Removed info about power save modes, under Wireless Features and Mechanisms, section 7.
-
Added a note about rsi_cfgenable in WLAN commands.
-
Added config_feature_bit_map[18] to select ULP_GPIO_9 as UART2 port for NWP (Network Processor) debug prints.
-
Updated RTS threshold range to 0-2347
-
Added example to Associate to an Access Point with BSSID (With WPA2-PSK Security) as Client and these example present in Master Appendix C: Sample AT command sequences
-
Added note for join command (join with BSSID).
-
Calibration error codes are added under section 6,WLAN Error Codes at Page 215.
-
Removed a note specifying “Enabling Aggregation bit (feature_bit_map[2]) and Low power mode bit(ext_custom_feature_bit_map[19]) in Opermode will result in Wi-Fi data not working. So, they cannot be enabled at the same time.” under section 5.1.
2.4
-
Added the error code "0xFF5F" and it's description under section, WLAN error codes.
-
Made the ext_tcp_ip_feature_bitmap[5] as reserved under section WLAN commands, as that bit is used for an additional WLAN feature which is not generic.
-
Replaced ssl_ciphers with ssl_ciphers_bitmap in at+rsi_tcp command and added information about ssl_ciphers_bitmap
-
Added a note point "Maximum number of SSL sockets to be opened is including user opened sockets and internal sockets" under ext_tcp_ip_feature_bit_map
-
Added new example for 5GHZ in rsi_setregion_ap command.
2.5
-
Modified Response structure and Example for at+rsi_tcp,at+rsi_tcp6,at+rsi_ltcp,at+rsi_ltcp6,at+rsi_ludp,at+rsi_ludp6
-
Updated Bgscan and Roaming thresholds in sample commands in Master WLAN Commands section.
2.6
-
Added two Note points about the Payload_len parameter and pointed the link about the detailed procedure for inputting Payload under User Configurable Gain Table AT command.
-
Added the error code "0x00AF" and it's description under section Master WLAN Error Codes Master WLAN Error Codes
-
Added procedure for loading certificates using at+rsi_cert and at+rsi_cert_inx under Master WLAN Commands section.
2.7
-
Added the description for the bits, BIT(19) and BIT(20) in config_feature_bitmap of Opermode command.
-
Added a note about Region code-4 in Set Region AT command.
-
Added a note about rsi_cfgenable in Master WLAN Commands .
-
Added the description for socket_bitmap[5] in at+rsi_tcp AT command under section, Master WLAN Commands
-
Added reference example for bytes_send_count under bytes transmitted count on socket.
-
Added last channel as 144 for both Europe and Japan regions under setregion command.
-
Removed IAP Init and Load MFI IE AT commands under Master WLAN Commands section.
-
Added number bytes for the command parameters of WLAN Statistics Command under Master WLAN Commands section.
-
Added more explanation about bitmaps of HT_CAPS command under Master WLAN Commands section.
-
Modified TLS versions to EAP TLS versions in config_feature_bit_map of 14 & 15 bits under Master WLAN Commands section.
-
Added Enhanced MAX PSP configuration info in Master WLAN Commands section.
-
Added a note about at+rsi_per command in Master WLAN Commands section.
-
Updated note for join with BSSID command.
-
Updated PER Mode/Transmit Test Command Flow in Continuous Mode in Master Appendix C: Sample AT command sequences.
-
Added note for switching PER continuous wave mode in Master WLAN Commands
-
Added a note for Co-Ex modes which are not supported in Master WLAN Commands.
-
Modified the Opermode reference example in Master WLAN Commands.
-
Updated the Output Power dBm table format in Master WLAN Commands.
-
Mentioned the default port number as 80 for HTTP OTAF command in Master WLAN Commands
-
Updated the information about "offset" response parameter in all HTTP commands in Master WLAN Commands.
-
Removed reserved parameter under scan and join commands in Master WLAN Commands.
-
Added reference example for join command in Master WLAN Commands.
-
Modified parameter sequence order in nwparams command in Master WLAN Commands.
-
Added response for timeout command in Master WLAN Commands.
-
Modified response parameters of mqtt_create in Master WLAN Commands.
-
Modified response parameters of mqtt_delete in Master WLAN Commands.
-
Added note point regarding SSID_LENGTH in scan,join and nwparams command in Master WLAN Commands.
-
Added BURN_XO_FAST_DISABLE in rsi_calib_write command and this bit is used to apply patch for cold temperature issue on A7DB module.
2.8
-
Added the error code "0xFF5F" and its description in Master WLAN Error Codes section.
-
Made the ext_tcp_ip_feature_bitmap[5] as reserved under section 5.1 of Master WLAN Commands
-
Replaced ssl_ciphers with ssl_ciphers_bitmap in at+rsi_tcp command and added information about ssl_ciphers_bitmap, in Master WLAN Commands.
-
Added a note about "Maximum number of SSL sockets" under ext_tcp_ip_feature_bit_map in Master WLAN Commands.
-
Added new example for 5GHZ in setregion_ap command, of Master WLAN Commands
-
Modified Response structure and Example for at+rsi_tcp,at+rsi_tcp6,at+rsi_ltcp,at+rsi_ltcp6,at+rsi_ludp,at+rsi_ludp6 in Master WLAN Commands
-
Added two Note about the Payload_len parameter and how to provide input for Payload in User configurable Gain Table command, of Master WLAN Commands
-
Added the Procedure for inputting AT command with a mix of ASCII and decimal format by taking user gain_table as an example in Master Appendix C: Sample AT command sequences
-
Added the error code "0x00AF" and its description in Master WLAN Error Codes section.
-
Added two new commands at+rsi_calib_write , at+rsi_freq_offset in calibration functions of Master WLAN Commands
-
Updated Bgscan, and Roaming thresholds in Master WLAN Commands
-
Added the description for the bits, BIT(19) and BIT(20) in config_feature_bit_map, in Master WLAN Commands
-
Added a note about Region code-4 in Set Region command, of Master WLAN Commands
-
Changed WLAN keep alive time as 10s by default in Request timout command of Master WLAN Commands
-
Added the Pre condition about when cfgget command should be called in Get information about Stored configuration command of Master WLAN Commands
-
Added the description for socket_bitmap[5] in Open Socket command of Master WLAN Commands.
-
Added reference example for at+rsi_bytes_sent_count command in Master WLAN Commands.
-
Added last channel as 144 for both Europe and Japan regions in at+rsi_setregion command of Master WLAN Commands.
-
Removed IAP Init and Load MFI IE AT commands.
-
Added number of bytes for the command parameters of WLAN Statistics Command in Master WLAN Commands
-
Added more explanation about bitmaps of at+rsi_ht_caps command in Master WLAN Commands
-
Modified TLS versions to EAP TLS versions in config_feature_bit_map of 14 & 15 in Master WLAN Commands.
-
Added a note about at+rsi_per command in Master WLAN Commands
-
Added a note for join command in Master WLAN Commands
-
Updated comment for PER Mode/Transmit Test Command Flow in Master Appendix C: Sample AT command sequences.
-
Added note for switching PER Continuous wave mode in Master WLAN Commands
-
Added a note for Co-Ex modes which are not supported in Operating mode command of Master WLAN Commands
-
Modified the Opermode reference example in Master WLAN Commands(Not required AFAIK)
-
Updated the Output Power dBm table format in at+rsi_per command of Master WLAN Commands
-
Mentioned the default port number as 80 for HTTP OTAF command in Master WLAN Commands.
-
Updated the information about "offset" response parameter in all HTTP commands of Master WLAN Commands.
-
Added the new command at+rsi_udp in Master WLAN Commands.
-
Removed reserved parameters in Scan and Join commands in Master WLAN Commands.
-
Added reference example for join command in Master WLAN Commands.
-
Modified parameter sequence order in Query Network Parameters Section in Master WLAN Commands.
-
Added response format for Request Timeout command in Master WLAN Commands.
-
Updated response structure for mqtt_create in MQTT Client section in Master WLAN Commands.
-
Updated response structure for mqtt_delete in MQTT Client section in Master WLAN Commands.
-
Added note point regarding SSID_LENGTH in Scan and Join commands in Master WLAN Commands.
-
Added an example in Set EAP Configuration in Master WLAN Commands
-
Added reserved field in PER Statistics of the Module section of Master WLAN Commands
-
Updated Flow diagram in Send Data section in Master WLAN Commands
-
Removed operating mode ‘1’ (WiFi direct) from all the sections.
-
Updated notes in send data section in Master WLAN Commands
-
Updated note in Open Socket section in Master WLAN Commands
-
Added an example for Wireless firmware upgradation in Master WLAN Commands
-
Added at+rsi_calib_write, at+rsi_freq_offset commands to perform chip calibration in Master WLAN Commands
-
Added BIT(18) in config_feature_bit_map in opermode section for selecting ULP_GPIO_9 as UART2 port for NWP (Network Processor) debug prints in Master WLAN Commands
-
Added BIT(19) in config_feature_bit_map in opermode section for disabling higher MCS rates(i.e., MCS5, MCS6, MCS7) in Master WLAN Commands
-
Added BIT(20) in config_feature_bit_map in opermode section for disabling Short GI in Master WLAN Commands
-
Added BIT(26) in config_feature_bit_map in opermode section to enable enhanced max PSP for Power save in Master WLAN Commands
-
Added a bit EXT_TCP_IP_FEAT_SSL_HIGH_PERFORMANCE in EXT_TCPIP_FEATURE_BITMAP in opermode section for enabling high-performance socket in SSL in Master WLAN Commands
-
Added a flag RSI_HTTP_USER_DEFINED_CONTENT_TYPE in at+ rsi_http_client_put_start command for user-defined content type in extended header of HTTP Put request in Master WLAN Commands
-
Added new bitmap ssl_ciphers_bitmap in Open Socket section for selecting specific cipher in SSL in Master WLAN Commands
-
Updated param lengths info for
-
user gain table
-
DNS Update
-
FW version
-
ping
-
loading webpage
-
JSON create
-
Feature frame Sections in Master WLAN Commands.
-
In PER/Transit test command, updated the min and max supported power values in Master WLAN Commands.
-
Updated channel number tables and note regarding auto channel selection in Master WLAN Commands.
-
Updated max supported SSID length
-
ap_conf command
-
scan command
-
join sections in Master WLAN Commands.
-
Added supporting security modes table in join command in Master WLAN Commands.
-
Updated the ulp_mode_enable param info, powersave modes info in powersave section in Master WLAN Commands.
-
Updated supporting opermode modes info in all sections in Master WLAN Commands.
-
Updated Note regarding IPv6 in all sections in Master WLAN Commands.
-
Updated info about unsupported features for this current release are :
-
SNMP,
-
FTP,
-
SNTP broadcast method,
-
SMTP,
-
POP3 in Master WLAN Commands.
-
Updated the note and params info of the Open Socket section in Master WLAN Commands.
-
Updated the query a listening socket's active connection status command params info in Master WLAN Commands.
-
Added demo AT command sequence for
-
BG scan,
-
Roam params commands
-
Opening a UDP broadcast IPv4 Socket in Station and Access Point modes
sections in Master Appendix C: Sample AT command sequences.
-
Added HTTP Get command length of extended header param and added example format and response format for the HTTP get and HTTP post sections in Master WLAN Commands.
-
Added note for HTTP post command for max supported chunk length in Master WLAN Commands.
-
Updated the DFS Client description, and response format for example for various Silicon versions in Master WLAN Commands.
-
Added note max supported multicast groups in multicast command in Master WLAN Commands.
-
Added pre-condition for
-
erasing JSON data,
-
clear the webpages,
-
webpage bypass,
-
bytes transmitted count on the socket,
-
debug prints on UART,
-
UART hardware flow control,
-
MDNS & DNS-SD,
-
OTAF,
-
store configuration in flash memory,
-
autojoin /Auto create,
-
set RTC time,
-
feature frame,
-
Get RAM dump,
-
configure Tx, Rx buffer ratio,
-
commands
-
HTTP Get command
-
HTTP post data command
-
multicast command
-
ping command sections in Master WLAN Commands.
-
Added info and note for max supported Register service param in MDNSD command in Master WLAN Commands.
-
Removed MFI Authentication cert command info in Master WLAN Commands.
-
Removed TSF command info in Master WLAN Commands.
2.9
-
Added Master Appendix D: Host interface detection issue on CC0/CC1 modules at cold temperatures
2.10
-
Added the procedure to be followed if the user gets “Valid firmware not present” message even for correct firmware, under Wireless firmware upgradation section of Bootloader.
2.11
-
Added Korea domain under commands: rsi_setregion, rsi_usercfg.
-
Added Korea domain regulations table under rsi_setregion command.
-
Added WPA3 security mode.
-
Added an example: "Associating to an Access Point (with WPA3-PSK Security) as Client" in Sample AT command sequences.
-
Added note under join_feature_bitmap in rsi_join command.
-
Changed the description of error code : 0x0033 in wlan error codes.
-
Added DFS client, PTA 3-Wire Co-Existence under wireless features and mechanisms.
2.12
-
Added a note that TCP_IP BYPASS mode is currently not supported under the section of wifi-operation-modes.
-
Updated a note about recalibrating the gain offset after it has been burnt to flash in at+rsi_calib_write command, under wlan commands.
-
Updated a note about maximum published window size in at+rsi_socket_config command, under wlan commands.
-
Changed AT PRM images and text for powersave mode 8 and 9, explaining the new logic, under wlan commands.
-
Removed unsupported 40 MHz feature.
-
Updated a note that Wi-Fi direct mode is not supported in Opermode section, under wlan commands.
-
Added a note with list of all AT commands that affect the stored configuration in at+rsi_cfgsave command, under wlan commands.
-
Added a note that hardware flow control is not supported in auto-create/auto-join mode.
-
Added description of security mode 6 in at+rsi_join command, under wlan commands.
-
Removed the description of RF current mode, as it is not supported.
-
Made the required changes to the descriptions of rf_type and afe_type and also updated the example in at+rsi_feat_frame command, under wlan commands.
-
Added new command
at+rsi_gpioconf
under the section, wlan-commands.
-
Added new SNTP error code(0xBB08) in WLAN error codes.
-
Added separate table for DFS channels in 5GHz in at+rsi_scan command.
-
Added psk_type '5' in the response structure of at+rsi_psk command.
-
Removed Wireless Firmware upgrade through webpage procedure, as it is currently not supported.
-
Added new AT command 'rsi_store_server_ip_port' and added new error code '0xFF24'.
-
Added new error code '0xFF75'.