AT Command Examples
The following AT command examples show how to operate the module in different modes.
Note!
-
All commands must be terminated with
\r\n(CRLF).
Create an Access Point
at+rsi_opermode=6,1,16,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_ipconf=0,192.168.50.1,255.255.255.0,192.168.50.1
This command can be used optionally in this flow to configure the IP (192.168.50.1 in this example) of the AP.
If this command is not issued, a default IP of 192.168.100.76 will be used.
at+rsi_apconf=1,AP_SSID,2,2,12345678,300,2,4
This command will configure the SSID of the AP to
AP_SSID
and password will be set to
12345678
.
at+rsi_join=AP_SSID,0,2
This command will create the Access Point with SSID
AP_SSID
.
A client device (Named
Device A
in this example) can now associate to the AP, open sockets and transfer data.
For example,
at+rsi_ltcp=5001,5,0
Opens a server TCP socket inside the module with port number 5001 with TOS (type of service) type 0 and max clients support count as 5.
A client socket at the remote node (Device A) can connect to the server socket.
To send a test string
This is a test
from the module to the remote node, issue the below command
at+rsi_snd=1,14,0,0,This is a test
If the remote node (Device A) sends data, the module receives the data and transfers to the Host with a
AT+RSI_READ
message
Another client (Named
Device
in this example) can also connect to the Access Point in the module and data transfer can be executed between Device A and Device B through the AP. A maximum of 4 clients are supported.
Associate to an AP (with WPA2-PSK Security)
at+rsi_opermode=0,1,260,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_scan=0
This command scans for the Access Points and reports the APs found.
Note!
- After a scan, if the user want to join an AP as enterprise client then user need to issue a soft reset first and then follow the flow of commands as in “Associate to an Enterprise Security enabled Access Point as a client”
at+rsi_psk=1,12345678
This command configures the PSK to be used to associate to the Access Point.
at+rsi_join=Test_AP,0,2,2
This command associates the module to the AP.
It is assumed that the SSID of the AP is Test_AP with WPA2-PSK security key of
12345678
.
at+rsi_ipconf=1,0,0,0
This configures the IP address of the module in DHCP mode.
at+rsi_dnsserver=1,0,0
Optional command to provide the IP address of a DNS server.
Note!
- If the user wants to use the DNS command to get DNS server IP, then the user must enable tcp_ip_feature_bit_map[8] in the oper_mode command.
at+rsi_dnsget=\<domain_name\>,1
Optional command to resolve IP of a given domain name.
at+rsi_ltcp=5001,5,0
Opens a server TCP socket inside the module with port number 5001 with TOS(type of service) type 0 and max clients support count as 5.
Now connect another client (called
Device A
in this example) to the same Access Point and open a client socket to bind to the module’s socket.
To send a test string
This is a test
from the module to the remote node, issue the below command
at+rsi_snd=1,14,0,0,This is a test
If the remote node (Device A) sends data, the module receives the data and transfers to the Host with a
AT+RSI_READ
message
Associate to an AP (with WPA3-PSK Security)
at+rsi_opermode=0,1,260,2147483648,8192
Set the operating mode of the module.
at+rsi_band=0
Set the operating band of the module.
at+rsi_init
Initialize the module.
at+rsi_scan=0
Scan for the Access points and report the APs found.
Note!
- After a scan, if the user want to join an AP as enterprise client then user need to issue a soft reset first and then follow the flow of commands as in “Associate to an Enterprise Security enabled Access Point as a client”.
at+rsi_psk=1,12345678
Configure the PSK to be used to associate to the Access Point.
at+rsi_join=Test_AP,0,2,7,96,0,0,1
Associate the module to the AP.
It is assumed that the SSID of the AP is Test_AP with WPA3-PSK security key of
12345678
.
at+rsi_ipconf=1,0,0,0
Configure the IP address of the module in DHCP mode.
at+rsi_dnsserver=1,0,0
Optional command to provide the IP address of a DNS server.
Note!
- If the user wants to use the DNS command to get DNS server IP, then the user must enable tcp_ip_feature_bit_map[8] in the oper_mode command.
at+rsi_dnsget=\<domain_name\>,1
Optional command to resolve IP of a given domain name.
at+rsi_ltcp=5001,5,0
Open a server TCP socket inside the module with port number 5001 with TOS(type of service) type 0 and max clients support count as 5.
Now connect another client (called
Device A
in this example) to the same Access Point and open a client socket to bind to the module’s socket.
To send a test string
This is a test
from the module to the remote node, issue the below command
at+rsi_snd=1,14,0,0,This is a test
If the remote node (Device A) sends data, the module receives the data and transfers to the Host with a
AT+RSI_READ
message
Associate to an AP (with WEP Security)
at+rsi_opermode=0,2,4,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_scan=0
This command scans for APs and reports the APs found.
at+rsi_wepkey=0,ABCDE12345,0,0,0
This command configures the PSK to be used to associate to an Access Point.
at+rsi_join=Test_AP,0,2,3
This command associates the module to the AP.
at+rsi_ipconf=1,0,0,0
This configures the IP address of the module in DHCP mode.
at+rsi_ltcp=5001,5,0
Opens a server TCP socket inside the module with port number 5001 with tos(type of service) type 0 and max clients support count as 5.
Now connect another client (called
Device A
in this example) to the same Access Point and open a client socket to bind to the module’s socket.
To send a test string
This is a test
from the module to the remote node, issue the below command
at+rsi_snd=1,14,0,0,This is a test
If the remote node (Device A) sends data, the module receives the data and transfers to the Host with a
AT+RSI_READ
message
Associate to an AP with WPS Enabled
at+rsi_opermode=0,2,4,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_scan=0
This command scans for available Aps and reports the Aps found.
at+rsi_join=,0,2
This command associates the module to the AP using WPS push button method. Note that, we have to send null in place of ssid .
at+rsi_ipconf=1,0,0,0
This command configures the IP address of the module in DHCP mode.
at+rsi_ltcp=5001,5,0
Opens a server TCP socket inside the module with port number 5001 with tos (type of service) type 0 and max clients support count as 5.
Now connect another client (called
Device A
in this example) to the same Access Point and open a client socket to bind to the module’s socket.
To send a test string
This is a test
from the module to the remote node, issue the below command
at+rsi_snd=1,14,0,0,This is a test
If the remote node (Device A) sends data, the module receives the data and transfers to the Host with a
AT+RSI_READ
message.
Associate to an AP with Enterprise Security
The example demonstrates the flow for EAP-TLS mode.
at+rsi_opermode=2,0,4,0
This sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_eap=TLS,MSCHAPV2,user1,password1
This command sets the Enterprise mode.
at+rsi_scan=0
This command scans for Aps and reports the Aps found.
Note!
- After a scan, if the user want to join an AP with WPA2-AES PSK then user need to issue a soft reset first and then follow the flow of commands as in “Associate to an Access Point (with WPA2-PSK security) as a client”.
at+rsi_cert=1,cert_len,key_password,<TLS certificate>
This command provides the TLS certificate to the module
at+rsi_join=Test_AP,0,2,4
This command associates the module to the AP. It is assumed that the SSID of the AP is Test_AP.
at+rsi_ipconf=1,0,0,0
This command configures the IP address of the module in DHCP mode.
at+rsi_ltcp=5001,5,0
Opens a server TCP socket inside the module with port number 5001 with tos(type of service) type 0 and max clients support count as 5.
Now connect another client (called
Device A
in this example) to the same Access Point and open a client socket to bind to the module’s socket.
To send a test string
This is a test
from the module to the remote node (Device A), issue the below command
at+rsi_snd=1,14,0,0,This is a test
If the remote node (Device A) sends data, the module sends the received data with a AT+RSI_READ message to the Host.
PER Tx Mode in Burst Mode
at+rsi_opermode=8
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_feat_frame=0,1,0,0,1,0
This command sets the correct RF type and path
at+rsi_init
This command initializes the module.
at+rsi_antenna=0
This is the command for antenna .
at+rsi_setregion = 1,4
This command configures the region to worldwide
at+rsi_per=1,127,139,1000,0,6,0,0,0,0
This command sends the packets in burst mode in channel number 6, with packet length 1000, with max power, with data rate 6Mbps.
at+rsi_per=0
To stop transmission
PER Tx Mode in Continuous Mode
at+rsi_opermode=8
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_feat_frame=0,1,0,0,1,0
This command sets the correct RF type and path
at+rsi_init
This command initializes the module.
at+rsi_antenna=0
This is the command for antenna
at+rsi_setregion = 1,4
This command configures the region to worldwide
at+rsi_per=1,127,139,260,1,6,0,0,0,0
This command starts Continuous mode in channel number 6, with packet length 260, with max power, with data rate 1Mbps.
at+rsi_per=0
To stop transmission
PER Tx Mode in Continuous Wave Mode
at+rsi_opermode=8
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_feat_frame=0,1,0,0,1,0
This command sets the correct RF type and path
at+rsi_init
This command initializes the module.
at+rsi_antenna=0
This is the command for antenna .
at+rsi_setregion = 1,4
This command configures the region to worldwide
at+rsi_per=1,127,139,260,1,6,0,0,0,0
This command starts Continuous mode in channel number 6, with packet length 260, with max power, with data rate 1Mbps.
at+rsi_per=0
To stop transmission
at+rsi_per=1,127,0,260,2,6,0,0,0,0
This command sends the packets in Continuous Wave mode 2 in channel number 6, with packet length 260, with max power, with data rate 1Mbps.
PER Receive Mode
at+rsi_opermode=8
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_feat_frame=0,1,0,0,1,0
This command sets the correct RF type and path
at+rsi_init
This command initializes the module.
at+rsi_setregion = 1,4
This command configures the region to worldwide
at+rsi_per_stats=0,1
This command here is used to see the WLAN Receive stats.
at+rsi_per_stats=1
This command is used to stop the WLAN PER RECEIVE STATS
WLAN Scan in Client
at+rsi_opermode=0,1,4,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_scan=0
This command scans for available APs in the channels mentioned in channel_bit_map_2_4 in 2.4GHz, channel_bit_map_5 in 5GHz and reports the APs found.
at+rsi_join=test,0,2,0
This command associates the module to the AP in open mode.
at+rsi_bgscan=1,1,10,4,10,15,20,1
This command enables the back ground scan functionality in module.
Here instant bgscan is enabled hence module will send probe requests in the air on to the channels mentioned in the channel bitmap and results will go to host.
at+rsi_ipconf=1,0,0,0
This command configures the IP address of the module in DHCP mode.
Roaming as a Client
at+rsi_opermode=0,1,4,0
This command sets the operating mode of the module.
at+rsi_band=0*
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_scan=0
This command scans for available APs in the channels mentioned in channel bitmap and reports the APs found.
at+rsi_join=test,0,2,0
This command associates the module to the AP in open mode.
at+rsi_bgscan=1,1,10,4,10,15,20,1
This command enables the back ground scan functionality in module.
Here instant bgscan is enabled hence module will send probe requests in the air and results will go to host and in background scan will be continued based upon the parameters given in the command.
at+rsi_roam_params= 1,5,2
This command enables roaming in module.
at+rsi_ipconf=1,0,0,0
This command configures the IP address of the module in DHCP mode.
WMM Powersave as a Client
at+rsi_opermode=0,1,4,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_scan=6,test
This command scans for available AP in the given channel with the given SSID and reports, if the AP is found.
at+rsi_wmm_config=1,0,0,1
This command enables the WMM feature in the module.
at+rsi_join=test,0,2,0
This command associates the module to the AP which is in open mode.
at+rsi_pwmode=1
This command configures the power save mode 1 in the module.
at+rsi_ipconf=1,0,0,0
This command configures the IP address of the module in DHCP mode.
Open a Multicast IPv4 Socket
at+rsi_opermode=0,1,4,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_scan=0
This command scans for APs and reports the APs found.
at+rsi_join=Test_AP,0,2,0
This command associates the module to the AP.
at+rsi_ipconf=1,0,0,0
This configures the IP address of the module in DHCP mode.
at+rsi_multicast=1,239.0.0.0
To join IPv4 multicast group with address 239.0.0.0.
at+rsi_ludp=5001
To open ludp socket with port number 5001.
at+rsi_multicast=0,239.0.0.0
To leave multicast group with address 239.0.0.0.
Sends an AT command with a mix of ASCII and Array input
Let us consider the example of user gain table for giving the input in ASCII and array input.
For 2.4 GHz
at+rsi_opermode=6,1,48,0
This command sets the operating mode of the module.
Note!
- It is not mandatory that the first parameter of opermode is AP only. User can provide any other mode except PER.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_gain_table=1,0, 67,array(3,0,13,1,34,20,20,2,34,28,28,3,34,32,32,4,34,36,36,5,34,38,38,6,34,40,40,7,34,38,38,8,34,36,36,9,34,32,32,10,34,32,32,11,34,24,24,12,34,16,24,13,34,12,12,2,17,255,20,16,16,4,17,255,26,20,20)
This command is used to set the user gain table. User can give input either in hex or decimal. For instance if the user intends to give input in decimal format, then the following procedure can be followed to run the Application using Docklight tool to provide input in decimal format.
- Go to Docklight and provide sequence by double clicking on the left side provided send sequences column and enter the sequence normally up to init.
- For at+rsi_gain_table command, Please enter the sequence normally in ASCII format, up to third parameter as shown in below figure.
.
- Now for giving fourth Parameter i.e Payload ,user need to change the mode of the input either hex or decimal. In the screenshot decimal format is shown.
- After the switching the mode to decimal, the input sequence will look like the following Figure.
.
- Now from fourth parameter on wards, give the input in decimal format without any commas as the Application is expecting an array input(decimal) as shown in below figure.
.
- After providing the payload of the gain table, the user has to again switch back to the ASCII format for providing \<CR> and \<LF>. Please follow the below figure. With this the gain_command sequence is successfully completed.
.
- Once the sequence of commands and gain_table parameters are given properly, and executed the output will look like the below Figure.
.
For 5 GHz
at+rsi_opermode=6,1,48,0
This command sets the operating mode of the module.
Note!
- It is not mandatory that the first parameter of opermode is AP only. User can provide any other mode except PER.
at+rsi_band=1
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_gain_table=2,0,35,array(2,0,6,1,9,10,2,8,9,100,4,4,3,6,8,149,3,3,4,6,7,2,4,1,9,10,2,8,10,3,6,8,4,6,7)
This command is used to set the user gain table. User can give input either in hex or decimal. For instance if the user intends to give input in decimal format, then please consider the following
Please follow the below Procedure to run the Application using Docklight tool to provide input in decimal format.
- Go to Docklight and provide sequence by double clicking on the left side provided send sequences column and enter the sequence normally up to init.
- For at+rsi_gain_table command, Please enter the sequence normally in ASCII format, up to third parameter as shown in below figure.
.
- Now for giving fourth Parameter i.e Payload ,user need to change the mode of the input to decimal in which each ASCII character is equivalent to three decimal digits.
- After the switching the mode to decimal, the input sequence will look like the following Figure.
.
- Now from fourth parameter on wards, give the input in decimal format without any commas as the Application is expecting an array input(decimal) as shown in below figure.
.
- After providing the payload of the gain table, the user has to again switch back to the ASCII format for providing \<CR> and \<LF>. Please follow the below figure. With this the gain_command sequence is successfully completed.
.
- Once the sequence of commands and gain_table parameters are given properly, and executed the output will look like the below Figure.
.
Open a UDP broadcast IPv4 Socket in Client Mode
at+rsi_opermode=0,1,4,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_scan=0
This command scans for APs and reports the APs found.
at+rsi_psk=1,987654321
This command configures the PSK to be used to associate to the Access Point.
at+rsi_join=Test_AP,0,2,2
This command associates the module to the AP.
at+rsi_ipconf=1
This command configures the IP address of the module in DHCP mode.
at+rsi_ludp=5000,0,0
Opens an UDP server socket inside the module with port number 5000 with tos (type of service) type 0 and socket bitmap[0] (synchronous data read).
To send a test string
12345678
from the module to the remote node (Device A), issue the below command
at+rsi_snd=1,200,255.255.255.255,5000,12345678
If the remote node (Device A) sends data, the module sends the received data with an AT+RSI_READ message to the Host.
at+rsi_snd=1,750,192.168.43.255,5000,123456789012345678901234567890123456789012345678901
2345678901234567890123456789012345678901234567890123456789012345678901234567890123
4567890123456789012345678901234567890123456789012345678901234567890123456789012345
6789012345678901234567890123456789012345678901234567890123456789012345678901234567
8901234567890123456789012345678901234567890123456789012345678901234567890123456789
0123456789012345678901234567890123456789012345678901234567890123456789012345678901
2345678901234567890123456789012345678901234567890123456789012345678901234567890123
4567890123456789012345678901234567890123456789012345678901234567890123456789012345
6789012345678901234567890123456789012345678901234567890123456789012345678901234567
8901234567890123456789012345678901234567890
Open a UDP broadcast IPv4 Socket in Access Point Mode
at+rsi_opermode=6,1,18,0
This command sets the operating mode of the module.
at+rsi_band=0
This command sets the operating band of the module.
at+rsi_init
This command initializes the module.
at+rsi_ipconf=0,192.168.12.105,255.255.255.0,192.168.12.105
This command configures the IP address of the module.
at+rsi_apconf=0,UDP_TEST,2,2,12345678,100,3,3
This command will configure the SSID of the AP to
UDP_TEST
and password will be set to
12345678
.
at+rsi_join=UDP_TEST,0,2,6
This command associates the module to the AP.
at+rsi_ludp=5000,0,0
Opens an UDP server socket inside the module with port number 5000 with tos (type of service) type 0 and socket bitmap[0] (synchronous data read).
at+rsi_snd=1,25,255.255.255.255,5000,Sigmavision_TRHH:60100067
If the remote node (Device A) sends data, the module sends the received data with an AT+RSI_READ message to the Host.
Wireless Firmware Upgradation Example in STA mode
The firmware of the module can be upgraded through web page . Execution:
- Bring up the Silabs_STA using the following commands:
at+rsi_opermode=0,1,22,2147483648,2097152
at+rsi_band=0
at+rsi_init
at+rsi_scan=0,Silabs_AP
at+rsi_psk=1,13456789
at+rsi_join=Silabs_AP,0,2,2
at+rsi_ipconf=1,0,0,0
- Give the IP address of the module in the browser(in this case 192.168.1.3), Redpine configuration page will be open.
- Click on Administration.
- Choose an .rps file from PC and click on upgrade.
- After clicking upgrade button on webpage, module will send asynchronous notification
AT+RSI_FWUPREQ
- Module has to issue the following command:
at+rsi_fwupok
- If host has failed to give above command within specified timeout(~20 seconds), request will expire and upgradation process terminates.
-
After the firmware upgradation is successful, a popup message "Firmware Upgraded Successfully" will appear on webpage screen. And asynchronous success message
AT+RSI_FWUPSUCCESSis send to host from the module.
Wireless Firmware Upgradation Example
The firmware of the module can be upgraded through web page . Sequence of events:
- Start the Silicon labs device as an AP.
- Allows stations to connect to update firmware through webpage.
- A Laptop having WiFi card can be used as Wireless station.
- Silicon Labs device creates a network and acts as router between the connected stations
- Upgrade the received Firmware into the device.
Execution
- Bring up the Silabs_AP using the following commands:
at+rsi_opermode=6,1,18, 2147483648,2097152
at+rsi_band=0
at+rsi_init
at+rsi_apconf=0,Silabs_AP,0,0,0,100,5,4
at+rsi_join=Silabs_AP,0,2,0,0,0,0
.
Note!
- ‘Authentication Required’ pop up window will only appear if BIT[23] in Custom feature bitmap is enabled. In that case opermode command should be at+rsi_opermode=6,1,18,2155872256,2097152\r\n Login credentials in case of ‘Authentication required’ : User Id : redpine password : admin
- Connect to the Silabs_AP from a STA(in this example a laptop).
.
- Open the AP configuration page by entering the IP address of the module in the browser.(in this case 192.168.100.76 by default).
.
- Click on Administration.
- Choose a .rps file and click on upgrade.
.
- Upon clicking upgrade button on the webpage, host will get asynchronous notification
AT+RSI_FWUPREQ
if it is connected to module through UART or USB-CDC interface.
- So host has to issue the following command:
at+rsi_fwupok
- If host failed to reply within specified timeout(~20 seconds), request will expire and upgradation process terminates.
.
-
After the firmware upgradation is successful, a popup will appear on remote peer screen to intimate the process completion . An asynchronous success message
AT+RSI_FWUPSUCCESSis forwarded to the host connected with the module.
.
-
On firmware upgradation failure, there will be a pop-up on remote peer screen to intimate the process failure. Similarly, an asynchronous failure message
AT+RSI_FWUPFAILED(for UART/USB-CDC) will be forwarded to the host connected with the module.
Note!
- Wireless firmware upgradation is supported only for the latest versions of Firefox and Google Chrome.
- When the user clicks on the upgrade button, the module starts erasing flash for storing image. This may take few seconds, after this, upgradation will start automatically.
- After wireless firmware upgrade, the user needs to wait for few minutes (~ 1.5 minutes) after reboot so that the bootloader will copy upgraded image into the actual flash location.
- Firmware upgrade will fail if server(module) does not receive packets from the client (browser) within the timeout i.e., 40 seconds.
- Firmware upgradation failed message will be received if server/client closes the TCP connection.
- Wireless firmware upgradation is possible in client mode also. Enter the IP address of the module in browser to land on configuration page.
Storing Configuration From User
This is an example sequence to store configuration from user.
at+rsi_opermode=0,1,4,0
at+rsi_band=1
at+rsi_init
at+rsi_usercfg=1294,payload in hex format>
Payload hex format
.
Above command configures module with the values set by the user. The values set here are:
| Parameter | Value |
|---|---|
ssid
|
silabs |
psk
|
password |
opermode
|
0 |
feature_bit_map
|
1 |
tcp_ip_feature_bit_map
|
4 |
custom_feature_bit_map
|
0 |
band
|
1 |
cfg_enable
|
1 |
ip address
|
192.168.1.2 |
scan
|
0 (scans all channels) |
Note!
- To configure more parameters, refer Store configuration structure parameters .
- Parameters that are not required by the user can be configured as NULL values.
at+rsi_cfgenable=1
This command enables auto-join or auto-create on power up. To check the configured parameters give:
at+rsi_cfgget?
On power up, after bootloader options, immediately after the firmware is loaded you would receive OKC if the AP is available and the parameters are given correctly.
If you want to give new configuration, disable the current configuration using
at+rsi_cfgenable=0