Error Codes#
RTL library Error Codes.
Enumerations#
RTL error code.
Enumeration Documentation#
sl_rtl_error_code#
sl_rtl_error_code
RTL error code.
Enumerator | |
---|---|
SL_RTL_ERROR_SUCCESS | Successful execution / estimation complete. |
SL_RTL_ERROR_ARGUMENT | Invalid argument. |
SL_RTL_ERROR_OUT_OF_MEMORY | Memory / allocation failure. |
SL_RTL_ERROR_ESTIMATION_IN_PROGRESS | Estimation not yet finished. |
SL_RTL_ERROR_NUMBER_OF_SNAPHOTS_DO_NOT_MATCH | Initialized and calculated number of snapshots do not match. |
SL_RTL_ERROR_ESTIMATOR_NOT_CREATED | Estimator not yet created. |
SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED | Estimator already created, operation is not supported. |
SL_RTL_ERROR_NOT_INITIALIZED | Library item not yet initialized. |
SL_RTL_ERROR_INTERNAL | An internal error occurred. |
SL_RTL_ERROR_IQ_SAMPLE_QA | IQ sample quality analysis failed. |
SL_RTL_ERROR_FEATURE_NOT_SUPPORTED | The requested feature is not supported by the library. |
SL_RTL_ERROR_INCORRECT_MEASUREMENT | The error of the last measurement for this locator was too large. |
SL_RTL_ERROR_CS_CHANNEL_MAP_TOO_SPARSE | Too many skipped channels in the proposed channel map. |
SL_RTL_ERROR_CS_CHANNEL_MAP_TOO_FEW_CHANNELS | Too few channels in the proposed channel map. |
SL_RTL_ERROR_CS_CHANNEL_SPACING_TOO_LARGE | Channel spacing is too large in the proposed channel map. |
SL_RTL_ERROR_POOR_INPUT_DATA_QUALITY | The input data quality is poor. |
SL_RTL_ERROR_LAST | Number of error codes. |