Public Attributes#
Public Attribute Documentation#
min_main_mode_steps#
uint8_t sl_rtl_cs_params::min_main_mode_steps
Minimum number of CS main mode steps to be executed before a sub mode step. Currently only value 2 is supported. Field is ignored if sub mode is set to SL_RTL_CS_MODE_NONE.
max_main_mode_steps#
uint8_t sl_rtl_cs_params::max_main_mode_steps
Maximum number of CS main mode steps to be executed before a sub mode step. Currently only value 2 is supported. Field is ignored if sub mode is set to SL_RTL_CS_MODE_NONE.
main_mode_repetition#
uint8_t sl_rtl_cs_params::main_mode_repetition
Number of main modes steps repeated from previous subevent (0, 1, 2, 3).
channel_map_repetition#
uint8_t sl_rtl_cs_params::channel_map_repetition
Number of times the channel map is repeated. Currently only value 0x01 is supported.
channel_selection_type#
uint8_t sl_rtl_cs_params::channel_selection_type
Channel selection algorithm. Currently only value 0x01 (Channel Selection Algorithm #3b) is supported.
num_antenna_paths#
uint8_t sl_rtl_cs_params::num_antenna_paths
Number of antenna paths supported by the local controller for the CS tone exchanges. - Range: 1 to 4. The number of antenna paths used during the phase measurement stage of the CS step. - Value: 0. Phase measurement does not occur during the CS step, therefore ignored.
connection_interval#
uint16_t sl_rtl_cs_params::connection_interval
Connection interval in units of 1.25 ms