RTL API for Ranging Service (RAS)#
RTL API for Ranging Service (RAS)
This is a supplementary RAS API wrapper for the Channel Sounding (CS) API. The RAS API provides a method to calculate distance and confidence estimates based on RAS format data. Please refer to the CS API for initialization and configuration of the CS libitem.
Note
The legacy sl_rtl_ras_process() API follows the same guidance as legacy sl_rtl_cs_* APIs: direct use is not recommended for new applications. Use the RTL Service APIs (sl_rtl_service_*) as the replacement interface. In projects where an RTOS kernel is present, sl_rtl_ras_process() returns SL_RTL_ERROR_FEATURE_NOT_SUPPORTED.
Modules#
sl_rtl_ras_ranging_data_header
sl_rtl_ras_procedure.initiator
sl_rtl_ras_procedure.reflector
Typedefs#
Functions#
Typedef Documentation#
Function Documentation#
sl_rtl_ras_process#
enum sl_rtl_error_code sl_rtl_ras_process (sl_rtl_cs_libitem * item, const uint8_t num_procedures, const sl_rtl_ras_procedure * procedure_data)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rtl_cs_libitem * | [in] | item | Pointer to the initialized and configured CS libitem |
| const uint8_t | [in] | num_procedures | Number of procedures in the procedure_data array |
| const sl_rtl_ras_procedure * | [in] | procedure_data | Data structure with the completed RAS procedures |
Process RAS procedures to calculate distance estimate.
Returns
SL_RTL_ERROR_SUCCESS if successful and SL_RTL_ERROR_ESTIMATION_IN_PROGRESS if estimate is not yet final and more input data needs to be processed.
Calculate the distance estimate from the given procedure data. Use sl_rtl_cs_get_distance to fetch the latest distance estimate. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.