Angle of Arrival / Departure
Angle of Arrival / Departure.
| Data Structures | |
| struct | sl_rtl_clib_iq_sample_qa_antenna_data_t | 
| struct | sl_rtl_clib_iq_sample_qa_dataset_t | 
| Macros | |
| #define | SL_RTL_AOX_IQ_SAMPLE_QA_ALL_OK 0 | 
| #define | SL_RTL_AOX_IQ_SAMPLE_QA_FAILURE 0xffffffff | 
| #define | SL_RTL_AOX_IQ_SAMPLE_QA_CLEAR_BIT (code, bit) (code &= ~(1UL << bit)) | 
| #define | SL_RTL_AOX_IQ_SAMPLE_QA_SET_BIT (code, bit) (code |= (1UL << bit)) | 
| #define | SL_RTL_AOX_IQ_SAMPLE_QA_IS_SET (code, bit) (code & (1UL << bit)) | 
| Typedefs | |
| typedef void * | sl_rtl_aox_libitem | 
| Angle of Arrival / Departure library item. | |
| typedef void * | sl_rtl_aox_antenna_pattern | 
| Angle of Arrival / Departure antenna array radiation pattern. | |
Detailed Description
Angle of Arrival / Departure.
These functions are related to the calculation of the Angle of Arrival and Angle of Departure from I/Q samples. The angles can be calculated following these steps:
- Initialize a sl_rtl_aox_libitem instance.
- Set up the antenna array and angle calculation parameters.
- Create the estimator.
- Set the antenna switching pattern.
- Input the I/Q data into the libitem.
- Process the I/Q data into an angle.
Data Structure Documentation
◆ sl_rtl_clib_iq_sample_qa_antenna_data_t
| struct sl_rtl_clib_iq_sample_qa_antenna_data_t | 
◆ sl_rtl_clib_iq_sample_qa_dataset_t
| struct sl_rtl_clib_iq_sample_qa_dataset_t | 
Macro Definition Documentation
◆ SL_RTL_AOX_IQ_SAMPLE_QA_ALL_OK
| #define SL_RTL_AOX_IQ_SAMPLE_QA_ALL_OK 0 | 
◆ SL_RTL_AOX_IQ_SAMPLE_QA_FAILURE
| #define SL_RTL_AOX_IQ_SAMPLE_QA_FAILURE 0xffffffff | 
◆ SL_RTL_AOX_IQ_SAMPLE_QA_CLEAR_BIT
| #define SL_RTL_AOX_IQ_SAMPLE_QA_CLEAR_BIT | ( | 
            code,
            | |
| 
            bit
            | |||
| ) | (code &= ~(1UL << bit)) | 
◆ SL_RTL_AOX_IQ_SAMPLE_QA_SET_BIT
| #define SL_RTL_AOX_IQ_SAMPLE_QA_SET_BIT | ( | 
            code,
            | |
| 
            bit
            | |||
| ) | (code |= (1UL << bit)) | 
◆ SL_RTL_AOX_IQ_SAMPLE_QA_IS_SET
| #define SL_RTL_AOX_IQ_SAMPLE_QA_IS_SET | ( | 
            code,
            | |
| 
            bit
            | |||
| ) | (code & (1UL << bit)) | 
Typedef Documentation
◆ sl_rtl_aox_libitem
| typedef void* sl_rtl_aox_libitem | 
Angle of Arrival / Departure library item.
◆ sl_rtl_aox_antenna_pattern
| typedef void* sl_rtl_aox_antenna_pattern | 
Angle of Arrival / Departure antenna array radiation pattern.
Enumeration Type Documentation
◆ sl_rtl_aox_array_type
AoX antenna array type.
◆ sl_rtl_aox_switch_pattern_array
◆ sl_rtl_aox_switch_pattern_options
◆ sl_rtl_aox_mode
| enum sl_rtl_aox_mode | 
AoA, AoD (and AoX for backward compatibility) estimator modes.
◆ sl_rtl_aox_constraint_type
◆ sl_rtl_aox_switch_pattern_mode
◆ sl_rtl_slib_iq_sample_qa_result_t
Function Documentation
◆ sl_rtl_aox_init()
| enum sl_rtl_error_code sl_rtl_aox_init | ( | sl_rtl_aox_libitem * | 
            item
            | ) | 
Initialize the AoX libitem instance.
- Parameters
- 
         [in] itemPointer to the libitem to be initialized. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_deinit()
| enum sl_rtl_error_code sl_rtl_aox_deinit | ( | sl_rtl_aox_libitem * | 
            item
            | ) | 
Deinitialize a libitem instance of the AoX estimator.
- Parameters
- 
         [in] itemPointer to the libitem to be deinitialized. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_set_num_snapshots()
| enum sl_rtl_error_code sl_rtl_aox_set_num_snapshots | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint32_t | 
            num_snapshots
            | ||
| ) | 
Set the number of signal snapshots to be used in the angle estimation.
- Parameters
- 
         [in] itemPointer to the initialized AoX libitem. [in] num_snapshotsNumber of snapshots as positive integer value. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_set_array_type()
| enum sl_rtl_error_code sl_rtl_aox_set_array_type | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| enum sl_rtl_aox_array_type | 
            array_type
            | ||
| ) | 
Set the array type used with the estimator.
- Parameters
- 
         [in] itemPointer to the initialized AoX libitem. [in] array_typeArray type as sl_rtl_aox_array_type . 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
Set the array type used with the estimator. For example, the array type should be set to SL_RTL_AOX_ARRAY_TYPE_4x4_URA when using the reference 4x4 URA board.
◆ sl_rtl_aox_set_mode()
| enum sl_rtl_error_code sl_rtl_aox_set_mode | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| enum sl_rtl_aox_mode | 
            mode
            | ||
| ) | 
Set the estimation mode.
- Parameters
- 
         [in] itemPointer to the initialized AoX libitem. [in] modeEstimator mode as sl_rtl_aox_mode . 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
Set the estimation mode. For example, ::SL_RTL_AOX_MODE_BASIC sets medium filtering and estimates both azimuth and elevation. For further description of the modes, see the documentation of sl_rtl_aox_mode .
◆ sl_rtl_aox_calculate_iq_sample_phase_rotation()
| enum sl_rtl_error_code sl_rtl_aox_calculate_iq_sample_phase_rotation | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float | 
            iq_data_downsampling_factor,
            | ||
| float * | 
            i_samples,
            | ||
| float * | 
            q_samples,
            | ||
| uint32_t | 
            num_samples,
            | ||
| float * | 
            phase_rotation_out
            | ||
| ) | 
Estimate the I/Q-sample phase rotation error in degrees.
- Parameters
- 
         [in] itemPointer to the initialized AoX libitem. [in] iq_data_downsampling_factorRatio between reference period IQ-data sampling rate. and actual IQ-data (i.e., antenna array data) sampling rate. For example, 1e6 / 500e3 = 2.0 [in] i_samplesFloat-array of the reference period I samples. [in] q_samplesFloat-array of the reference period Q samples. [in] num_samplesNumber of samples, or size of the I or Q sample array. [out] phase_rotation_outReturned phase rotation value as float in degrees. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
Estimate the I/Q-sample phase rotation error caused by switching and CTE frequency error based on I/Q samples from the reference period.
◆ sl_rtl_aox_set_iq_sample_phase_rotation()
| enum sl_rtl_error_code sl_rtl_aox_set_iq_sample_phase_rotation | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float | 
            phase_rotation
            | ||
| ) | 
Set a constant value of I/Q sample phase rotation in degrees.
- Parameters
- 
         [in] itemPointer to the initialized AoX libitem. [in] phase_rotationFloat value of I/Q sample phase rotation in degrees. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
Set a constant value of I/Q sample phase rotation in degrees. The sample rotation can be used to correct the switching and CTE frequency error.
- Note
- : This function should be called only after the estimator is created.
◆ sl_rtl_aox_add_constraint()
| enum sl_rtl_error_code sl_rtl_aox_add_constraint | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| enum sl_rtl_aox_constraint_type | 
            constraint_type,
            | ||
| float | 
            min_value,
            | ||
| float | 
            max_value
            | ||
| ) | 
Add constraints for the estimator. Call before sl_rtl_aox_create_estimator.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] constraint_typeSelect which constraints should be added. [in] min_valueStarting (minimum) value of the range including the min_value. [in] max_valueEnding (maximum) value of the range including the max_value. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
For example, constraint for SL_RTL_AOX_CONSTRAINT_TYPE_AZIMUTH with min_value = 0 and max_value = 90 means that the angular range 0 to 90 degrees is excluded from the estimators internal processing range and angle estimated between that range are not considered as valid results. Setting constraints will help ruling out false multipath-detections when the locator is installed nearby a wall or a RF-reflective surface.
- Note
- : This function must called before the estimator is created.
◆ sl_rtl_aox_set_sample_rate()
| enum sl_rtl_error_code sl_rtl_aox_set_sample_rate | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float | 
            sampleRate
            | ||
| ) | 
Configure the IQ sampling sample rate for the library.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] sampleRateThe new sample rate. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_set_num_radio_channels()
| enum sl_rtl_error_code sl_rtl_aox_set_num_radio_channels | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint32_t | 
            channels
            | ||
| ) | 
Configure the number of radio channels.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] channelsThe new number of radio channels. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_iq_sample_qa_configure()
| enum sl_rtl_error_code sl_rtl_aox_iq_sample_qa_configure | ( | sl_rtl_aox_libitem * | 
            item
            | ) | 
Configure the IQ sample quality analysis.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
This function turns the IQ sample quality analysis, which is not done by default.
◆ sl_rtl_aox_iq_sample_qa_get_results()
| uint32_t sl_rtl_aox_iq_sample_qa_get_results | ( | sl_rtl_aox_libitem * | 
            item
            | ) | 
Get the IQ sample quality analysis overall results.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. 
- Returns
- bitmask of found problems, zero indicates that everything is OK
◆ sl_rtl_aox_iq_sample_qa_get_details()
| enum sl_rtl_error_code sl_rtl_aox_iq_sample_qa_get_details | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| sl_rtl_clib_iq_sample_qa_dataset_t * | 
            results,
            | ||
| sl_rtl_clib_iq_sample_qa_antenna_data_t * | 
            antenna_data
            | ||
| ) | 
Get the IQ sample quality analysis detailed results for the latest packet.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [out] resultsThe data structure with data related to the latest data packet. [out] antenna_dataThe array of antenna-specific results. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
Fetch the results for the latest packet.
◆ sl_rtl_aox_iq_sample_qa_get_channel_details()
| enum sl_rtl_error_code sl_rtl_aox_iq_sample_qa_get_channel_details | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint8_t | 
            channel,
            | ||
| sl_rtl_clib_iq_sample_qa_dataset_t * | 
            results,
            | ||
| sl_rtl_clib_iq_sample_qa_antenna_data_t * | 
            antenna_data
            | ||
| ) | 
Get the IQ sample quality analysis detailed results for the requested radio channel.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] channelRadio channel to show results for. [out] resultsThe data structure with data related to the last data packet using the requested channel. [out] antenna_dataThe array of antenna-specific results 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
Fetch the latest results for the given radio channel, which may be other than the latest packet received.
◆ sl_rtl_aox_create_estimator()
| enum sl_rtl_error_code sl_rtl_aox_create_estimator | ( | sl_rtl_aox_libitem * | 
            item
            | ) | 
Create the estimator after initializing the libitem and setting parameters.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_convert_raw_samples()
| enum sl_rtl_error_code sl_rtl_aox_convert_raw_samples | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint32_t | 
            start_offset,
            | ||
| float | 
            iq_data_downsampling_factor,
            | ||
| float * | 
            raw_i_samples_in,
            | ||
| float * | 
            raw_q_samples_in,
            | ||
| uint32_t | 
            num_raw_samples_in,
            | ||
| float ** | 
            i_samples_out,
            | ||
| float ** | 
            q_samples_out,
            | ||
| uint32_t | 
            num_snapshots_out
            | ||
| ) | 
Convert data in RAW IQ-data buffers to downsampled IQ-data buffers.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] start_offsetThe start offset in the buffer (for example, for skipping a reference period). [in] iq_data_downsampling_factorRatio between chip IQ-data sampling rate and downsampled rate. For example, 4.8e6 / 500e3 = 9.6 [in] raw_i_samples_inI-part sample buffer input [in] raw_q_samples_inQ-part sample buffer input [in] num_raw_samples_inNumber of IQ-sample pairs in the input buffers. [out] i_samples_outBuffer for the processed I-samples. Must be allocated by the user. Indexing: i_samples_out[snapshot][antenna] [out] q_samples_outBuffer for the processed Q-samples. Must be allocated by the user. Indexing: q_samples_out[snapshot][antenna] [in] num_snapshots_outNumber of snaphots allocated in the output buffers. This function checks if the given number of snaphots and calculated snapshots based on the length of RAW-data match 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_calculate_number_of_snapshots()
| enum sl_rtl_error_code sl_rtl_aox_calculate_number_of_snapshots | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint32_t | 
            num_raw_samples_in,
            | ||
| uint32_t | 
            start_offset,
            | ||
| float | 
            iq_data_downsampling_factor,
            | ||
| uint32_t | 
            num_channels,
            | ||
| uint32_t * | 
            num_snapshots_out
            | ||
| ) | 
Calculate the number of downsampled snaphots in a RAW IQ-data buffer. Use this function to get the number of snaphots to allocate the i_samples and q_samples buffers for the process-function.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] num_raw_samples_inTotal number of RAW IQ-sample pairs. [in] start_offsetThe start offset in the buffer, for example, for skipping a reference period. [in] iq_data_downsampling_factorRatio between chip IQ-data sampling rate and downsampled rate. For example, 4.8e6 / 500e3 = 9.6. [in] num_channelsNumber of channels in the RAW data [out] num_snapshots_outCalculated number of snaphots based on the input. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_set_switch_pattern_mode()
| enum sl_rtl_error_code sl_rtl_aox_set_switch_pattern_mode | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| enum sl_rtl_aox_switch_pattern_mode | 
            mode
            | ||
| ) | 
Set switch pattern mode. Sets internal mode used by the library. See enum sl_rtl_aox_switch_pattern_mode for detailed description of the modes. If this function isn't called, a default switch pattern of: 0, 1, 2, 3, ..., N-1 will be used, where N is the number of antennas. Call this function at run-time after initializing and creating the estimator.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] modeRequired mode. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_update_switch_pattern()
| enum sl_rtl_error_code sl_rtl_aox_update_switch_pattern | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint32_t * | 
            switch_pattern_in,
            | ||
| uint32_t ** | 
            switch_pattern_out
            | ||
| ) | 
Update switch pattern, which is used by the estimator algorithm. This function must be called before calling the function sl_rtl_aox_process. Call this function at run-time after initializing and creating the estimator.
When using a custom pattern in SL_RTL_AOX_SWITCH_PATTERN_MODE_EXTERNAL mode, the pattern in switch_pattern_in must not contain duplicate elements and the antenna indices must be within the range 0 to (number_of_antennas - 1). Number_of_antennas is the amount of antennas in the set array type, for example for the 4x4 URA this is 16 and for the 1x4 ULA this is 4. The length of the switching pattern must be equal to number_of_antennas.
Note: The RF switch pattern indices may be different to the indices required by the RTL algorithm. For example, a 1x4 ULA might use RF controls [12, 13, 14, 15] for switching the antennas 1-4, but the RTL algorithm requires the switch pattern [0, 1, 2, 3]. If the RF controls are switched as [14, 15, 13, 12], the RTL algorithm requires the pattern [2, 3, 1, 0].
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] switch_pattern_inPointer to the switch pattern array. The pointer must point to a valid switch pattern when SL_RTL_AOX_SWITCH_PATTERN_MODE_EXTERNAL is used. [out] switch_pattern_outPointer to the user defined uint32_t* variable. This pointer must be non-zero when using internally defined switch pattern modes, otherwise can be zero. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_set_switch_pattern_seed()
| enum sl_rtl_error_code sl_rtl_aox_set_switch_pattern_seed | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| int32_t | 
            seed_value
            | ||
| ) | 
Set the random seed for the switch pattern, which is used for the random pattern mode. Call this function at run-time after initializing and creating the estimator.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] seed_valueThe seed value to be used. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_convert_switch_pattern()
| enum sl_rtl_error_code sl_rtl_aox_convert_switch_pattern | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint32_t | 
            array_id,
            | ||
| uint32_t | 
            options,
            | ||
| uint32_t | 
            switch_pattern_size_in,
            | ||
| uint32_t * | 
            switch_pattern_in,
            | ||
| uint32_t * | 
            switch_pattern_size_out,
            | ||
| uint32_t ** | 
            switch_pattern_out
            | ||
| ) | 
Convert switching pattern from antenna indices to antenna switching pin control logic. Call this function at run-time after initializing and creating the estimator.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] array_idArray ID, see sl_rtl_aox_switch_pattern_array , for example SL_RTL_AOX_SWITCH_PATTERN_ARRAY_4x4_DP [in] optionsSwitch pattern options, see sl_rtl_aox_switch_pattern_options . Can be used to set for example dual polarization (default is single polarization). [in] switch_pattern_size_inThe length of the input switching pattern. [in] switch_pattern_inThe input switching pattern. [out] switch_pattern_size_outThe outputted length of the converted switching pattern. [out] switch_pattern_outThe outputted switching pattern. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_reset_estimator()
| enum sl_rtl_error_code sl_rtl_aox_reset_estimator | ( | sl_rtl_aox_libitem * | 
            item
            | ) | 
Reset estimator state. Calling this function causes the selected aox-mode to start from its initial state. Call this function at run-time after initializing and creating the estimator.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_process()
| enum sl_rtl_error_code sl_rtl_aox_process | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float ** | 
            i_samples,
            | ||
| float ** | 
            q_samples,
            | ||
| float | 
            tone_frequency,
            | ||
| float * | 
            az_out,
            | ||
| float * | 
            el_out
            | ||
| ) | 
Calculate the angle estimate.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] i_samplesTwo-dimensional float-array of captured I samples as i_samples[snapshot][antenna]. [in] q_samplesTwo-dimensional float-array of captured Q samples as q_samples[snapshot][antenna], corresponding to the I samples array. [in] tone_frequencyThe frequency of the signal from which the I/Q data was captured from as float (e.g., 2.46e9f). [out] az_outOutput azimuth angle. [out] el_outOutput elevation angle. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful and SL_RTL_ERROR_ESTIMATION_IN_PROGRESS if estimate is not yet final and more I/Q data needs to be processed.
Calculate the angle estimate from the given I/Q samples captured at the given frequency. Call this function with new I/Q data as many times as indicated by the sl_rtl_aox_mode used by the estimator before the final estimate is output.
◆ sl_rtl_aox_get_latest_aox_standard_deviation()
| enum sl_rtl_error_code sl_rtl_aox_get_latest_aox_standard_deviation | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float * | 
            az_std_dev,
            | ||
| float * | 
            el_std_dev
            | ||
| ) | 
Get the standard deviation for the latest AoA/AoD-estimate.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [out] az_std_devPointer for getting standard deviation of the latest azimuth estimate. [out] el_std_devPointer for getting standard deviation of the latest elevation estimate. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
Call this function after sl_rtl_aox_process to fetch standard deviation for the latest AoA/AoD-estimate. Positive standard deviations indicate line-of-sight detection and negative values indicate likely non-line-of-sight detection.
◆ sl_rtl_aox_get_latest_aoa_standard_deviation()
| 
 | inline static | 
Kept for backward compatibility
◆ sl_rtl_aox_get_latest_aod_standard_deviation()
| 
 | inline static | 
Kept for backward compatibility
◆ sl_rtl_aox_set_expected_direction()
| enum sl_rtl_error_code sl_rtl_aox_set_expected_direction | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float | 
            expected_az,
            | ||
| float | 
            expected_el
            | ||
| ) | 
Feed the expected angles back to the locator.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] expected_azExpected azimuth angle calculated by position algorithm. [in] expected_elExpected elevation angle calculated by position algorithm. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
The position algorithm has a more complete view of the asset's location. The direction it should be found can be calculated back and fed to the locator, so that it can recover faster when, for example, it has locked to a reflection rather than to the line of sight signal. See also sl_rtl_loc_get_expected_direction() .
◆ sl_rtl_aox_set_expected_deviation()
| enum sl_rtl_error_code sl_rtl_aox_set_expected_deviation | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float | 
            deviation_az,
            | ||
| float | 
            deviation_el
            | ||
| ) | 
Feed the expected angle deviations back to the locator.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. [in] deviation_azDeviation of the expected azimuth angle calculated by position algorithm. [in] deviation_elDeviation of the expected elevation angle calculated by position algorithm. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
Report expected deviations calculated by the position algorithm back to the locator so that angles are calculated more accurately taking in account the correctness of the expected directions. If sl_rtl_aox_set_expected_direction() is called but this function is not called, the algorithm will use default values for the expected deviations. See also sl_rtl_loc_get_expected_deviation() and sl_rtl_aox_set_expected_direction() .
◆ sl_rtl_aox_clear_expected_direction()
| enum sl_rtl_error_code sl_rtl_aox_clear_expected_direction | ( | sl_rtl_aox_libitem * | 
            item
            | ) | 
Clear the expected directions and deviations from the locator.
- Parameters
- 
         [in] itemPointer to the initialized and configured AoX libitem. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
See also sl_rtl_aox_set_expected_direction() and sl_rtl_aox_set_expected_deviation() .
◆ sl_rtl_aox_enable_spectrum()
| enum sl_rtl_error_code sl_rtl_aox_enable_spectrum | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| bool | 
            enable
            | ||
| ) | 
Enable or disable outputting the pseudospectrum. This function should be called before creating the estimator.
- Parameters
- 
         [in] itemPointer to the initialized libitem. [in] enableSet to true to enable outputting the pseudospectrum. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_get_spectrum_size()
| enum sl_rtl_error_code sl_rtl_aox_get_spectrum_size | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint32_t * | 
            rows,
            | ||
| uint32_t * | 
            cols
            | ||
| ) | 
Get the size of the pseudospectrum. This function should be called after calling the AoX process function.
- Parameters
- 
         [in] itemPointer to the initialized libitem. [out] rowsNumber of rows in the pseudospectrum data array. [out] colsNumber of columns in the pseudospecutrm data array. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_get_polarization_spectrum_size()
| enum sl_rtl_error_code sl_rtl_aox_get_polarization_spectrum_size | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| uint32_t * | 
            rows,
            | ||
| uint32_t * | 
            cols
            | ||
| ) | 
Get the size of the polarization pseudospectrum. This function should be called after calling the AoX process function.
- Parameters
- 
         [in] itemPointer to the initialized libitem. [out] rowsNumber of rows in the polarization pseudospectrum data array. [out] colsNumber of columns in the pseudospecutrm data array. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_get_spectrum()
| enum sl_rtl_error_code sl_rtl_aox_get_spectrum | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float ** | 
            spectrum_out
            | ||
| ) | 
Get the pseudospectrum. Memory for the output spectrum must be allocated by the user, the size of the rows and columns are given by sl_rtl_aox_get_spectrum_size() .
- Parameters
- 
         [in] itemPointer to the initialized libitem. [out] spectrum_outOutputted pseudospectrum. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_get_polarization_spectrum()
| enum sl_rtl_error_code sl_rtl_aox_get_polarization_spectrum | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| float ** | 
            spectrum_out
            | ||
| ) | 
Get the polarization spectrum. Memory for the output spectrum must be allocated by the user, the size of the rows and columns are given by sl_rtl_aox_get_polarization_spectrum_size() .
- Parameters
- 
         [in] itemPointer to the initialized libitem. [out] spectrum_outOutputted polarization pseudospectrum. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_antenna_pattern_init()
| enum sl_rtl_error_code sl_rtl_aox_antenna_pattern_init | ( | sl_rtl_aox_antenna_pattern * | 
            pattern,
            | 
| enum sl_rtl_aox_array_type | 
            array_type
            | ||
| ) | 
Initialize the antenna radiation pattern item for the given array board. The antenna pattern item can be shared by multiple different estimators.
- Parameters
- 
         [in] patternPointer to the pattern item to initialize. [in] array_typeArray type of the board for which the pattern is loaded. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_set_antenna_pattern()
| enum sl_rtl_error_code sl_rtl_aox_set_antenna_pattern | ( | sl_rtl_aox_libitem * | 
            item,
            | 
| sl_rtl_aox_antenna_pattern * | 
            pattern
            | ||
| ) | 
Set the given estimator to use the given antenna radiation pattern in the model. The same antenna pattern can be shared between multiple estimators. The antenna pattern can be cleared for an estimator by setting it to NULL. The estimator will then use the default model.
- Note
- : This function should be called only after the estimator is created.
- Parameters
- 
         [in] itemPointer to the initialized libitem. [in] patternPointer to the initialized antenna pattern item. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful
◆ sl_rtl_aox_antenna_pattern_deinit()
| enum sl_rtl_error_code sl_rtl_aox_antenna_pattern_deinit | ( | sl_rtl_aox_antenna_pattern * | 
            pattern
            | ) | 
Deinitialize the antenna radiation pattern item.
- Parameters
- 
         [in] patternPointer to the initialized pattern item. 
- Returns
- SL_RTL_ERROR_SUCCESS if successful