Error Codes#
RTL library Error Codes.
Enumerations#
enum
SL_RTL_ERROR_SUCCESS = 0
SL_RTL_ERROR_ARGUMENT 
SL_RTL_ERROR_OUT_OF_MEMORY 
SL_RTL_ERROR_ESTIMATION_IN_PROGRESS 
SL_RTL_ERROR_NUMBER_OF_SNAPHOTS_DO_NOT_MATCH 
SL_RTL_ERROR_ESTIMATOR_NOT_CREATED 
SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED 
SL_RTL_ERROR_NOT_INITIALIZED 
SL_RTL_ERROR_INTERNAL 
SL_RTL_ERROR_IQ_SAMPLE_QA 
SL_RTL_ERROR_FEATURE_NOT_SUPPORTED 
SL_RTL_ERROR_INCORRECT_MEASUREMENT 
SL_RTL_ERROR_LAST 
}
RTL error code.
Enumeration Documentation#
sl_rtl_error_code#
sl_rtl_error_code
RTL error code.
| Enumerator | |
|---|---|
| SL_RTL_ERROR_SUCCESS | Successful execution / estimation complete.  | 
| SL_RTL_ERROR_ARGUMENT | Invalid argument.  | 
| SL_RTL_ERROR_OUT_OF_MEMORY | Memory / allocation failure.  | 
| SL_RTL_ERROR_ESTIMATION_IN_PROGRESS | Estimation not yet finished.  | 
| SL_RTL_ERROR_NUMBER_OF_SNAPHOTS_DO_NOT_MATCH | Initialized and calculated number of snapshots do not match.  | 
| SL_RTL_ERROR_ESTIMATOR_NOT_CREATED | Estimator not yet created.  | 
| SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED | Estimator already created, operation is not supported.  | 
| SL_RTL_ERROR_NOT_INITIALIZED | Library item not yet initialized.  | 
| SL_RTL_ERROR_INTERNAL | An internal error occurred.  | 
| SL_RTL_ERROR_IQ_SAMPLE_QA | IQ sample quality analysis failed.  | 
| SL_RTL_ERROR_FEATURE_NOT_SUPPORTED | The requested feature is not supported by the library.  | 
| SL_RTL_ERROR_INCORRECT_MEASUREMENT | The error of the last measurement for this locator was too large.  | 
| SL_RTL_ERROR_LAST | Number of error codes.  |