Public Attributes#
Number of frequencies, 0xFFFFFFFF or 0 if invalid. In case of invalid input, the previously estimated distance shall be returned.
Array of RSSI values from device 1, enter INVALID_RSSI_VALUE for any unavailable RSSI measurement.
Array of RSSI values from device 2, enter INVALID_RSSI_VALUE for any unavailable RSSI measurement.
Array of time measurements from device 1, enter INVALID_TIME_VALUE for any unavailable time measurement.
Array of time measurements from device 2, enter INVALID_TIME_VALUE for any unavailable time measurement.
Public Attribute Documentation#
num_time_stamps#
uint32_t sl_rtl_abr_rtt_data::num_time_stamps
Number of frequencies, 0xFFFFFFFF or 0 if invalid. In case of invalid input, the previously estimated distance shall be returned.
749
of file /mnt/raid/workspaces/ws.SJgwRTPM2/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h
rssi_d1#
int32_t* sl_rtl_abr_rtt_data::rssi_d1
Array of RSSI values from device 1, enter INVALID_RSSI_VALUE for any unavailable RSSI measurement.
750
of file /mnt/raid/workspaces/ws.SJgwRTPM2/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h
rssi_d2#
int32_t* sl_rtl_abr_rtt_data::rssi_d2
Array of RSSI values from device 2, enter INVALID_RSSI_VALUE for any unavailable RSSI measurement.
751
of file /mnt/raid/workspaces/ws.SJgwRTPM2/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h
time_d1#
int32_t* sl_rtl_abr_rtt_data::time_d1
Array of time measurements from device 1, enter INVALID_TIME_VALUE for any unavailable time measurement.
752
of file /mnt/raid/workspaces/ws.SJgwRTPM2/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h
time_d2#
int32_t* sl_rtl_abr_rtt_data::time_d2
Array of time measurements from device 2, enter INVALID_TIME_VALUE for any unavailable time measurement.
753
of file /mnt/raid/workspaces/ws.SJgwRTPM2/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h