Error Codes#
RTL library Error Codes.
Enumerations#
enum
SL_RTL_ERROR_SUCCESS = 0
SL_RTL_ERROR_ARGUMENT
SL_RTL_ERROR_OUT_OF_MEMORY
SL_RTL_ERROR_ESTIMATION_IN_PROGRESS
SL_RTL_ERROR_NUMBER_OF_SNAPHOTS_DO_NOT_MATCH
SL_RTL_ERROR_ESTIMATOR_NOT_CREATED
SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED
SL_RTL_ERROR_NOT_INITIALIZED
SL_RTL_ERROR_INTERNAL
SL_RTL_ERROR_IQ_SAMPLE_QA
SL_RTL_ERROR_FEATURE_NOT_SUPPORTED
SL_RTL_ERROR_INCORRECT_MEASUREMENT
SL_RTL_ERROR_LAST
}
RTL error code.
Enumeration Documentation#
sl_rtl_error_code#
sl_rtl_error_code
RTL error code.
Enumerator | |
---|---|
SL_RTL_ERROR_SUCCESS | Successful execution / estimation complete. |
SL_RTL_ERROR_ARGUMENT | Invalid argument. |
SL_RTL_ERROR_OUT_OF_MEMORY | Memory / allocation failure. |
SL_RTL_ERROR_ESTIMATION_IN_PROGRESS | Estimation not yet finished. |
SL_RTL_ERROR_NUMBER_OF_SNAPHOTS_DO_NOT_MATCH | Initialized and calculated number of snapshots do not match. |
SL_RTL_ERROR_ESTIMATOR_NOT_CREATED | Estimator not yet created. |
SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED | Estimator already created, operation is not supported. |
SL_RTL_ERROR_NOT_INITIALIZED | Library item not yet initialized. |
SL_RTL_ERROR_INTERNAL | An internal error occurred. |
SL_RTL_ERROR_IQ_SAMPLE_QA | IQ sample quality analysis failed. |
SL_RTL_ERROR_FEATURE_NOT_SUPPORTED | The requested feature is not supported by the library. |
SL_RTL_ERROR_INCORRECT_MEASUREMENT | The error of the last measurement for this locator was too large. |
SL_RTL_ERROR_LAST | Number of error codes. |
Definition at line
59
of file /mnt/raid/workspaces/ws.FLBdB2bOZ/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h