Utility Functionality#

Utility Functionality.

These functions provide supporting functionality such as conversions, additional filtering, diagnostics, and setup functions.

Enumerations#

enum
SL_RTL_UTIL_PARAMETER_AMOUNT_OF_FILTERING = 0
}

Util parameter.

Typedefs#

typedef void *

Utility library item.

Functions#

sl_rtl_util_init(sl_rtl_util_libitem *item)
sl_rtl_util_deinit(sl_rtl_util_libitem *item)
sl_rtl_util_set_parameter(sl_rtl_util_libitem *item, enum sl_rtl_util_parameter parameter, float value)
sl_rtl_util_filter(sl_rtl_util_libitem *item, float value_in, float *value_out)
sl_rtl_util_rssi2distance(float tx_power, float rssi, float *distance_out)
sl_rtl_util_iq_sample_qa_setup(sl_rtl_util_libitem *item, uint32_t level, uint32_t num_antennas, bool raw_samples)
sl_rtl_util_iq_sample_qa_set_parameters(sl_rtl_util_libitem *item, uint32_t sample_rate, uint8_t sample_offset, uint8_t samples_in_slot, uint8_t number_of_channels)
sl_rtl_util_iq_sample_qa_set_data_offset(sl_rtl_util_libitem *item, uint32_t offset)
sl_rtl_util_iq_sample_qa_set_switch_pattern(sl_rtl_util_libitem *item, uint32_t size, uint32_t *pattern)
sl_rtl_util_iq_sample_qa_add_reference(sl_rtl_util_libitem *item, uint32_t num_samples, float *i_samples, float *q_samples)
sl_rtl_util_iq_sample_qa_add_data(sl_rtl_util_libitem *item, uint32_t num_snapshots, float **i_samples, float **q_samples, uint8_t channel)
uint32_t
sl_rtl_util_iq_sample_qa_get_results(sl_rtl_util_libitem *item)
sl_rtl_util_iq_sample_qa_get_details(sl_rtl_util_libitem *item, sl_rtl_clib_iq_sample_qa_dataset_t *iq_sample_qa_results, sl_rtl_clib_iq_sample_qa_antenna_data_t *antenna_data)
sl_rtl_util_iq_sample_qa_get_channel_details(sl_rtl_util_libitem *item, uint8_t channel, sl_rtl_clib_iq_sample_qa_dataset_t *iq_sample_qa_results, sl_rtl_clib_iq_sample_qa_antenna_data_t *antenna_data)
char *
sl_rtl_util_iq_sample_qa_code2string(char *buf, int size, uint32_t code)

Enumeration Documentation#

sl_rtl_util_parameter#

sl_rtl_util_parameter

Util parameter.

Enumerator
SL_RTL_UTIL_PARAMETER_AMOUNT_OF_FILTERING

Amount of filtering in range [0.0f, 1.0f].


Definition at line 1522 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

Typedef Documentation#

sl_rtl_util_libitem#

typedef void* sl_rtl_util_libitem

Utility library item.


Definition at line 1519 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

Function Documentation#

sl_rtl_util_init#

enum sl_rtl_error_code sl_rtl_util_init (sl_rtl_util_libitem * item)
Parameters
[in]item

Pointer to the libitem to be initialized

Initialize the Util libitem instance.

Returns


Definition at line 1532 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_deinit#

enum sl_rtl_error_code sl_rtl_util_deinit (sl_rtl_util_libitem * item)
Parameters
[in]item

Pointer to the libitem to be deinitialized

Deinitialize a Util libitem instance.

Returns


Definition at line 1540 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_set_parameter#

enum sl_rtl_error_code sl_rtl_util_set_parameter (sl_rtl_util_libitem * item, enum sl_rtl_util_parameter parameter, float value)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]parameter

Parameter to change

[in]value

Value of the parameter

Set util parameters.

Returns


Definition at line 1550 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_filter#

enum sl_rtl_error_code sl_rtl_util_filter (sl_rtl_util_libitem * item, float value_in, float * value_out)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]value_in

Value to be fed to the filter

[out]value_out

Pointer to the filtered value

Filter a value using the moving average.

Returns


Definition at line 1560 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_rssi2distance#

enum sl_rtl_error_code sl_rtl_util_rssi2distance (float tx_power, float rssi, float * distance_out)
Parameters
[in]tx_power

Reference RSSI value of the TX-device at 1.0 m distance in dBm, for example -45.0f

[in]rssi

Measured RSSI from the receiver

[out]distance_out

Distance in meters

Convert an RSSI-value to distance in meters.

Returns


Definition at line 1570 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_setup#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_setup (sl_rtl_util_libitem * item, uint32_t level, uint32_t num_antennas, bool raw_samples)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]level

Analysis level

[in]num_antennas

The number of antennas in the array

[in]raw_samples

Data contains raw samples instead of picked ones

Set up the IQ sample quality analysis.

Returns


Definition at line 1581 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_set_parameters#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_set_parameters (sl_rtl_util_libitem * item, uint32_t sample_rate, uint8_t sample_offset, uint8_t samples_in_slot, uint8_t number_of_channels)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]sample_rate

The sampling rate

[in]sample_offset

The offset for the picked sample in the sampling slot

[in]samples_in_slot

Number of samples in the sampling slot

[in]number_of_channels

Number of radio channels

Set up parameters for the IQ sample quality analysis.

Returns


Definition at line 1593 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_set_downsampling_factor#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_set_downsampling_factor (sl_rtl_util_libitem * item, float dsf)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]dsf

The downsampling factor

Set up IQ sample QA downsampling ratio.

Set the downsampling factor used during the antenna samples (related to the sampling rate of the reference period)

Returns


Definition at line 1605 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_set_data_offset#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_set_data_offset (sl_rtl_util_libitem * item, uint32_t offset)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]offset

The data samples' offset

Set data samples offset.

Set the offset for the data samples from the start of the reference period. The use of this function is optional and, if not given, the default values are used.

Returns


Definition at line 1618 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_set_switch_pattern#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_set_switch_pattern (sl_rtl_util_libitem * item, uint32_t size, uint32_t * pattern)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]size

The size of the switch pattern

[in]pattern

Array of integers representing the switch pattern

Set the switch pattern for the IQ sample quality.

Returns


Definition at line 1628 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_add_reference#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_add_reference (sl_rtl_util_libitem * item, uint32_t num_samples, float * i_samples, float * q_samples)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]num_samples

The size of data

[in]i_samples

I-part of the sample data

[in]q_samples

Q-part of the sample data

Feed the IQ sample quality analysis the reference period data.

Returns


Definition at line 1639 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_add_data#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_add_data (sl_rtl_util_libitem * item, uint32_t num_snapshots, float ** i_samples, float ** q_samples, uint8_t channel)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]num_snapshots

The size of the data

[in]i_samples

I-part of the sample data

[in]q_samples

Q-part of the sample data

[in]channel

Radio channel the packet is using.

Feed the IQ sample quality analysis the antenna data.

Returns


Definition at line 1650 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_get_results#

uint32_t sl_rtl_util_iq_sample_qa_get_results (sl_rtl_util_libitem * item)
Parameters
[in]item

Pointer to the initialized Util libitem

Get the overall results of the IQ sample quality analysis.

Returns

  • Bitmask of the failing tests, zero if everything passed


Definition at line 1659 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_get_details#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_get_details (sl_rtl_util_libitem * item, sl_rtl_clib_iq_sample_qa_dataset_t * iq_sample_qa_results, sl_rtl_clib_iq_sample_qa_antenna_data_t * antenna_data)
Parameters
[in]item

Pointer to the initialized Util libitem

[out]iq_sample_qa_results

The data structure with data related to the previous data packet

[out]antenna_data

The array of antenna-specific results

Get the detailed results of the IQ sample quality analysis.

Returns


Definition at line 1669 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_get_channel_details#

enum sl_rtl_error_code sl_rtl_util_iq_sample_qa_get_channel_details (sl_rtl_util_libitem * item, uint8_t channel, sl_rtl_clib_iq_sample_qa_dataset_t * iq_sample_qa_results, sl_rtl_clib_iq_sample_qa_antenna_data_t * antenna_data)
Parameters
[in]item

Pointer to the initialized Util libitem

[in]channel

Radio channel to show results for.

[out]iq_sample_qa_results

The data structure with data related to the last data packet using the requested channel

[out]antenna_data

The array of antenna specific results

Get the detailed results of the IQ sample quality analysis for the specified radio channel.

Returns


Definition at line 1680 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h

sl_rtl_util_iq_sample_qa_code2string#

char * sl_rtl_util_iq_sample_qa_code2string (char * buf, int size, uint32_t code)
Parameters
[in]buf

Buffer for the results to be written

[in]size

Size of the buffer

[in]code

The results previously received from the sl_rtl_util_iq_sample_qa_get_results()

Write the IQ sample quality analysis code as human readable strings in the provided buffer.

Returns

  • pointer to the buffer containing data, or to a constant string


Definition at line 1690 of file /mnt/raid/workspaces/ws.HsAs8Mhm7/overlay/gsdk/util/silicon_labs/aox/inc/sl_rtl_clib_api.h