Logging#
Logging.
RTL events are logged as follows:
Initialize the logging.
Configure the logging with the configuration parameters.
Configuration is only allowed once in a logging session.
Enable logging for the RTL libitem(s).
The libitem(s) can be added before or after the estimator(s) are created.
Disable logging for the RTL libitem(s) to stop the logging for the given RTL libitem.
Deinitialize logging. This will disable logging for all the remaining RTL libitems.
Typedefs#
typedef void(*
sl_rtl_log_callback_function)(uint8_t *log_data, size_t log_data_len)
Functions#
typedef(struct { sl_rtl_log_callback_function log_callback_function;char sdk_version[SL_RTL_LOG_SDK_VERSION_CHAR_ARRAY_MAX_SIZE];char command_line_options[SL_RTL_LOG_COMMAND_LINE_OPTIONS_CHAR_ARRAY_MAX_SIZE];}) sl_rtl_log_params
enum sl_rtl_error_code
sl_rtl_log_init(void)
enum sl_rtl_error_code
sl_rtl_log_configure(const sl_rtl_log_params *log_params)
enum sl_rtl_error_code
sl_rtl_log_deinit(void)
Macros#
Typedef Documentation#
sl_rtl_log_callback_function#
typedef void(* sl_rtl_log_callback_function) (uint8_t *log_data, size_t log_data_len) )(uint8_t *log_data, size_t log_data_len)
Function Documentation#
typedef#
typedef (struct { sl_rtl_log_callback_function log_callback_function;char sdk_version[SL_RTL_LOG_SDK_VERSION_CHAR_ARRAY_MAX_SIZE];char command_line_options[SL_RTL_LOG_COMMAND_LINE_OPTIONS_CHAR_ARRAY_MAX_SIZE];} )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| struct { sl_rtl_log_callback_function log_callback_function;char sdk_version[SL_RTL_LOG_SDK_VERSION_CHAR_ARRAY_MAX_SIZE];char command_line_options[SL_RTL_LOG_COMMAND_LINE_OPTIONS_CHAR_ARRAY_MAX_SIZE];} | N/A |
sl_rtl_log_init#
enum sl_rtl_error_code sl_rtl_log_init (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initiate the RTL logging.
sl_rtl_log_configure#
enum sl_rtl_error_code sl_rtl_log_configure (const sl_rtl_log_params * log_params)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_rtl_log_params * | [in] | log_params | Pointer to the sl_rtl_log_params |
Register the configuration parameters for the logging.
Returns
SL_RTL_ERROR_SUCCESS if successful
sl_rtl_log_deinit#
enum sl_rtl_error_code sl_rtl_log_deinit (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Deinitiate the RTL logging.