Local Host Configuration#

This document will go over the hardware and software pre-requisites for building and running a multiprotocol solution locally. Note that this section will be using Raspberry Pi + Raspian OS, however, this is not necessarily required and you can build and run the multiprotocol solution on similar ARM host platforms.

Hardware#

  • Raspberry Pi 4

  • SD Card 32GB+

  • EFR32 Radio Board (For example BRD4180B)

  • Either: WSTK / WPK (BRD4001 / BRD4002)

  • PC with Simplicity Studio

Note: For SPI configuration, you can use a Pi Hat Expansion Header BRD8016A in replacement for a WSTK/WPK.

Software#

  • Linux host OS: The following sections use raspberry Pi OS Lite using Debian Bookworm Version 12

  • Silicon Labs SDK

For GSDK 4.4.0 and up (Including SiSDK) you can use raspberry Pi OS Lite using Debian Version 12 (Bookworm), which uses GCC v12.2.

Note: Zigbee Specific: Refer to Building Zigbeed & Z3Gateway to find supported Zigbeed platforms.

Install Required Prerequisite Packages#

sudo apt-get update && sudo apt-get upgrade -y
sudo apt-get install cmake git libreadline-dev libmbedtls-dev socat
sudo apt-get install bluetooth bluez bluez-tools rfkill libbluetooth-dev

Some versions of operating systems for the Raspberry Pi have enabled a swapfile. This file creates a lot of unnecessary wear on the SD card and causes performance to degrade drastically over time. It is recommended to disable this with the following commands:

sudo dphys-swapfile swapoff
sudo dphys-swapfile uninstall
sudo apt remove dphys-swapfile 

SPI Configuration#

This section is intended only for users running the co-processor with SPI, UART co-processor configurations can skip this section.

Configuring RasperryPi OS to run the SPI Driver#

  1. Open /boot/config.txt and add the following configuration:

    # Enable SPI0 with 1 chip select
    [all]
    dtoverlay=spi0-1cs
    
    # If the CS pin number must be changed, use and adapt this line **instead**:
    dtoverlay=spi0-1cs,cs0_pin=8
    
    # If you need two CS pins, use and adapt this line instead:
    dtoverlay=spi0-2cs,cs0_pin=8,cs1_pin=7 
  2. Reboot for changes to take effect.

    sudo reboot
  3. Validate that your changes are successful, by running:

    ls /dev | grep spi

success will yield the following output:

```bash
spidev0.0
```
  1. To make sure the chip select GPIOs are proper, run: dtc -I fs /sys/firmware/devicetree/base and make sure you can find the following configuration:

    spi0_cs_pins{    
        brcm,function = <0x01>;    
        phandle = <0x0f>;
        brcm,pins = <0x08>;
    };

In this configuration the CS pin is connected to GPIO 8 so this is the correct and expected pin configuration of the RasperryPi host.

SPI Pin mapping of Raspberry Pi to Co-Processor#

The following pinout diagram shows the GPIO mappings for a RaspberryPi 4:

Raspberry Pi 4 Pin MappingRaspberry Pi 4 Pin Mapping

The following table provides the pin mapping required between the RaspberryPi 4 GPIO, the WSTK Pin out, and the cpcd.conf file:

Pin Name

Pin Tool Mapping

Radio Board Pin

EXP Header Pin

Raspi Config

IRQ

PB00

P4

EXP7

GPIO22 (Pin 15)

Bootloader Wake

PB01

P6

EXP9

GPIO24 (Pin 18)

MOSI

PC00

P1

EXP4

GPIO10 (Pin 19)

MISO

PC01

P3

EXP6

GPIO9 (Pin 21)

CLK

PC02

P5

EXP8

GPIO11 (Pin 23)

CS

PC03

P7

EXP10

GPIO8 (Pin 24)

Reset

EFR32_Reset

F4

NA

GPIO23 (Pin 16)

GND

-

-

EXP1

Ground (Pin 20)

Using the WPK: The SPI signals can be manually wired from the WPK EXP pins to the RaspberryPi GPIO. Please note that these signals listed above are using the default cpcd.conf file configuration. If you are using different GPIO pins you will need to modify the various pin configurations in the cpcd.conf file using your text editor of choice. Specifically the MOSI, MISO, CLK, CS, GND pins are all defined by the SPI driver your RaspberryPi is utilizing.

Using the BRD8016A Wireless Expansion board: you will need to mount the expansion board on the RaspberryPi and make sure that the expansion board switch is set to the high power mode. By default, the SPI configuration on the co-processor and CPCD should match this configuration.