Simplicity AI SDK Beta1 (Sept 2026) Release Notes#
Welcome to the first public Beta release of the Simplicity AI SDK, which provides AI-assisted access to supported Silicon Labs development workflows.
Release Summary#
Key Features#
Added in Beta1#
Enables natural-language Bluetooth LE application development, including application creation and configuration, code generation, project builds, firmware flashing on supported hardware, and iterative development.
Provides Simplicity SDK-grounded guidance using Silicon Labs documentation, APIs, examples, and project metadata to deliver contextual, version-specific responses.
Enables AI assistants to use Silicon Labs configuration and hardware tools for project configuration, GATT profile creation and validation, board discovery, device programming, and firmware flashing.
Introduces AI-guided debugging workflows for investigating build failures and device behavior, including log interpretation, GDB-based inspection, fault analysis, and suggested corrective actions.
Enables AI assistants to work with Silicon Labs analysis tools, including Advanced Energy Monitoring (AEM), Network Intelligence, and Channel Sounding Analyzer.
Provides initial support for GitHub Copilot and Codex IDE agents through Visual Studio Code, and for Cursor.
Bug Fixes#
Fixed in Beta1#
None
All bug fixes are listed in the table below.
Chip Enablement#
None
Removed and Deprecated Features#
None
Known Issues and Limitation#
UID | Issue | Workaround |
|---|---|---|
None | Wireless Protocol Support: This release supports Bluetooth LE development workflows only. Other wireless protocols and their associated SDK and tools are not fully supported. | - |
None | Network Intelligence Support: On Windows OS, the Network Intelligence workflow does not install Wireshark automatically. | Manually install Wireshark before using the Network Intelligence workflow on Windows. |
None | Codex Authentication with mcp.silabs.com: Codex refreshes MCP credentials while the refresh token is valid. After the refresh token expires and the server returns a standard | Log out and sign in again. Alternatively, run: |
Fixed Issues#
Fixed in Beta1#
UID | Description |
|---|---|
- | None |