Simplicity Commander Commands#

This section includes the following information for using each Simplicity Commander command:

  • Command Line Syntax

  • Command Line Input Example

  • Command Line Output Example

In cases where the Command Line Syntax is the same as the Command Line Input Example, only the former is included.

The Simplicity Commander commands are organized in the following categories: