Device Lock and Protection Commands#
Debug Lock#
Locks access to the debug interface of the device. This feature is only supported on EFM32 and EFR32 devices. The --debug enable option is no longer required as of Simplicity Commander version 1.8.
Command Line Syntax
$ commander device lock [--debug enable]Command Line Usage Output
Locking debug access...
DONEDebug Unlock#
Unlocks access to the debug interface of the device. This triggers a mass erase if the device was locked before.
This feature is only supported on EFM32 and EFR32 devices.
Command Line Syntax
$ commander device lock --debug disableCommand Line Usage Output
ERROR: Could not get MCU information
Removing all locks/protection...
Unlocking debug access (triggers a mass erase)...
DONEIn Simplicity Commander version 1.8, an alternative command syntax was introduced.
Command Line Syntax
$ commander device unlockCommand Line Usage Output
Unlocking debug access (triggers a mass erase)...
Chip successfully unlocked.
DONEWrite Protect Flash Ranges#
Protects all flash pages affected by the given memory range from any writes or erases. The available granularity of flash write protection is device-dependent. Consult the device reference manual for details. For EFM32 and EFR32 devices, for example, the write protect feature operates on flash pages. On EM3xx devices, this works on 8 kB or 16 kB blocks.
For all devices, if the given range doesn't match the block size supported by the device, it will be extended to always protect entire regions.
Command Line Syntax
$ commander device protect ‑‑write --range <startaddress>:<endaddress>Command Line Input Example
$ commander device protect --write --range 0x0:0x4000Protects all flash pages in the first 16 kB from being erased or written to. Useful for protecting a bootloader from being modified by buggy application code, for example.
Command Line Output Example
Write protecting range 0x00000000 - 0x00004000
DONEWrite Protect Flash Region#
Protects all flash pages in the named region from being written to or erased.
Command Line Syntax
$ commander device protect ‑‑write --region @<region>Command Line Input Example
$ commander device protect --write --region @mainflashProtects the entire main flash from being written to or erased.
Command Line Output Example
Write-protecting all pages in main flash.
DONEDisable Write Protection#
Disables write protection for all pages.
Command Line Syntax
$ commander device protect ‑‑write --disableCommand Line Output Example
Disabling all write protection...
DONE