Install SLT#

You can install SLT by following the steps in Install and Configure Packages.

SLT supports online help: slt --help or slt -h or slt COMMAND --help.

SLT Locations#

SLT is downloaded as a zip file that contains the slt executable (slt.exe on Windows and just slt on MacOS or Linux). Extract the executable to any location you want. Silicon Labs recommends using a folder on your environment search path or else adding the folder to the environment search path.

After you run slt, the path to the slt executable is stored in the user’s .silabs/slt/slt.location file. Other Silicon Labs tools use this file, and it is also helpful when multiple copies of slt are installed.