Install SLC-CLI#

To install SLC-CLI with SLT-CLI, see [Install and Configure Packages].

Other Tools#

SLC-CLI provides a number of options for generating project files. The compiler toolchain needed to build an application image with SLC is installed by SLT. See [Install and Configure Packages].

To flash the image to a target device, you need Simplicity Commander. Simplicity Commander lets you complete these essential tasks:

  • Flash an application.

  • Configure the application image.

  • Manage the target device.

Simplicity Commander is installed with SLT and is one of the recommended packages, but you can also download an Operating System-specific Simplicity Commander zip file here: https://www.silabs.com/developers/mcu-programming-options.

For instructions on using Simplicity Commander, see the Simplicity Commander Reference Guide.