Import and Export#
Simplicity Studio® 5 (SSv5) File > Import and File > Export options allow you to import a project from Keil® µVision4®, IAR Embedded Workbench, or the 8-bit Silicon Labs IDE into Simplicity IDE, and to export a project in a variety of formats.
Import#
Select File > Import, and locate the folder with the project to be imported.
![simp ide import](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-import.png)
![simp ide import](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-import.png)
Select the project and click Next. If anything about the project is unresolved you can resolve it.
![simp ide import unresolved](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-import-unresolved.png)
![simp ide import unresolved](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-import-unresolved.png)
![simp ide import resolved](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-import-resolved.png)
![simp ide import resolved](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-import-resolved.png)
Click Next. Name the project and click Finish.
Export#
Select File > Export, and select the file(s) to be exported.
![simp ide export](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-export.png)
![simp ide export](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-export.png)
The default export format is an .sls file, which can easily be re-imported into SSv5. However, other options are available. Click More export options... and select a wizard.
![simp ide export options](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-export-options.png)
![simp ide export options](/ss-5-users-guide-about-the-simplicity-ide/0.2/images/simp-ide-export-options.png)