Known Issues#
Simplicity Studio® Version 5.4.0.0#
ID | Issue | Workaround |
|---|---|---|
620727 | When Radio Boards are used that contain both an EFR32 or EFM32 target as well as one of the Energy Friendly EFP parts, the Launcher perspective incorrectly shows the EFP as the target part and so the Preferred SDK is wrong and there are no software examples for the board. | Create a new project through File > Silicon Labs Project Wizard so that the Target, SDK, and Toolchain Selection dialog opens. In the Target Device drop down, select the other target part on the board. If it is not already displayed, select the correct Gecko SDK Suite in the SDK drop down list. from the list. Click Next. Now the correct software examples will be listed for the board. |
639643 | When building projects with the IAR ARM toolchain, local variables are not always displayed correctly in the Simplicity Studio debugger. | Use the GDB debugger. Select Preferences > Simplicity Studio > Debuggers > GNU Debugger (GDB) and click Apply and Close. When a debug session is started it will use GDB. |
702086 | Slower project build times are seen on Windows compared to Linux. | Use an external 64-bit make.exe such as the one available from mingw. Once the make.exe is available, use a text editor on the studio.ini line in the Simplicity Studio installation directory and add a line like this to the end of the file: |
701928 | Most EFR32xG22 and EFM32xG22 peripheral registers are not displayed correctly with the Simplicity Studio debugger. | Use the GDB debugger. Select Preferences > Simplicity Studio > Debuggers > GNU Debugger (GDB) and click Apply and Close. When a debug session is started it will use GDB. |
726091 | Linux: Font for Launch Console and TCP/IP Adapter preferences is sometimes not readable. | No known workaround. A suggestion is to copy the text and paste it into a text editor. The preferences can be edited in the text editor and then pasted back to the preference window. |
735426 | A GNU ARM C++ created project (such as an OpenThread project) may generate build errors similar to this: | Open the Project Configurator (.slcp) file and click Force Generation from the Overview tab. |
758963 | Navigation buttons (back, forward, etc.) do not show on the Simplicity IDE toolbar after restart in the Simplicity IDE perspective. | Change to a different perspective, such as the Launcher perspective, and then change back to the Simplicity IDE perspective. |
773819 | If a project's properties are changed, and then the project is renamed, the Refresh Policy folder name is not updated and every build is treated as a full rebuild. | Right-click the project folder and select Properties >C/C++ Build. Go to the Refresh Policy tab and delete the folder name. Click Add Resource... and add the folder for the renamed project. |