Prerequisites#

To streamline your Simplicity Studio® 5 (SSv5) installation:

SSv5 System Requirements#

Operating Systems

Operating System

Version

Windows

Windows 10 (64-bit), Windows 11

macOS

10.14 Mojave, 10.15 Catalina, 11.x Big Sur, 12.x Monterey

Linux

Ubuntu 20.04 LTS

Hardware

Hardware Component

Item

CPU

1 GHZ or better

Memory

1 GB RAM minimum, 8 GB recommended for Wireless Protocol development

Disk Space

600 MB disk space for minimum FFD installation; 7 GB for Wireless Dynamic Protocol support

Hardware#

A Silicon Labs development kit is not required to get started with Simplicity Studio. However, if Simplicity Studio detects an official development kit, it can be used to help select the appropriate software and tools for installation. If you don't have a development kit, you can explore the available options here.

EFR32 Kits#

If you have a Silicon Labs Wireless Starter Kit (WSTK) or Pro Kit, mount a radio board on the mainboard and connect the mainboard to your PC using the USB cable supplied with the kit.

Note: For best performance in SSv5, be sure that the power switch on the mainboard is in the Advanced Energy Monitoring or “AEM” position.

WSTK mainboard with the power switch in the AEM positionWSTK mainboard with the power switch in the AEM position

Customer Account#

If you do not already have one, create an account on the Silicon Labs Customer Support portal. Be sure to record your account username and password as you will use it to log in through SSv5. Your account properties determine not only what software components you can download, but also what notifications you will receive.

To review or change your notification subscriptions, log in to the portal, click HOME to go to the portal home page and then click the Manage Notifications tile. Make sure that Software/Security Advisory Notices & Product Change Notices (PCNs) is checked, and that you are subscribed at minimum for your platform and protocol. Silicon Labs strongly recommends that you receive these notifications. Click Save to save any changes.