Amazon Sidewalk Version 2.8.0 - Release Notes (Jan 22, 2026)#

Simplicity SDK Version 2025.12.0

Amazon Sidewalk is a secure, low-bandwidth, long-range wireless protocol designed to connect smart devices and extend their range beyond standard Wi-Fi or Bluetooth. It enables seamless connectivity for IoT devices in homes and neighborhoods, supporting features like device tracking, smart lighting, and sensor networks. For information about previous releases, see the release notes archive.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

  • Support for Simplicity SDK 2025.12.0.

  • Support for RAIL 3.0.

API Changes#

None.

Bug Fixes#

  • DULT related bug fixes.

  • KG100S Software component fixes.

Chip Enablement#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

None.

Enhancements#

None.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

None.

Modified APIs#

None.

Removed APIs#

None.

Deprecated APIs#

None.

Bug Fixes#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1512585 DULT - Handle stopped BLE stack. None.
  • Amazon Sidewalk - SoC CLI
  • All BLE OPNs and boards
  • SoC
1528095 Semtech component not added automatically with KG100S Software component. None.
  • Amazon Sidewalk - SoC Hello Neighbor, Amazon Sidewalk - SoC CLI
  • All the OPNs
  • SoC
  • PAL

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

None.

Modified Examples#

None.

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

None.

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

None.

Migration Guide#

None.

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

The Sidewalk MCU SDK v2.8.0 release introduces mainly support for the latest SiSDK 2025.12.0 and stability improvements. RAIL 3.0 support is available with this release.

Compatible Software#

Software Compatible Version or Variant
Simplicity SDK Simplicity SDK 2025.12.0
Amazon Sidewalk SDK 1.19.1

Installation and Use#

To run your first demo, see our Getting Started Guides.

To kick start your development, see our Developer's Guide.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

For recommended settings, configurations, and usage guidelines, see our Developer's Guide.

To learn more about the software in this release, dive into our online documentation.

Help and Feedback#

Feature Matrix#

Unsupported Features#

  • Sidewalk Bulk Data Transfer (SBDT): Sidewalk BLE integrated OTA mechanism is available in our Sidewalk alpha repository, as it is not publicly accessible on the Amazon AWS side.

  • Switched Multiprotocol (SMP): Sidewalk, BLE, Z-Wave SMP PoC are available in our alpha repository.

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.