Bluetooth LE - 802.15.4 Mesh + BLE Multiprotocol Version 11.0.0 (Jan 22, 2025) - Release Notes#
This document provides release information for the 802.15.4 Mesh + BLE Multiprotocol SDK.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Concurrent Listening support with CMP on SiMG301x.
Bi-directional Green Power support with CMP Zigbee NCP + OpenThread RCP.
API Changes#
None.
Bug Fixes#
Targeted quality improvements and bug fixes.
Chip Enablement#
xGM270S Leopard SiP Module GA SW support.
xG301 Explorer Kit and Pro-kit support.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Bi-directional Green Power support with CMP Zigbee NCP + OpenThread RCP#
Added bi-directional Green Power support with CMP Zigbee NCP + OT RCP configuration, enabling Green Power Proxy functionality in NCP-RCP multiprotocol applications.
Enhancements#
None.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
None.
Deprecated APIs#
Deprecated API Name | Planned Removal Date |
|---|---|
2026 Q1 |
Bug Fixes#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1471746 | Fixed an issue where the Zigbee + Bluetooth NCP application examples did not appear in Studio. | N/A | Zigbee + Bluetooth NCP app |
| 1524505 | Fixed an issue that could pass an invalid mac layer packet to cause an assert. | N/A | All OPNs, boards, modes and interfaces |
| 1568095 | Changed default SL_BT_CONTROLLER_BUFFER_MEMORY value for OpenThread NCP + BLE RCP application to work on parts with 96kB RAM. | N/A | OpenThread NCP + BLE RCP app |
Chip Enablement#
xGM270S Leopard SiP Module: Added GA software support for xGM270S Leopard SiP Module.
xG301 Explorer Kit and Pro-kit Support: Added support for Explorer Kit and Pro-kit boards for xG301 devices.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
| Example Name | Description | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
ot-ncp-ble-rcp See README |
New sample application that integrates DMP BLE-RCP components with OpenThread NCP FTD CPC application, enabling OpenThread NCP with BLE RCP support. | N/A | NCP | All supported OPNs, boards, modes and interfaces | CPC |
|
zigbee_ncp_ot_rcp_uart_gp_multi_rail See README |
New sample application providing bi-directional Green Power support with CMP Zigbee NCP + OT RCP configuration using multi-rail UART interface. | N/A | NCP/RCP | All supported OPNs, boards, modes and interfaces | UART |
Modified Examples#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Zigbee - BLE Dynamic Multiprotocol Light SED See sample here |
The Zigbee BLE - DynamicMultiprotocolLightSed sample project can now be built for boards with only one LED if the LED1 component is excluded from the project. | N/A | N/A | N/A | N/A |
|
Zigbeed See sample here |
The Zigbeed sample application is now extended with the --conf parameter, so the location of the zigbeed.conf is now configurable and not being hardcoded to /usr/local/etc/zigbeed.conf | N/A | N/A | N/A | N/A |
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1209958 | The Zigbee + OpenThread + BLE RCP may stop working in endurance testing (~2 hours) on MG24 and MG21 devices with constant and concurrent traffic on all three stacks. | N/A | None | Zigbee + OpenThread + BLE RCP app |
| 1385052 | Coex-enabled RCP may still occasionally transmit TX ACK after losing the Grant even when Acking is disabled and TX Abort is enabled. | N/A | This will be fixed in future releases. | Coex-enabled RCP |
| 1385486 | TX from coex-enabled RCP may infrequently happen without the request after turning on the non-802.15.4 compliant MAC Holdoff coex option. | N/A | This will be fixed in future releases. | Coex-enabled RCP |
| 1457086 | Coex-enabled EFR32MG24 RCP may sometimes output higher than expected grant denied counts in the PTA counters. | N/A | This will be fixed in future releases. | Coex-enabled RCP |
| 1458795 | Using BLE GAP scanning stop command in the Zigbee DMP GP - Proxy app may not be able to stop BLE scanning on certain parts. | N/A | None | Zigbee DMP GP - Proxy app |
| 1514786 | Wi-Fi coexistence on SixG301 is currently not supported. Other references: 1514794, 1515385. |
N/A | This will be supported in future releases. | SixG301 devices |
| 1569847 | Using the CMP Zigbee NCP + OpenThread RCP application with Bi-directional Green Power support, bi-directional commissioning may intermittently fail. | N/A | None | EFR32xG24 devices |