Simplicity SDK Platform - Bootloader Version 3.2.0 - Release Notes (Jan 22, 2026)#

Simplicity SDK Platform Version 6.0.0

The Gecko Bootloader is a common bootloader framework used across modern Silicon Labs MCUs and wireless SoCs. It offers configurable features such as device initialization and secure firmware updates.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

  • EM4 GPIO retention during Firmware Upgrade for Series-2 devices.

  • Added support for the xG2D device family.

API Changes#

None.

Bug Fixes#

Fixed a boot hardfault caused by power loss during the AXiP erase phase.

Chip Enablement#

None.

Key Features#

Gecko Bootloader has been updated to support the latest devices, enabling bootloading functionality on the latest hardware platforms. It now includes the ability to parse GBL version 4 files, ensuring compatibility with the latest firmware formats. Sample applications demonstrating these features are included in the SDK.

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

  • EM4 GPIO retention during Firmware Upgrade for Series-2 devices.

  • Added support for the xG2D device family.

Enhancements#

None.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

New API Signature

Deprecated API replaced by this (if any)

bootloader_rebootAndInstallWithGpioRetention()

None

Modified APIs#

None.

Removed APIs#

None.

Deprecated APIs#

None.

Bug Fixes#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1521516 Resolved an issue where loss of power during the AXiP erase phase could leave the application region partially erased and incorrectly treated as valid, resulting in a hardfault on boot. The bootloader now detects this state and reliably re-enters firmware-upgrade mode for seamless recovery. None

None

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

None.

Modified Examples#

None.

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitation#

None.