Simplicity SDK Version 2025.12.1 - Release Notes (Feb 5, 2026)#
The primary tool for the Silicon Labs IoT software development ecosystem, combining wireless software development kits (SDKs) and platform into a single, integrated package.
Release Announcement#
Starting with the 2025.12 release, the Simplicity SDK transitions from GitHub-based monolithic delivery to a modular, Conan-based package model.
To obtain and work with the Simplicity SDK 2025.12, customers must use Silicon Labs Tool (SLT) v1.1.0 or newer, available through:
SLT-CLI (v1.1.0+) – a standalone command-line tool
Simplicity Installer (v1.1.0+) – a graphical installer that integrates SLT-CLI functionality
This update also introduces a new directory structure organized by technology and functional domain, which may affect how SDKs are integrated, consumed, and automated in developer workflows.
Developer Guidance#
CLI development (Headless or CI/CD dev setups)#
Need to update scripts that rely on ‘git clone’ and integrate SLT to manage and automate the SDK delivery.
Any tooling, scripts, or manual workflows that rely on fixed SDK paths may need to be updated accordingly.
GUI development (Simplicity Studio 6)#
No SLT-CLI integration is needed, but note that SDKs are now stored in versioned Conan package directories managed by SLT.
Directory path changes:
Studio 5 (SDK 2025.6): ~/SimplicityStudio/SDKs/simplicity_sdk
Studio 6 (SDK 2025.12): ~/.silabs/slt/installs/conan/p/simplxxxxxxxxxxx/p
Resources#
For SDK download and installation instructions, see the SLT-CLI Getting Started Guide or Simplicity Installer Getting Started Guide.
For project migration, refer to the SLC-CLI Project Migration Guide or Simplicity Studio Project Migration Guide.
Note: This Simplicity SDK release will be published on GitHub for reference purposes only, not recommended for development. Development should use the SDK packages delivered via SLT.
Release Summary#
| Release Item | Version | Release Date | Key Features | Chip Enablement |
|---|---|---|---|---|
Platform |
6.0.0 |
Jan 22, 2026 |
Platform MCU
|
|
RAIL Library |
3.0.1 |
Feb 5, 2026 |
|
No new chips enabled this release. |
RAIL SDK |
3.0.0 |
Jan 22, 2026 |
|
No new chips enabled this release. |
USB |
1.6.0 |
Jan 22, 2026 |
Underlying platform changes only. | No new chips enabled this release. |
Wi-Fi 6 + BLE (WiSeConnect) |
4.0.0 |
Jan 22, 2026 |
Wi-Fi
|
No new chips enabled this release. |
OpenThread |
3.0.0 |
Jan 22, 2026 |
OpenThread
|
OpenThread
|
Zigbee |
9.0 |
Jan 22, 2026 |
Zigbee
|
Zigbee
|
Bluetooth LE |
11.0.0 |
Jan 22, 2026 |
Example and Middleware
|
Bluetooth LE
|
Bluetooth Mesh |
10.0.0 |
Jan 22, 2026 |
GCC LTO (Link-Time Optimization) | No new chips enabled this release. |
Bluetooth Location Services |
11.0.0 |
Jan 22, 2026 |
|
No new chips enabled this release. |
Z-Wave |
8.0.0 |
Jan 22, 2026 |
|
No new chips enabled this release. |
Wi-SUN |
2.10.0 |
Jan 22, 2026 |
|
No new chips enabled this release. |
Silicon Labs Matter |
2.8.0-1.5 |
Jan 22, 2026 |
|
This release supports Series 2 and Series 3 EFR32 devices. Use v2.2.x-1.2 for Series 1 devices. |
Amazon Sidewalk |
2.8.0 |
Jan 22, 2026 |
|
No new chips enabled this release. |
Connect |
4.2.0 |
Jan 22, 2026 |
Added RAIL 3.0.0. integration in both Stack and SDK. | No new chips enabled this release. |
Machine Learning |
2.2.0 |
Jan 22, 2026 |
|
|
Simplicity Connect Mobile App |
3.2.0 |
Jan 22, 2026 |
Added:
|
No new chips enabled this release. |
Note: Click here for earlier releases on GitHub.
Looking for older release notes? You can still access previous versions for both Simplicity SDK (prior to 2025.6.0) and Gecko SDK here.