SiSDK Platform - Micrium OS Version 5.18.1 (July 21, 2025) - Release Notes#
Simplicity SDK Platform Version 5.2.1
Simplicity SDK Version 2025.6.1
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 5.2.1#
None.
Added in 5.2.0#
Improved support for main stack overflow detection.
Added support for GCC Link Time Optimization (LTO).
API Changes#
None.
Bug Fixes#
Fixed in 5.2.1#
None.
Fixed in 5.2.0#
Resolved false positive link time warnings in the MicriumOS CMSIS-RTOS layer when Link Time Optimization (LTO) is enabled.
Chip Enablement#
Added in 5.2.1#
None.
Added in 5.2.0#
Added support for the EFR32BG29 and EFR32MG29 devices (Series 2).
Added support for the EFR32BG22L devices (EFR32BG22L122F352GM32).
Added support for the EFR32BG24L devices (EFR32BG24L010F768IM40 and EFR32BG24L210F768IM40).
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 5.18.1#
Restricted Micrium OS usage to Series 2 devices.
Added in 5.18.0#
Added support for GCC Link Time Optimization (LTO).
Enhancements#
Added in 5.2.1#
None.
Added in 5.2.0#
Improved support for main stack overflow detection utilizing the MSPLIM register.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
Fixed in 5.2.1#
None.
Fixed in 5.2.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1426961 | Fixed link time warnings in the MicriumOS CMSIS-RTOS layer by reworking code implementation, eliminating false positive warnings that occurred only when Link Time Optimization (LTO) was activated. | None | Series 2 Devices |
Chip Enablement#
None.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None.
Modified Examples#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1166857 | OSTaskQPost doesn't send a message to current task when called with a null pointer as argument. | None | None | All Devices |