Wi-SUN SDK Version 2.8.0 (September 24, 2025) - Release Notes#
Simplicity SDK Version 2025.6.2
Wireless Smart Ubiquitous Network (Wi-SUN) is the leading IPv6 sub-GHz mesh technology for smart city and smart utility applications. Wi-SUN brings Smart Ubiquitous Networks to service providers, utilities, municipalities/local government, and other enterprises, by enabling interoperable, multi-service, and secure wireless mesh networks. Wi-SUN can be used for large-scale outdoor IoT wireless communication networks in a wide range of applications covering both line-powered and battery-powered nodes.
Silicon Labs' Wi-SUN hardware is certified by the Wi-SUN Alliance, a global industry association devoted to seamless LPWAN connectivity. Wi-SUN builds upon open standard internet protocols (IP) and APIs, enabling developers to extend existing infrastructure platforms to add new capabilities. Built to scale with long-range capabilities, high-data throughput and IPv6 support, Wi-SUN simplifies wireless infrastructure for industrial applications and the evolution of smart cities.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 2.8.0#
Added an event logging system that forwards network events to the application. It can be used for troubleshooting or passive scanning.
Added in 2.7.0#
None.
Added in 2.6.0#
Added Wi-SUN+BLE dynamic multi-protocol (DMP) support.
Added concurrent detection support.
API Changes#
Changed in 2.8.0#
Added a new API to configure network events logging.
Changed in 2.7.0#
Added new APIs to fine tune the regional regulation mechanisms
Extended the connection parameters with lower-MAC configurations
Changed in 2.6.0#
Added sl_wisun_set_preferred_pan() API that sets a FFN preferred PAN. A router will try to roam to its preferred PAN if it is available.
Bug Fixes#
Fixed in 2.8.0#
Fixed multiple issues exposed by failing memory allocations.
Fixed in 2.7.0#
Fixed a security vulnerability in the Border Router SoC authenticator. It was introduced in 2.6.0.
Fixed in 2.6.0#
Fixed an issue causing devices to be stuck in join state 3.
Fixed multiple MAC issues causing RCP instabilities.
Chip Enablement#
Added in 2.8.0#
None.
Added in 2.7.0#
None.
Added in 2.6.0#
EFR32FG23 as RCP.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 2.8.0#
Added sl_wisun_set_event_filter()
API. Its function provides a mechanism to configure event filtering for Wi-SUN devices based on a specific MAC address and event flags. This allows developers to selectively monitor only the events of interest for a given device, improving efficiency and reducing unnecessary event handling. With appropriate configuration, it can be used for passive scanning (e.g., load balancing) or troubleshooting connection issues.
Added in 2.7.0#
Added
sl_wisun_set_regulation_parameters()
API. It is now recommended to use this new interface to configure the regional regulation mechanisms used in the stack. Whilesl_wisun_set_regulation()
is not yet deprecated, usingsl_wisun_set_regulation_parameters()
is strongly encouraged. The new interface offers finer control over the parameters that impact compliance with regional regulations and is decoupled from the Regulator Domain set in the connection parameters. Presets per region are exposed in sl_wisun_regulation_api.h and could be used as-is or copied and edited.Added
sl_wisun_reset_regulation_duty_cycle()
API. This API resets the transmission duty cycle counters. It is recommended to call this API after a maintenance operation if the regional regulation permits excluding certain operations from duty cycling constraints.Added
sl_wisun_set_eap_identity()
. This function sets the identity used in the EAP Identity Response during EAP authentication.Extended the capacities of sl_wisun_set_connection_parameters() with low-MAC configurations in a backward-compatible manner. Is is now possible to fine-tune the CSMA and retransmission configurations. It is recommended to lower the min_be value to reach higher throughput.
Made the statistic type definition public and added a new statistic field to distinguish between file transfer time and total firmware update time.
Added in 2.6.0#
Added concurrent detection support. EFR32FG25 is capable of receiving and processing FSK and OFDM without any prior negotiation, optimizing the mode switch procedure by making the mode switch PHR optional. Refer to AN1410 Getting Started with Concurrent Mode on EFR32FG25 using RAILtest for more information.
Added
sl_wisun_config_concurrent_detection()
API. It configures whether an alternate PHY can be used concurrently for transmissions instead of the standard mode switch.Added Wi-SUN/BLE dynamic multiprotocol (DMP) support.
Updated BZ and SG channel plans according to Wi-SUN PHY TPS 2v03.
Ownership of
chan_params_table
is now transferred to the application. Each entry ofchan_params_table
defines a specific configuration containing PHY information such as the frequency, the channel numbers, and the modulation. It is recommended to adapt the content of the table to the end application use to optimize flash consumption. It is critical to ensure the content of the table is well aligned with the content of the configuration set in Simplicity Studio Radio Configurator.Added
sl_wisun_set_preferred_pan()
API. It sets a preferred PAN ID that the device will always select during connection if available, or seek to roam to while connected to another PAN.Added
sl_wisun_config_neighbor_table()
API. It configures the maximum number of RPL children, neighbors, and security neighbors, allowing fine-tuning of memory usage and network scalability.Added
sl_wisun_br_trigger_global_repair()
border router API to manually trigger a global repair. It allows manual triggering of a global repair operation on the border router.Added
sl_wisun_br_get_routing_table_entry_count()
andsl_wisun_br_get_routing_table()
for the SoC Border Router. They can be used to retrieve the number of routing table entries and the routing table itself in order to render the network topology.Added an event
SL_WISUN_MSG_BR_ROUTING_TABLE_UPDATE_IND_ID
that is triggered when the Border Router (BR) routing table is updated, with differentiation by update type. The structure returned by this event contains details about the routing table change, including the type of update and relevant routing entry information.Introduced
sl_wisun_lfn_params_t
v3, with neweapol_unicast_interval_ms
parameter.Extended the network statistics (
sl_wisun_statistics_network_t
) with MPL statistics.Extended the network statistics (
sl_wisun_statistics_network_t
) with the node's estimated hop count to the BR. Paired withsl_wisun_set_leaf()
, it could be used to limit the depth of the network.A
SL_WISUN_MSG_NETWORK_UPDATE_IND
event is now triggered upon a hop count estimation update. Added a new valueSL_WISUN_NETWORK_UPDATE_FLAGS_HOP_COUNT
tosl_wisun_msg_network_update_ind_body_t
flag
field.Extended the MAC statistics (
sl_wisun_statistics_mac_t
) with the time spent in idle and TX states.Extended the Heap statistics (
sl_wisun_statistics_heap_t
) with output highest used, currently used, free, and total heap space.Extended the connection parameters (
sl_wisun_connection_params_t
) with fragmentation and EDFE configuration parameters.Extended the LFN configuration parameters (
sl_wisun_lfn_params_t
) with EAPOL unicast wake-up interval.Added multi-fragment EDFE support. EDFE is used automatically on all fragmented packets.
Introduced Wi-SUN NVM versioning.
ETSI Adaptive Power Control is now available for EU PHYs. It was previously limited to Indian configurations.
FFN and LFN now store frame counters for up to 15 different PANs. It was necessary to be able to navigate between two PANs either in the context of a switch to a preferred PAN or following multiple power outages.
Enhancements#
Added in 2.8.0#
Improved DIS transmission strategy in order to reduce the congestion in dense networks.
Updated the default eapol key-request parameters.
Added in 2.7.0#
None.
Added in 2.6.0#
Rework the supplicant leading to significant RAM and Flash usage diminution.
Enhanced debug and trace capabilities for RCP and SoC. MAC traces are now enabled by default in the RCP.
ACK timeout is now measured to the start of the response frame, allowing faster RX channel return if no response is received.
EDFE FC-IE transmit flow control now matches estimated frame duration. It was previously set to the maximum value and was not used on the receiver's side.
Wi-SUN Header IEs (WH-IEs) from duplicate frames are now processed.
Delayed initial DIS to avoid overlap with PC sequence.
Added more meaningful status codes for
SL_WISUN_MSG_SOCKET_DATA_SENT_IND_ID
indication.Temporary denial of routers unable to parent. Do not send unicast DIS to denied neighbors.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added in 2.8.0#
New API Signature | Deprecated API replaced by this (if any) |
---|---|
None |
Added in 2.7.0#
New API Signature | Deprecated API replaced by this (if any) |
---|---|
None | |
None | |
None | |
None |
Added in 2.6.0#
New API Signature | Deprecated API replaced by this (if any) |
---|---|
None | |
None | |
None | |
None | |
None |
Modified APIs#
Modified in 2.7.0#
Extended the capacities of sl_wisun_set_connection_parameters() with low-MAC configurations in a backward-compatible manner. Is is now possible to fine-tune the CSMA and retransmission configurations. It is recommended to lower the min_be value to reach higher throughput.
Modified in 2.6.0#
Extended the capacities of sl_wisun_set_connection_parameters() with fragmentation and EDFE configuration in a backward-compatible manner.
Extended the capacities of sl_wisun_set_lfn_parameters() with EAPOL unicast wake-up interval in a backward-compatible manner.
Removed APIs#
None.
Deprecated APIs#
Deprecated in 2.8.0#
None.
Deprecated in 2.7.0#
None.
Deprecated in 2.6.0#
Deprecated API Name | Planned Removal Date |
---|---|
Not before June 5, 2026 |
Bug Fixes#
Fixed in 2.8.0#
ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
---|---|---|---|
1479175 | Fixed an issue causing the supplicant to become non-responsive to 4-WHS message 3 retries. | ||
1484842 | Added a missing frame counter increment on reboot during initial connection. It was causing a misalignment between a device and its neighbors and was significantly slowing down the reconnection. | ||
1486556 | Fixed an invalid frame counter reset when setting eapol.allow_skip to false. | ||
1486624 | Fixed an issue causing LFN directly connected to the border router to be missing in the routing graph. | ||
1488042 | Fixed the scheduling of the packets transmissions when switching to the secondary parent. NS with zero lifetime were sent before receiving a DAO-ACK. It was causing disconnections in case the DAO was lost. | ||
1490185 | Stopped forwarding DHCP and EAPOL messages when no longer in Join State 5 (Operational). | ||
1488565 | Fixed radio being disabled after mode switch PHR RX on LFN, which could block further TX/RX. | ||
1483332 | Fixed initial_key_max_s overflowing when set above 65. It was causing the delay between the PAN selection and the beginning of the authentication to be to short and was ultimately generating congestion. | ||
1499563 | Fixed MAC security neighbor table growing beyond configured maximum. It was causing an unexpected and uncontrolled heap consumption increase. | ||
1499563 | Fixed invalid security neighbor table entry allocation on unsecured frame reception. | ||
1484185 | Fixed memory corruption when processing RPL source routing header (SRH) with size increase. SRH are only resized on rare occasions. | ||
1479175 | Fixed assert when memory allocation fails. Improved the overall stability of the solution when it is running out of memory. | ||
1485281 | Fixed segmentation fault if sl_wisun_reset_statistics() is called before the initial connection. | ||
1486065 | Fixed segmentation fault if aborting during transmission of a ack/response frame or mode switch. | ||
1502406 | Fixed possible lock in MAC during mode switch. It was causing all transmissions to be randomly staled. | ||
1507522 | Fixed the reception of empty source routing headers (SRH). Non-Silicon Labs Wi-SUN stack can send SRH with no route. |
Fixed in 2.7.0#
ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
---|---|---|---|
1474061 | Fixed authenticator vulnerability to installation of predictable keys. | BR | |
1466748 | Corrected an issue where the authenticator was dropping supplicant retries under high congestion conditions. This fix ensures that supplicants re-initiating TLS while already on the active list are no longer dropped. | ||
1465055 | Fixed asynchronous fragments splitting with DFE/EDFE frames. | BR, FFN | |
1464297 | Fixed socket TX buffer filling in case of routing or memory error. | BR, FFN, LFN | |
1468808 | Fixed segmentation fault when unexpected EDFE final frame is received. | BR, FFN | |
1473077 | Fixed a fault when an LFN fails to complete multiple handshakes in join state 5. | LFN | |
1458827 | Fixed node failing to connect after obtaining an inactive GTK first. | FFN | |
1432653 | Fixed an invalid hop limit when forwarding multicast packets to LFNs. It was not decremented | BR, FFN | |
1476119 | Fixed CCA threshold value used for O-QPSK PHYs. | BR, FFN, LFN | |
1478072 | Fixed memory corruption when returning to join state 1 while proxying RPL for LFNs. | FFN | |
1479483 | Fixed MAC TX confirmation overwriting previous one in case of consecutive failures. | BR, FFN, LFN, RCP | |
1464597 | Fixed timeout management on asynchronous packets. It was causing blockage in the RPC when trying to start new asynchronous transmissions. | RCP |
Fixed in 2.6.0#
ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
---|---|---|---|
1373901 | Fixed mode switch from router to LFN. | FFN | |
1384392 | Fixed a PSA crypto key leak that prevented authentication after multiple attempts during the device's lifetime. | FFN | |
1385981 | Fixed a critical failure when receiving a GKH in join state 1 by dropping security handshake frames from previous connections. | FFN | |
1385791 | Fixed an issue that prevented LFNs from sending LPAS. | LFN | |
1388948 | Fixed LFNs not unregistering from multicast groups when the corresponding socket was closed. | LFN | |
1144019 | Fixed MPL messages being transmitted more times than the MPL "TimerExpirations" configuration allowed. | BR, FFN | |
1392144 | Fixed DHCP preferred lifetime being invalid when the address lifetime was infinite. | FFN | |
1393742 | Fixed SoC BR task priority starvation by the Wi-Fi backhaul task. | BR | |
1366711 | Fixed unregistering when changing parent (sent NS(ARO) with no lifetime). | FFN | |
1394368 | Fixed RPL Global Repair not transmitting DAO if the same preferred parent was selected. | FFN | |
1390717 | Fixed memory corruption causing authentication failures on Secure Vault Mid devices. | BR, FFN, LFN | |
1399233 | Fixed neighbor cache refresh procedure. | BR, FFN | |
1389186 | Fixed LFN being blocked in reception state for the duration of a broadcast interval. | LFN | |
1394656 | Fixed aborted frames not generating confirmation, which caused many RCP stalls. | BR, FFN, LFN | |
1401857 | Fixed LFN PAN Advertisement transmissions sometimes being stuck until timeout. | LFN | |
1230806 | Fixed EDFE retransmissions not performing retries with CCA backoff. | BR, FFN | |
1412771 | Fixed an FHSS synchronization issue caused by incorrect UFSI values. | BR, FFN, LFN | |
1412117 | Fixed a radio configuration file error with SG PHYs. | BR, FFN, LFN | |
1412791 | Fixed an issue where border router address/prefix lifetime was advertised as 0 instead of infinite in DIO packets. | BR | |
1411742 | Fixed an issue where nodes roamed back and forth with PAN Defect and Preferred PAN enabled. A device could not re-join its previous PAN before a given duration hardcoded in the stack. | FFN | |
1414646 | Fixed an issue by analyzing inner IPv6 headers to refresh neighbor address registrations. | BR, FFN | |
1419046 | Fixed an issue that caused devices to be stuck in join state 3 when they could not decrypt a PC from their previous PAN. | FFN | |
1271915 | Fixed an issue that prevented DAO path sequence counter from resetting when going to join state 1 and 3. | FFN | |
1426446 | Fixed a rescheduling issue with LFN frames that would make a node completely unable to operate. | FFN, LFN | |
1425204 | Fixed invalid duplicated frame detection from LFN neighbors as an FFN. | LFN | |
1425204 | Fixed invalid duplicated frame detection from FFN parent as an LFN. | FFN | |
1438701 | Fixed an LFN issue when multiple frames advertised an updated LUS-IE. | LFN | |
1440283 | Fixed an issue handling invalid 4WH message 3 and GKH message 1. | FFN, LFN | |
1437500 | Fixed the return option value of getsockopt() for SO_SNDLOWAT option. | BR, FFN, LFN | |
1436839 | Fixed send/sendto setting the wrong errno when sendq was full and socket was not in blocking mode. | BR, FFN, LFN | |
1436839 | Fixed send/sendto not returning the correct number of sent bytes in the case of a partial packet send. | BR, FFN, LFN | |
1435786 | Fixed setting errno values for socket API. It was missing for some of the socket APIs. | BR, FFN, LFN | |
1442451 | Fixed synchronization to broadcast schedule after LFN parent selection. | FFN, LFN | |
1429143 | Fixed an issue by deleting ND entries upon the reception of a NS with ARO containing a lifetime of 0. | BR, FFN | |
1445797 | Fixed incorrect backoff slot duration with SUN OFDM. | BR, FFN, LFN | |
1441981 | Fixed an issue where LFN failed in join state 3 when it failed to decrypt an FFN-specific packet. | LFN | |
1424293 | Fixed an issue where PAN Defect IE was relayed twice by FFNs. | FFN | |
1446315 | Fixed ETSI Adaptive Power Control with FAN TPS version 1.0. | BR, FFN, LFN | |
1452100 | Fixed invalid default k trickle parameter. | BR | |
1453003 | Fixed an issue that caused the connections to be significantly longer when an error occurred while trying to send a DAO. Routers were unable to send a second DAO until PAN timeout. | FFN | |
1454000 | Fixed an issue where Preferred PAN and PAN Defect generated too much traffic. | FFN | |
1387966 | Fixed an issue where RCP reset was triggered when MAC purged LFN frames upon LFN PAN Advertisement transmission. It was an abusive critical failure. | RCP | |
1402855 | Fixed Source Addressing Mode of EDFE Response Frames in the RCP. | RCP | |
1377305 | Fixed a wrong error message when reconnecting during an ongoing disconnection. | CLI | |
1390370 | Fixed handling of SL_WISUN_MSG_REGULATION_TX_LEVEL_IND_ID. | BR | |
1484837 | Fixed a memory leak in the authenticator. | BR |
Chip Enablement#
Added in 2.8.0#
None.
Added in 2.7.0#
None.
Added in 2.6.0#
Chip Family | OPNs / Boards / OPN Combinations | Supported Software Variants (if applicable) | Supported Modes | Supported Host Interfaces |
---|---|---|---|---|
EFR32xG23 |
|
N/A | RCP | UART |
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
Added in 2.8.0#
None.
Added in 2.7.0#
None.
Added in 2.6.0#
Example Name | Description | Supported Software Variants (if applicable) | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
---|---|---|---|---|---|
Wi-SUN BLE DMP - SoC Empty |
The Wi-SUN Bluetooth DMP - SoC Empty example project serves as a starting point for developing Wi-SUN and BLE DMP applications. This example can be tested using the Simplicity Connect smartphone application, available on iOS and Android. | N/A | SoC |
|
N/A |
Wi-SUN BLE DMP - SoC SPP |
The Wi-SUN BLE DMP - SoC SPP example demonstrates how to use the Serial Port Profile (SPP) over Bluetooth Low Energy (BLE) to enable wireless serial communication between devices, providing a wireless alternative to traditional wired serial connections. This application reroutes the command line interface (CLI) over BLE, allowing users to interact with the device remotely. You can test this example using the Serial Bluetooth Terminal app for Android. | N/A | SoC |
|
N/A |
Modified Examples#
Modified in 2.8.0#
Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
---|---|---|---|---|---|
All examples |
The legacy Chinese FAN1.0 PHY is replaced by the appropriate FAN1.1 equivalent PHY. | N/A | N/A | brd4272a | N/A |
Wi-SUN RCP |
|
N/A | N/A | All supported boards | N/A |
Modified in 2.7.0#
None.
Modified in 2.6.0#
Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
---|---|---|---|---|---|
All examples |
Migrated all the examples to the new System Setup component. | N/A | N/A |
|
N/A |
All examples |
Refactored polling loops in the CoAP, TFTP Client, OTA DFU, and Ping components. Introduced a new sl_tftp_clnt_wait_op_finished API to wait for the operation finished event flag. | N/A | N/A |
|
N/A |
All examples |
Enabled RTS/CTS flow control in the applications. | N/A | N/A |
|
N/A |
All examples |
Introduced new CLI command configuring RTT Trace level and forwarding the content of RTT traces. | N/A | N/A |
|
N/A |
Wi-SUN - SoC Network Measurement |
Added support for displaying estimated hop count to the Border Router in the measurement output. | N/A | N/A |
|
N/A |
Wi-SUN - SoC Socket application |
Updated socket_read CLI command for UDP. Removed the misleading read size argument. The whole received buffer should be read, this argument is unnecessary. | N/A | N/A |
|
N/A |
OTA DFU component |
Increased SL_WISUN_OTA_DFU_TFTP_TIMEOUT_SEC to 8 seconds in OTA DFU config | N/A | N/A |
|
N/A |
OTA DFU component |
Fixed TFTP Error code typos and added additional debug logs to the error handling in OTA DFU component. | N/A | N/A |
|
N/A |
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
ID | Issue or Limitation Description | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
---|---|---|---|
Wi-SUN Configuration is only capable of provisioning routers using the new Dynamic Data Provisioning methodology. The generation of border router certificates is not supported. | Use the previous provisioning methodology. | All supported parts and boards | |
1119464 | Packets sent when FSK FEC is enabled can infringe ARIB regulation. | Until this problem has been addressed correctly, the stack will refuse to start if both ARIB enforcement and FEC are enabled. | All supported parts and boards |
1067978 | Packets sent using a PHY with a bandwidth larger than the base PHY’s bandwidth can infringe ARIB regulation. | Limit the communications when using mode switch with ARIB enforcement enabled. | EFR32FG25 |
1176014 | FG25 asserts with a RAIL_ASSERT_FAILED_RTCC_SYNC_STALE_DATA error code when entering EM2. | Do not allow the power manager to go to EM2 by adding a requirement on EM1 in the application. | EFR32FG25 |
1373879 | The RCP is sometimes unable to send packets using mode switch. | None | EFR32FG25 |
Throughput is reduced compared to previous releases due to the fix for 1445797. The previous CSMA slot duration was too short, which artificially increased throughput. The impact is more noticeable with high-throughput modulations. Further investigation will be run to better understand and improve the current performances. | None | EFR32FG25 | |
Wi-SUN RCP operation on EFR32FG23 requires hardware flow control to be enabled. Without hardware flow control, CPC requires an additional buffer, which exceeds the available RAM on this device. | None | EFR32FG23 |
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
None.
Migration Guide#
Previous versions of "Wi-SUN - LFN CLI" were using SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM3 that was removed in that version 2025.6 of the Simplicity SDK. Applications generated with an older release of the Simplicity SDK will not compile against version 2025.6. All references to SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM3 can be safely deleted.
Using This Release#
What's in the Release?#
This release contains the following:
Wi-SUN stack library
Wi-SUN sample applications
Wi-SUN border router and RCP pre-compiled demos
Documentation
If you are a first-time user, see the Wi-SUN Getting Started Guide.
Compatible Software#
Software | Compatible Version or Variant |
---|---|
Wi-SUN Linux Border Router (wsbrd) | v2 and more recent. |
Wi-SUN Linux Router (wsrd) | v2.2 and more recent. |
Installation and Use#
The Wi-SUN SDK is distributed as part of the Simplicity SDK, Silicon Labs' unified software development kit suite. To get started quickly, install Simplicity Studio 5, which provides a complete development environment, including project and resource management, software configuration tools, a full IDE with GNU toolchain, and analysis utilities. Step-by-step installation instructions are available in the Simplicity Studio 5 User’s Guide.
Alternatively, you can manually install the Simplicity SDK by downloading or cloning the latest release from GitHub.
By default, Simplicity Studio installs the Simplicity SDK to:
Windows:
C:\Users\<NAME>\SimplicityStudio\SDKs\simplicity_sdk
macOS:
/Users/<NAME>/SimplicityStudio/SDKs/simplicity_sdk
Documentation for each SDK version is included with the SDK installation.
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note: Ask AI is experimental.
Get help from our developer community.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.