Over-The-Air Device Firmware Upgrade (Alpha)#

The Wi-SUN Over-The-Air Device Firmware Upgrade (OTA DFU) service is implemented to facilitate the updating of Wi-SUN device firmware. This component requires the Gecko Bootloader API to execute firmware writing, verification, and bootload operations.

To obtain a new Gecko Bootloader File (GBL) from a remote host Over-The-Air, a Trivial File Transfer Protocol (TFTP) client is employed, leveraging the Wi-SUN network. The entire firmware upgrade session is manageable over CoAP, with the service offering remote host connection settings, firmware file selection, notification, and status request capabilities. Configuration of the connection to the TFTP remote host can be accomplished within the component configuration file. To use this component, a bootloader must be flashed onto the device. The component relies on functions that reside within the bootloader. To choose the appropriate bootloader, consider factors such as flash location (internal or external) and size. To save on download time, we recommend applying compression on both the bootloader and device projects.

The following diagram shows the component architecture: ota-dfu-componentota-dfu-component

The example below shows how OTA DFU can be performed in any project.

#include <stdio.h>
#include "cmsis_os2.h"
#include "sl_wisun_ota_dfu.h"

static void start_ota_dfu(void) {
  sl_status_t api_status = SL_STATUS_FAIL;
  uint32_t fw_update_status = 0;

  // Set remote host that stores the firmware image.
  // TFTP protocol is used to download the firmware.
  // 69 is the default TFTP Port
  api_status = sl_wisun_ota_dfu_set_host_addr("2001:db8::1", 69);
  if (api_status != SL_STATUS_OK) {
    // Error handling
    return;
  }

  // Set GBL file path
  // The path is relative to the preconfigured TFTP shared directory
  api_status = sl_wisun_ota_dfu_set_gbl_path("my_new_firmware.gbl");
  if (api_status != SL_STATUS_OK) {
    // Error handling
    return;
  }

  // Start firmware update
  api_status = sl_wisun_ota_dfu_start_fw_update();
  if (api_status != SL_STATUS_OK) {
    // Error handling
    return;
  }

  // Waiting for the firmware download to finish.
  while(1) {
    fw_update_status = sl_wisun_ota_dfu_get_fw_update_status();
    if (fw_update_status & (1 << SL_WISUN_OTA_DFU_STATUS_FW_DOWNLOADED)) {
      printf("Firmware downloaded. Preparing to bootload\n");
      break;
    } else if (fw_update_status & (1 << SL_WISUN_OTA_DFU_STATUS_FW_DOWNLOAD_ERROR)) {
      printf("Firmware download failed\n");
      break;
    }
    osDelay(1);
  }
}

The CoAP remote settings can be configured as follows:

coap-client -m get -N -B 3 -t text coap://[$WISUN_NODE_IPV6_ADDR]:5683/ota/dfu -e "help"

Commands:

[P: POST (set), G: GET (get)]
[G] help
[G] (empty payload) status
[P] start
[P] stop
[P] install
[G|P] host_address <ipv6> <port>
[G|P] gbl <path>
[G|P] uri <path>
[G|P] notify_host_address <ipv6> <port>
[G|P] notify_uri <path>
[G|P] notify_chunk_cnt <count>

Modules#

Type definitions

Configurations

Functions#

void
sl_wisun_ota_dfu_error_hnd(const sl_wisun_ota_dfu_error_code_t error_code, sl_wisun_ota_dfu_error_ctx_t *const ctx)

OTA DFU error handler (weak implementation)

void

Free the status string buffer.

sl_status_t
sl_wisun_ota_dfu_get_fw_update_statistics(sl_wisun_ota_dfu_statistics_t *const stats)

Get firmware update statistics.

uint32_t

Get the status value.

bool
sl_wisun_ota_dfu_get_fw_update_status_flag(const sl_wisun_ota_dfu_status_t status_flag)

Get the status flag value.

const char *

Get the status string in JSON format.

sl_status_t
sl_wisun_ota_dfu_get_gbl_path(char *const dst_gbl_path, const uint16_t dst_gbl_path_size)

Get GBL file path.

sl_status_t
sl_wisun_ota_dfu_get_host_addr(char *const dst_host, const uint16_t dst_host_size, uint16_t *dst_port)

Get host addres and port.

sl_status_t
sl_wisun_ota_dfu_get_host_uri(char *const dst_uri, const uint16_t dst_uri_size)

Get host uri path.

void

Initialize the device firmware upgrade service.

sl_status_t
sl_status_t
sl_wisun_ota_dfu_set_gbl_path(const char *gbl_path)

Set GBL file path.

sl_status_t
sl_wisun_ota_dfu_set_host_addr(const char *host, const uint16_t port)

Set host address and port.

sl_status_t

Set host uri path.

sl_status_t

Start firmware update.

sl_status_t

Stop firmware update.

Macros#

#define

OTA DFU CoAP URI Path string buffer length.

#define

OTA DFU GBL File name string buffer length.

#define

OTA DFU IPV6 string buffer length.

#define

OTA DFU Service loop.

Function Documentation#

sl_wisun_ota_dfu_error_hnd#

void sl_wisun_ota_dfu_error_hnd (const sl_wisun_ota_dfu_error_code_t error_code, sl_wisun_ota_dfu_error_ctx_t *const ctx)

OTA DFU error handler (weak implementation)

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_ota_dfu_error_code_t[in]error_code

Error code

sl_wisun_ota_dfu_error_ctx_t *const[in]ctx

Error context with error details

Catch error in different stages of boot load.


sl_wisun_ota_dfu_free_fw_update_status_json_str#

void sl_wisun_ota_dfu_free_fw_update_status_json_str (const char * str)

Free the status string buffer.

Parameters
TypeDirectionArgument NameDescription
const char *[in]str

String ptr

Call CoAP free to release allocated memory


sl_wisun_ota_dfu_get_fw_update_statistics#

sl_status_t sl_wisun_ota_dfu_get_fw_update_statistics (sl_wisun_ota_dfu_statistics_t *const stats)

Get firmware update statistics.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_ota_dfu_statistics_t *const[out]stats

Pointer to statistics structure

Get firmware update statistics Returns

  • sl_status_t SL_STATUS_OK on success, otherwise failure


sl_wisun_ota_dfu_get_fw_update_status#

uint32_t sl_wisun_ota_dfu_get_fw_update_status (void )

Get the status value.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returning the value of event flags Returns

  • uint32_t Status


sl_wisun_ota_dfu_get_fw_update_status_flag#

bool sl_wisun_ota_dfu_get_fw_update_status_flag (const sl_wisun_ota_dfu_status_t status_flag)

Get the status flag value.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_ota_dfu_status_t[in]status_flag

Status flag enum

Bool representation of status variable bit value Returns

  • bool true if the flag is set, otherwise false


sl_wisun_ota_dfu_get_fw_update_status_json_str#

const char * sl_wisun_ota_dfu_get_fw_update_status_json_str (void )

Get the status string in JSON format.

Parameters
TypeDirectionArgument NameDescription
voidN/A

String buffer is allocated in heap by CoAP allocator Returns

  • const char * Allocated string pointer on success, otherwise NULL


sl_wisun_ota_dfu_get_gbl_path#

sl_status_t sl_wisun_ota_dfu_get_gbl_path (char *const dst_gbl_path, const uint16_t dst_gbl_path_size)

Get GBL file path.

Parameters
TypeDirectionArgument NameDescription
char *const[out]dst_gbl_path

GBL file path

const uint16_t[in]dst_gbl_path_size

GBL path size

Get GBL file path Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_get_host_addr#

sl_status_t sl_wisun_ota_dfu_get_host_addr (char *const dst_host, const uint16_t dst_host_size, uint16_t * dst_port)

Get host addres and port.

Parameters
TypeDirectionArgument NameDescription
char *const[out]dst_host

Host address

const uint16_t[in]dst_host_size

Host address size

uint16_t *[out]dst_port

Host port

Get host address and port Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_get_host_uri#

sl_status_t sl_wisun_ota_dfu_get_host_uri (char *const dst_uri, const uint16_t dst_uri_size)

Get host uri path.

Parameters
TypeDirectionArgument NameDescription
char *const[out]dst_uri

Uri path

const uint16_t[in]dst_uri_size

Uri path size

Get host uri path Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_init#

void sl_wisun_ota_dfu_init (void )

Initialize the device firmware upgrade service.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize Wi-SUN OTA Device Firmware Upgrade service.


sl_wisun_ota_dfu_reboot_and_install#

sl_status_t sl_wisun_ota_dfu_reboot_and_install (void )

Reboot device.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Reboot device with calling corresponding gecko bootloader 'bootloader_rebootAndInstall' API This functions is available if auto-reboot mode is disabled. Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_set_gbl_path#

sl_status_t sl_wisun_ota_dfu_set_gbl_path (const char * gbl_path)

Set GBL file path.

Parameters
TypeDirectionArgument NameDescription
const char *[in]gbl_path

GBL file path

Set GBL file path Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_set_host_addr#

sl_status_t sl_wisun_ota_dfu_set_host_addr (const char * host, const uint16_t port)

Set host address and port.

Parameters
TypeDirectionArgument NameDescription
const char *[in]host

Host address

const uint16_t[in]port

Host port

Set host address and port Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_set_host_uri#

sl_status_t sl_wisun_ota_dfu_set_host_uri (const char * uri)

Set host uri path.

Parameters
TypeDirectionArgument NameDescription
const char *[in]uri

Uri path

Set host uri path Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_start_fw_update#

sl_status_t sl_wisun_ota_dfu_start_fw_update (void )

Start firmware update.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Start firmware update by setting SL_WISUN_OTA_DFU_STATUS_FW_UPDATE_STARTED flag Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_stop_fw_update#

sl_status_t sl_wisun_ota_dfu_stop_fw_update (void )

Stop firmware update.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Stop firmware update by setting SL_WISUN_OTA_DFU_STATUS_FW_UPDATE_STOPPED flag Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


Macro Definition Documentation#

SL_WISUN_OTA_DFU_COAP_URI_PATH_STR_BUF_LEN#

#define SL_WISUN_OTA_DFU_COAP_URI_PATH_STR_BUF_LEN
Value:
128U

OTA DFU CoAP URI Path string buffer length.


SL_WISUN_OTA_DFU_GBL_PATH_STR_BUF_LEN#

#define SL_WISUN_OTA_DFU_GBL_PATH_STR_BUF_LEN
Value:
256U

OTA DFU GBL File name string buffer length.


SL_WISUN_OTA_DFU_IPV6_STR_BUF_LEN#

#define SL_WISUN_OTA_DFU_IPV6_STR_BUF_LEN
Value:
40U

OTA DFU IPV6 string buffer length.


SL_WISUN_OTA_DFU_SERVICE_LOOP#

#define SL_WISUN_OTA_DFU_SERVICE_LOOP
Value:
()

OTA DFU Service loop.