Ping#

The Ping component implements a ping service using the ICMPv6 protocol. It can send ICMPv6 Echo Request, receive corresponding responses, and calculate round-trip latency.

Applications can emit a single ping packet using the sl_wisun_ping_request() API. To receive the pong response, the sl_wisun_ping_response() API is called. The sl_wisun_ping() function offers a straightforward solution for periodic ping packet transmission and reception. To halt the process, use the sl_wisun_ping_stop() function.

Ping test parameters such as size, number of pings sent, and timeout for response absence are configurable. Initialization of the component is done by calling the sl_wisun_ping_init() function.

The following example demonstrates how the ping request can be called:

#include "sl_wisun_ping.h"

static void ping_remote(void) {
  int32_t ret = 0;
  sockaddr_in6_t remote_addr = { 0 };
  sl_status_t status = SL_STATUS_FAIL;

  // Create address structure from ping
  ret = inet_pton(AF_INET6,
                  "2001:db8::1",
                  &remote_addr.sin6_addr);

  if (ret != 1) {
    // Error handling
    return;
  }

  // Send and receive ping requests and responses
  status = sl_wisun_ping(&remote_addr, // Ping remote_addr IPv6 address
                         10, // with 10 packets
                         512, // packet length is 512 bytes
                         NULL, // Custom statitistic handler is not required
                         NULL); // Request/Response handler is not required
  if (status != SL_STATUS_OK) {
    // Error handling
    return;
  }
}

Modules#

Configurations

Type definitions

Functions#

sl_status_t
sl_wisun_ping(const sockaddr_in6_t *const remote_addr, const uint16_t packet_count, const uint16_t packet_length, sl_wisun_ping_stat_hnd_t stat_hnd, sl_wisun_ping_req_resp_done_hnd_t req_resp_sent_hnd)

Provide a high level ping API.

void

Initialize the ping service module.

void
sl_wisun_ping_request(const sl_wisun_ping_info_t *const ping_request)

Send a ping request.

void
sl_wisun_ping_response(sl_wisun_ping_info_t *const ping_response)

Retrieve a ping response.

void

Stop the current ping process.

Macros#

#define
SL_WISUN_PING_CODE_ECHO_REQUEST (0U)

Ping echo request code field value.

#define
SL_WISUN_PING_CODE_ECHO_RESPONSE (0U)

Ping echo response code field value.

#define
SL_WISUN_PING_ICMP_PORT (0U)

Dedicated port for ICMPv6 echo messages.

#define
SL_WISUN_PING_MAX_PACKET_LENGTH (SL_WISUN_PING_MIN_PACKET_LENGTH - 1 + SL_WISUN_PING_MAX_PAYLOAD_LENGTH)

Max packet length.

#define
SL_WISUN_PING_MAX_REQUEST_RESPONSE (128U)

Maximum count of ping request/response for message queues.

#define
SL_WISUN_PING_MIN_PACKET_LENGTH (9U)

Minimum packet length with 1 byte payload.

#define
SL_WISUN_PING_TYPE_ECHO_REQUEST (128U)

Ping echo request type field value.

#define
SL_WISUN_PING_TYPE_ECHO_RESPONSE (129U)

Ping echo response type field value.

Function Documentation#

sl_wisun_ping#

sl_status_t sl_wisun_ping (const sockaddr_in6_t *const remote_addr, const uint16_t packet_count, const uint16_t packet_length, sl_wisun_ping_stat_hnd_t stat_hnd, sl_wisun_ping_req_resp_done_hnd_t req_resp_sent_hnd)

Provide a high level ping API.

Parameters
TypeDirectionArgument NameDescription
const sockaddr_in6_t *const[in]remote_addr

Remote destination address

const uint16_t[in]packet_count

Count of packets

const uint16_t[in]packet_length

ICMPv6 packet length including header

sl_wisun_ping_stat_hnd_t[in]stat_hnd

Custom statistic handler function

sl_wisun_ping_req_resp_done_hnd_t[in]req_resp_sent_hnd

Request/Response sent handler function

The function provides an interface for periodically sending and receiving ping ICMPv6 packets, and collecting statistic data. Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL or SL_STATUS_ABORT


sl_wisun_ping_init#

void sl_wisun_ping_init (void )

Initialize the ping service module.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function initializes the service thread, mutex, and message queues.


sl_wisun_ping_request#

void sl_wisun_ping_request (const sl_wisun_ping_info_t *const ping_request)

Send a ping request.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_ping_info_t *const[in]ping_request

Ping Request Information

The function sends a single ICMPv6 request.


sl_wisun_ping_response#

void sl_wisun_ping_response (sl_wisun_ping_info_t *const ping_response)

Retrieve a ping response.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_ping_info_t *const[out]ping_response

Ping Response Information

The function retrieves a ping response information.


sl_wisun_ping_stop#

void sl_wisun_ping_stop (void )

Stop the current ping process.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Reset request and response queues and send a special ping request with interrupt ping status.