Socket API#

Socket API provides socket-based networking functions for IPv6 connectivity, closely aligning with the POSIX.1-2024 specification.

Modules#

cmsghdr

in6_addr

in6_pktinfo

iovec

ip6_mtuinfo

ipv6_mreq

msghdr

sockaddr

sockaddr_in6

IPv6 socket options#

IPv6 socket options summaryopt_name Data type set/getsockopt sendmsg recvmsg IPV6_TCLASS int Set/Get Yes No IPV6_UNICAST_HOPS int Set/Get No No IPV6_MULTICAST_HOPS int Set/Get No No IPV6_USE_MIN_MTU int Set/Get Yes No IPV6_HOPLIMIT int None Yes Yes IPV6_RECVHOPLIMIT int Set/Get No No IPV6_MULTICAST_LOOP int Set/Get Yes No IPV6_JOIN_GROUP ipv6_mreq_t Set only No No IPV6_ADD_MEMBERSHIP ipv6_mreq_t Set only No No IPV6_LEAVE_GROUP ipv6_mreq_t Set only No No IPV6_DROP_MEMBERSHIP ipv6_mreq_t Set only No No IPV6_PKTINFO in6_pktinfo_t None Yes Yes IPV6_RCVPKTINFO int Set/Get No No IPV6_RECVTCLASS int Set/Get No No IPV6_DONTFRAG int Set/Get Yes No

#define

Sets or reads the full 8-bit IPv6 Traffic Class (RFC 3542 section 6.5), as int.

#define

Set the unicast hop limit for the socket, as int.

#define

Set the multicast hop limit for the socket, as int.

#define

Specify PMTU preference, as int; Valid values -1 (PMTUD for unicast, default), 0 (PMTUD always), 1 (PMTUD off).

#define

Ancillary data option on sendmsg()/recvmsg(), value to be used for single ongoing packet, as int; Valid values 0-255, -1 for default.

#define

Ancillary data option on recvmsg(), specifies hop-limit for the single received ongoing packet, as int; A nonzero value enables the option; a value of 0 disables the option.

#define

Specify whether outgoing multicast packets are looped back, as int.

#define

Join a multicast group.

#define
IPV6_JOIN_GROUP IPV6_ADD_MEMBERSHIP

Sets or reads the full 8-bit IPv6 Traffic Class (RFC 3542 section 6.5), as int.

#define

Leave a multicast group.

#define
IPV6_LEAVE_GROUP IPV6_DROP_MEMBERSHIP

Sets or reads the full 8-bit IPv6 Traffic Class (RFC 3542 section 6.5), as int.

#define

Specify control messages packet info for recvmsg() as struct in6_pktinfo.

#define

Set delivery of the IPV6_PKTINFO control message on incoming datagrams, as int.

#define

Enables the application to receive the value of the traffic class field from the IPv6 header, as int; A nonzero value enables the option; a value of 0 disables the option.

#define

Specify not to fragment datagrams, as int; For Wi-SUN, direct neighbors can receive frames up to 1504 bytes, while the other nodes can receive frames up to 1280 bytes.

Differentiated Services Code Points (DSCP) — IANA assigned values#

These are the raw code-point values; combine with IPV6_TCLASS_FROM_DSCP or IPV6_TCLASS_FROM_DSCP_AND_ECN to obtain a Traffic Class octet suitable for use with IPV6_TCLASS.

#define
#define
#define

AF11.

#define

AF12.

#define

AF13.

#define

CS2.

#define

AF21.

#define

AF22.

#define

AF23.

#define

CS3.

#define

AF31.

#define

AF32.

#define

AF33.

#define

CS4.

#define

AF41.

#define

AF42.

#define

AF43.

#define

CS5.

#define

VOICE-ADMIT.

#define

EF.

#define

CS6.

#define

CS7.

Wi-SUN DSCP (Differentiated Services Code Point) QoS supported levels.#

#define
DSCP_DEFAULT IP_DSCP_CS0

Standard priority and it is socket default.

#define
DSCP_AF11 IP_DSCP_AF11

Application high priority service: Stack priorities these messages over the default priority messages.

#define
DSCP_EF IP_DSCP_EF

Expedited Forwarding (EF) QoS level enable high priority state: low loss, low delay, and low jitter services.

Explicit Congestion Notification (ECN) code points (RFC 3168)#

Two-bit ECN values occupying bits 1-0 of the IPv6 Traffic Class octet (and the equivalent IPv4 ToS field).

#define

Not ECN-Capable Transport.

#define

ECN-Capable Transport(1)

#define

ECN-Capable Transport(0)

#define

Congestion Experienced.

IPv6 Traffic Class byte (RFC 3542 section 6.5)#

The IPv6 Traffic Class is an 8-bit field placed in the IPv6 header: DSCP (Differentiated Services Code Point, RFC 2474) occupies bits 7-2 and ECN (Explicit Congestion Notification, RFC 3168) bits 1-0.Use IPV6_TCLASS_FROM_DSCP or IPV6_TCLASS_FROM_DSCP_AND_ECN to build a Traffic Class octet from a DSCP code point (0-63), and IPV6_DSCP_FROM_TCLASS for the inverse.These helpers are a Wi-SUN extension to RFC 3542; they live here because they manipulate the Traffic Class field of the IPv6 header.

#define

Six-bit DSCP code point (0-63).

#define

Six-bit DSCP code point (0-63).

#define

Six-bit DSCP code point (0-63).

#define

Traffic Class octet from DSCP code point and ECN Not-ECT.

#define

Traffic Class octet from DSCP code point (ECN Not-ECT)

#define

DSCP code point (0-63) from a full RFC 3542 Traffic Class octet (inverse of IPV6_TCLASS_FROM_DSCP).

Ancillary data object information MACROS#

#define

Returns the length of the data with the required alignment.

#define

Returns the number of bytes an ancillary element with payload of the passed data length occupies.

#define
CMSG_LEN (len)

Returns the value to store in the cmsg_len member of the cmsghdr structure.

#define

Returns a pointer to the first control message header in the given msghdr structure.

#define
CMSG_NXTHDR (mhdr, cmsg)

Returns a pointer to the next control message header in the ancillary data buffer.

#define
CMSG_DATA (cmsg)

Returns a pointer to the data portion of a cmsghdr.

Flags we can use with recv(), recvfrom() and recvmsg()#

#define
MSG_TRUNC 0x0001

Normal data truncated, to be used as msg_flags field in the msghdr structure.

#define
MSG_CTRUNC 0x0002

Control data truncated, to be used as msg_flags field in the msghdr structure.

#define
MSG_PEEK 0x0004

Leave received data in queue, to be used as the flags parameter.

Protocol levels used for socket_setsockopt.#

#define

Socket option level.

#define

Application socket option level.

application level socket options#

application level socket options summaryopt_name data type set/get sendmsg recvmsg SO_EVENT_MODE uint32_t Set only No Yes SO_NONBLOCK uint32_t Set only Yes Yes

#define

Specify event mode of a socket. When set, optval must point to an uint32_t.

Possible values are:

#define
SOCKET_EVENT_MODE SO_EVENT_MODE

Specify event mode of a socket. When set, optval must point to an uint32_t.

Possible values are:

#define

Enable/disable nonblocking mode.

socket level options#

socket level options summaryopt_name data type set/get sendmsg recvmsg SO_RCVBUF int32_t Set/Get No Yes SO_SNDBUF int32_t Set/Get Yes No SO_REUSEADDR int32_t Set/Get No No SO_SNDLOWAT int32_t Set/Get Yes No SO_WRITABLE int32_t Get No No SO_READABLE int32_t Get No No

#define

Specify receive buffer size in payload bytes. When set, optval must point to an int32_t.

0 means unread data are dropped, unless read in data callback.

#define

Specify send buffer size in payload bytes.

#define

Allow reuse of local addresses on bind().

#define

Specify send low water mark in payload bytes.

#define

Non-standard POSIX option SO_WRITABLE.

#define

Non-standard POSIX option SO_READABLE.

Socket-level Wi-SUN extensions#

#define

Enable Extended Directed Frame Exchange mode. When set, optval must point to an uint32_t. When set, all data from the socket will be sent using the EDFE mode even if there is a single fragment. Disabled by default.

#define
SOCKET_EDFE_MODE SO_EDFE_MODE

Enable Extended Directed Frame Exchange mode. When set, optval must point to an uint32_t. When set, all data from the socket will be sent using the EDFE mode even if there is a single fragment. Disabled by default.

Enumerations#

enum
SL_WISUN_SOCKET_EVENT_MODE_INDICATION = 0
SL_WISUN_SOCKET_EVENT_MODE_POLLING = 1
}

Enumerations for socket event mode.

enum
AF_INET6 = 0
}

Supported address families.

enum
IPPROTO_IP = 0
IPPROTO_ICMP = 1
IPPROTO_TCP = 2
IPPROTO_UDP = 3
IPPROTO_IPV6 = 41
}

IP protocols (used as protocol argument to socket() and as level argument to setsockopt()/getsockopt() for protocol-level options).

enum
SOCK_INVALID = 0
SOCK_STREAM = 1
SOCK_DGRAM = 2
SOCK_RAW = 3
}

Socket types.

Typedefs#

typedef struct cmsghdr

Control messages.

typedef struct in6_addr

IPv6 Internet address.

typedef struct in6_pktinfo

Structure to store the IPv6 packet information.

typedef uint16_t

Transport layer port.

typedef struct iovec

Structure to store scatter/gather array elements.

typedef struct ip6_mtuinfo

Structure to store the IPv6 MTU (Maximum Transmission Unit) information.

typedef struct ipv6_mreq

Structure to specify the multicast group and the interface.

typedef struct msghdr

The msghdr structure is used by the recvmsg() and sendmsg() functions.

typedef uint32_t

Address family.

typedef enum socket_domain

Supported address families.

typedef enum socket_protocol

IP protocols (used as protocol argument to socket() and as level argument to setsockopt()/getsockopt() for protocol-level options).

typedef enum socket_type

Socket types.

typedef int
typedef struct sockaddr_in6

IPv6 address format.

typedef uint32_t

Socket address length type definition.

Variables#

IPv6 wildcard address.

Functions#

int
accept(int sockid, struct sockaddr *addr, socklen_t *addrlen)

Accept a connection on a socket.

int
bind(int sockid, const struct sockaddr *addr, socklen_t addrlen)

Bind a name to a socket.

int
close(int sockid)

Close a socket.

int
connect(int sockid, const struct sockaddr *addr, socklen_t addrlen)

Initiate a connection on a socket.

int
getpeername(int socket, struct sockaddr *restrict address, socklen_t *restrict address_len)

Get the address of the peer connected to the socket.

int
getsockname(int socket, struct sockaddr *restrict address, socklen_t *restrict address_len)

Retrieves the local address of a socket.

int
getsockopt(int sockid, int level, int optname, void *optval, socklen_t *optlen)

Get socket option.

int
listen(int sockid, int backlog)

Listen for connections on a socket.

ssize_t
recv(int sockid, void *buf, size_t len, int flags)

Receive a message from a socket.

ssize_t
recvfrom(int sockid, void *buf, size_t len, int flags, struct sockaddr *src_addr, socklen_t *addrlen)

Receive messages from a socket.

ssize_t
recvmsg(int socket, struct msghdr *message, int flags)

Receive a message from a socket.

ssize_t
send(int sockid, const void *buff, size_t len, int flags)

Send a message on a socket.

ssize_t
sendmsg(int socket, const struct msghdr *message, int flags)

Send a message through a connection-mode or connectionless-mode socket.

ssize_t
sendto(int sockid, const void *buff, size_t len, int flags, const struct sockaddr *dest_addr, socklen_t addr_len)

Send a message to a given address.

int
setsockopt(int sockid, int level, int optname, const void *optval, socklen_t optlen)

Set socket option designated by optname at a given protocol level to the value pointed by optval.

int
socket(int domain, int type, int protocol)

Create an endpoint for communication and returns an Id that refers to that endpoint.

Macros#

#define
APP_LEVEL_SOCKET SOL_APPLICATION

For backward compatibility.

#define
IN6ADDR_ANY_INIT { { 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0 } }

Initialization value for IPv6 wildcard address.

#define

Length of the string form for IPv6.

#define

Size of an IPv6 address.

#define
SOCK_NONBLOCK 0X00010000

When bitwise ored with socket's type, it sets the O_NONBLOCK status flag on the opened socket file description.

IPv6 socket options Documentation#

IPV6_TCLASS#

#define IPV6_TCLASS
Value:
1

Sets or reads the full 8-bit IPv6 Traffic Class (RFC 3542 section 6.5), as int.


IPV6_UNICAST_HOPS#

#define IPV6_UNICAST_HOPS
Value:
2

Set the unicast hop limit for the socket, as int.

Valid values 0 and 255, -1 for using the route default.


IPV6_MULTICAST_HOPS#

#define IPV6_MULTICAST_HOPS
Value:
3

Set the multicast hop limit for the socket, as int.

Valid values 0 and 255, -1 for using the route default.


IPV6_USE_MIN_MTU#

#define IPV6_USE_MIN_MTU
Value:
5

Specify PMTU preference, as int; Valid values -1 (PMTUD for unicast, default), 0 (PMTUD always), 1 (PMTUD off).


IPV6_HOPLIMIT#

#define IPV6_HOPLIMIT
Value:
8

Ancillary data option on sendmsg()/recvmsg(), value to be used for single ongoing packet, as int; Valid values 0-255, -1 for default.


IPV6_RECVHOPLIMIT#

#define IPV6_RECVHOPLIMIT
Value:
11

Ancillary data option on recvmsg(), specifies hop-limit for the single received ongoing packet, as int; A nonzero value enables the option; a value of 0 disables the option.


IPV6_MULTICAST_LOOP#

#define IPV6_MULTICAST_LOOP
Value:
14

Specify whether outgoing multicast packets are looped back, as int.

A nonzero value enables the option; a value of 0 disables the option.


IPV6_ADD_MEMBERSHIP#

#define IPV6_ADD_MEMBERSHIP
Value:
15

Join a multicast group.

Only valid for SOCK_DGRAM or SOCK_RAW sockets. When set, optval is a pointer to a struct ipv6_mreq.


IPV6_JOIN_GROUP#

#define IPV6_JOIN_GROUP
Value:
IPV6_ADD_MEMBERSHIP

Sets or reads the full 8-bit IPv6 Traffic Class (RFC 3542 section 6.5), as int.


IPV6_DROP_MEMBERSHIP#

#define IPV6_DROP_MEMBERSHIP
Value:
16

Leave a multicast group.

Only valid for SOCK_DGRAM or SOCK_RAW sockets. When set, optval is a pointer to a struct ipv6_mreq.


IPV6_LEAVE_GROUP#

#define IPV6_LEAVE_GROUP
Value:
IPV6_DROP_MEMBERSHIP

Sets or reads the full 8-bit IPv6 Traffic Class (RFC 3542 section 6.5), as int.


IPV6_PKTINFO#

#define IPV6_PKTINFO
Value:
9

Specify control messages packet info for recvmsg() as struct in6_pktinfo.


IPV6_RECVPKTINFO#

#define IPV6_RECVPKTINFO
Value:
10

Set delivery of the IPV6_PKTINFO control message on incoming datagrams, as int.

Such control messages contain a struct in6_pktinfo, as per RFC 3542. Allowed only for SOCK_DGRAM or SOCK_RAW sockets.


IPV6_RECVTCLASS#

#define IPV6_RECVTCLASS
Value:
12

Enables the application to receive the value of the traffic class field from the IPv6 header, as int; A nonzero value enables the option; a value of 0 disables the option.


IPV6_DONTFRAG#

#define IPV6_DONTFRAG
Value:
6

Specify not to fragment datagrams, as int; For Wi-SUN, direct neighbors can receive frames up to 1504 bytes, while the other nodes can receive frames up to 1280 bytes.

0 (fragment to path MTU). 1 (no fragmentation, TX fails if bigger than PMTU).


Differentiated Services Code Points (DSCP) — IANA assigned values Documentation#

IP_DSCP_CS0#

#define IP_DSCP_CS0
Value:
0

CS0.


IP_DSCP_CS1#

#define IP_DSCP_CS1
Value:
8

CS1.


IP_DSCP_AF11#

#define IP_DSCP_AF11
Value:
10

AF11.


IP_DSCP_AF12#

#define IP_DSCP_AF12
Value:
12

AF12.


IP_DSCP_AF13#

#define IP_DSCP_AF13
Value:
14

AF13.


IP_DSCP_CS2#

#define IP_DSCP_CS2
Value:
16

CS2.


IP_DSCP_AF21#

#define IP_DSCP_AF21
Value:
18

AF21.


IP_DSCP_AF22#

#define IP_DSCP_AF22
Value:
20

AF22.


IP_DSCP_AF23#

#define IP_DSCP_AF23
Value:
22

AF23.


IP_DSCP_CS3#

#define IP_DSCP_CS3
Value:
24

CS3.


IP_DSCP_AF31#

#define IP_DSCP_AF31
Value:
26

AF31.


IP_DSCP_AF32#

#define IP_DSCP_AF32
Value:
28

AF32.


IP_DSCP_AF33#

#define IP_DSCP_AF33
Value:
30

AF33.


IP_DSCP_CS4#

#define IP_DSCP_CS4
Value:
32

CS4.


IP_DSCP_AF41#

#define IP_DSCP_AF41
Value:
34

AF41.


IP_DSCP_AF42#

#define IP_DSCP_AF42
Value:
36

AF42.


IP_DSCP_AF43#

#define IP_DSCP_AF43
Value:
38

AF43.


IP_DSCP_CS5#

#define IP_DSCP_CS5
Value:
40

CS5.


IP_DSCP_VOICE_ADMIT#

#define IP_DSCP_VOICE_ADMIT
Value:
44

VOICE-ADMIT.


IP_DSCP_EF#

#define IP_DSCP_EF
Value:
46

EF.


IP_DSCP_CS6#

#define IP_DSCP_CS6
Value:
48

CS6.


IP_DSCP_CS7#

#define IP_DSCP_CS7
Value:
56

CS7.


Wi-SUN DSCP (Differentiated Services Code Point) QoS supported levels. Documentation#

DSCP_DEFAULT#

#define DSCP_DEFAULT
Value:
IP_DSCP_CS0

Standard priority and it is socket default.


DSCP_AF11#

#define DSCP_AF11
Value:
IP_DSCP_AF11

Application high priority service: Stack priorities these messages over the default priority messages.


DSCP_EF#

#define DSCP_EF
Value:
IP_DSCP_EF

Expedited Forwarding (EF) QoS level enable high priority state: low loss, low delay, and low jitter services.


Explicit Congestion Notification (ECN) code points (RFC 3168) Documentation#

IP_ECN_NOT_ECT#

#define IP_ECN_NOT_ECT
Value:
0

Not ECN-Capable Transport.


IP_ECN_ECT_1#

#define IP_ECN_ECT_1
Value:
1

ECN-Capable Transport(1)


IP_ECN_ECT_0#

#define IP_ECN_ECT_0
Value:
2

ECN-Capable Transport(0)


IP_ECN_CE#

#define IP_ECN_CE
Value:
3

Congestion Experienced.


IPv6 Traffic Class byte (RFC 3542 section 6.5) Documentation#

IPV6_TCLASS_DSCP_SHIFT#

#define IPV6_TCLASS_DSCP_SHIFT
Value:
2

Six-bit DSCP code point (0-63).


IPV6_TCLASS_ECN_MASK#

#define IPV6_TCLASS_ECN_MASK
Value:
0x03u

Six-bit DSCP code point (0-63).


IPV6_DSCP_CODEPOINT_MASK#

#define IPV6_DSCP_CODEPOINT_MASK
Value:
0x3Fu

Six-bit DSCP code point (0-63).


IPV6_TCLASS_FROM_DSCP_AND_ECN#

#define IPV6_TCLASS_FROM_DSCP_AND_ECN
Value:
((int)((((unsigned)(dscp) & IPV6_DSCP_CODEPOINT_MASK) << IPV6_TCLASS_DSCP_SHIFT) \
| ((unsigned)(ecn) & IPV6_TCLASS_ECN_MASK)))

Traffic Class octet from DSCP code point and ECN Not-ECT.


IPV6_TCLASS_FROM_DSCP#

#define IPV6_TCLASS_FROM_DSCP
Value:
(dscp)

Traffic Class octet from DSCP code point (ECN Not-ECT)


IPV6_DSCP_FROM_TCLASS#

#define IPV6_DSCP_FROM_TCLASS
Value:
(tclass)

DSCP code point (0-63) from a full RFC 3542 Traffic Class octet (inverse of IPV6_TCLASS_FROM_DSCP).


Ancillary data object information MACROS Documentation#

CMSG_ALIGN#

#define CMSG_ALIGN
Value:
(len)

Returns the length of the data with the required alignment.

Returns

  • The aligned length of the data, rounded up to the nearest multiple of uint32_t


CMSG_SPACE#

#define CMSG_SPACE
Value:
(len)

Returns the number of bytes an ancillary element with payload of the passed data length occupies.

Returns

  • The size of the control message structure plus the aligned data length


CMSG_LEN#

#define CMSG_LEN
Value:
(len)

Returns the value to store in the cmsg_len member of the cmsghdr structure.

Returns

  • The size of the control message structure plus the data length


CMSG_FIRSTHDR#

#define CMSG_FIRSTHDR
Value:
((mhdr)->msg_controllen >= sizeof(struct cmsghdr) ? \
(struct cmsghdr *)(mhdr)->msg_control : \
(struct cmsghdr *) NULL)

Returns a pointer to the first control message header in the given msghdr structure.

Returns

  • A pointer to the first cmsghdr structure, or NULL if the buffer is empty or invalid


CMSG_NXTHDR#

#define CMSG_NXTHDR
Value:
(mhdr, cmsg)

Returns a pointer to the next control message header in the ancillary data buffer.

Returns

  • A pointer to the next cmsghdr structure, or NULL if there is no more space left in the buffer


CMSG_DATA#

#define CMSG_DATA
Value:
(cmsg)

Returns a pointer to the data portion of a cmsghdr.

Returns

  • A pointer to the data following the cmsghdr, casted to uint8_t *


Flags we can use with recv(), recvfrom() and recvmsg() Documentation#

MSG_TRUNC#

#define MSG_TRUNC
Value:
0x0001

Normal data truncated, to be used as msg_flags field in the msghdr structure.


MSG_CTRUNC#

#define MSG_CTRUNC
Value:
0x0002

Control data truncated, to be used as msg_flags field in the msghdr structure.


MSG_PEEK#

#define MSG_PEEK
Value:
0x0004

Leave received data in queue, to be used as the flags parameter.


Protocol levels used for socket_setsockopt. Documentation#

SOL_SOCKET#

#define SOL_SOCKET
Value:
0

Socket option level.


SOL_APPLICATION#

#define SOL_APPLICATION
Value:
1

Application socket option level.


application level socket options Documentation#

SO_EVENT_MODE#

#define SO_EVENT_MODE
Value:
10

Specify event mode of a socket. When set, optval must point to an uint32_t.

Possible values are:


SOCKET_EVENT_MODE#

#define SOCKET_EVENT_MODE
Value:
SO_EVENT_MODE

Specify event mode of a socket. When set, optval must point to an uint32_t.

Possible values are:


SO_NONBLOCK#

#define SO_NONBLOCK
Value:
11

Enable/disable nonblocking mode.

This option takes an uint32_t value.

Possible values are:

  • (1) enables nonblocking mode

  • (0) disables nonblocking mode


socket level options Documentation#

SO_RCVBUF#

#define SO_RCVBUF
Value:
1

Specify receive buffer size in payload bytes. When set, optval must point to an int32_t.

0 means unread data are dropped, unless read in data callback.


SO_SNDBUF#

#define SO_SNDBUF
Value:
2

Specify send buffer size in payload bytes.

When set, optval must point to an int32_t.

Used only for stream sockets.


SO_REUSEADDR#

#define SO_REUSEADDR
Value:
3

Allow reuse of local addresses on bind().

When set, optval must point to an int32_t. Defaults to 0 (disabled).

Must be set before bind().

Behavior follows the table below (socketA is already bound, socketB is calling bind() and SO_REUSEADDR is set for this latter one):

socketA (bound)     socketB (binding)   SO_REUSEADDR   Result
----------------------------------------------------------------
[2001:db8::1]:21    [2001:db8::1]:21    ON / OFF       EADDRINUSE
[2001:db8::1]:21    [2001:db8::2]:21    ON / OFF       OK
[::]:21             [2001:db8::1]:21    OFF            EADDRINUSE
[2001:db8::1]:21    [::]:21             OFF            EADDRINUSE
[::]:21             [2001:db8::1]:21    ON             OK
[2001:db8::1]:21    [::]:21             ON             OK
[::]:21             [::]:21             ON / OFF       EADDRINUSE

For TCP, a socket in TIME_WAIT does not prevent bind() when SO_REUSEADDR is enabled.


SO_SNDLOWAT#

#define SO_SNDLOWAT
Value:
4

Specify send low water mark in payload bytes.

When set, optval must point to an int32_t.


SO_WRITABLE#

#define SO_WRITABLE
Value:
5

Non-standard POSIX option SO_WRITABLE.

This option returns a non-zero value (amount of free space in bytes) if the socket is writable.

A socket is considered writable if: The number of bytes of available space in the socket send buffer is greater than or equal the current size of the send low-water mark and either: The socket is connected (TCP). The socket does not require a connection (e.g., UDP).

Returns

  • Non-zero value (amount of free space in bytes) if the socket is readable, 0 otherwise.


SO_READABLE#

#define SO_READABLE
Value:
6

Non-standard POSIX option SO_READABLE.

This option returns a non-zero value (amount of available bytes) if the socket is readable. A socket is considered readable under the following conditions:

The number of bytes of data in the socket receive buffer is greater than or equal to the current size of the recv low-water mark. The default is 1 for TCP and UDP. The read half of the connection is closed (i.e., a TCP connection that has received a FIN). The socket is a listening socket and the number of completed connections is nonzero.

Returns

  • Non-zero value (amount of data in bytes) if the socket is readable, 0 otherwise.


Socket-level Wi-SUN extensions Documentation#

SO_EDFE_MODE#

#define SO_EDFE_MODE
Value:
0xfb

Enable Extended Directed Frame Exchange mode. When set, optval must point to an uint32_t. When set, all data from the socket will be sent using the EDFE mode even if there is a single fragment. Disabled by default.


SOCKET_EDFE_MODE#

#define SOCKET_EDFE_MODE
Value:
SO_EDFE_MODE

Enable Extended Directed Frame Exchange mode. When set, optval must point to an uint32_t. When set, all data from the socket will be sent using the EDFE mode even if there is a single fragment. Disabled by default.


Enumeration Documentation#

sl_wisun_socket_event_mode_t#

sl_wisun_socket_event_mode_t

Enumerations for socket event mode.

Enumerator
SL_WISUN_SOCKET_EVENT_MODE_INDICATION

SL_WISUN_MSG_SOCKET_DATA_IND_ID is sent to the app with the packet contained in the indication.

SL_WISUN_SOCKET_EVENT_MODE_POLLING

SL_WISUN_MSG_SOCKET_DATA_AVAILABLE_IND_ID is sent to the app indicating the amount of data received recv() or recvfrom() should be invoked after indication reception to retrieve data This is the default socket event mode option.


socket_domain#

socket_domain

Supported address families.

Enumerator
AF_INET6

IP version 6.


socket_protocol#

socket_protocol

IP protocols (used as protocol argument to socket() and as level argument to setsockopt()/getsockopt() for protocol-level options).

Enumerator
IPPROTO_IP

Dummy protocol.

IPPROTO_ICMP

Internet Control Message Protocol.

IPPROTO_TCP

Transmission Control Protocol.

IPPROTO_UDP

User Datagram Protocol.

IPPROTO_IPV6

IPv6 socket option level.


socket_type#

socket_type

Socket types.

Enumerator
SOCK_INVALID

invalid socket type

SOCK_STREAM

stream (connection) socket (TCP)

SOCK_DGRAM

datagram (connectionless) socket (UDP)

SOCK_RAW

raw socket


Typedef Documentation#

cmsghdr_t#

typedef struct cmsghdr cmsghdr_t

Control messages.


in6_addr_t#

typedef struct in6_addr in6_addr_t

IPv6 Internet address.


in6_pktinfo_t#

typedef struct in6_pktinfo in6_pktinfo_t

Structure to store the IPv6 packet information.


in_port_t#

typedef uint16_t in_port_t

Transport layer port.


iovec_t#

typedef struct iovec iovec_t

Structure to store scatter/gather array elements.


ip6_mtuinfo_t#

typedef struct ip6_mtuinfo ip6_mtuinfo_t

Structure to store the IPv6 MTU (Maximum Transmission Unit) information.


ipv6_mreq_t#

typedef struct ipv6_mreq ipv6_mreq_t

Structure to specify the multicast group and the interface.


msghdr_t#

typedef struct msghdr msghdr_t

The msghdr structure is used by the recvmsg() and sendmsg() functions.


sa_family_t#

typedef uint32_t sa_family_t

Address family.


sl_socket_domain_t#

typedef enum socket_domain sl_socket_domain_t

Supported address families.


sl_socket_protocol_t#

typedef enum socket_protocol sl_socket_protocol_t

IP protocols (used as protocol argument to socket() and as level argument to setsockopt()/getsockopt() for protocol-level options).


sl_socket_type_t#

typedef enum socket_type sl_socket_type_t

Socket types.


sl_wisun_socket_id_t#

typedef int sl_wisun_socket_id_t

Socket id.


sockaddr_in6_t#

typedef struct sockaddr_in6 sockaddr_in6_t

IPv6 address format.


socklen_t#

typedef uint32_t socklen_t

Socket address length type definition.


Variable Documentation#

in6addr_any#

const in6_addr_t in6addr_any

IPv6 wildcard address.


Function Documentation#

accept#

int accept (int sockid, struct sockaddr * addr, socklen_t * addrlen)

Accept a connection on a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket descriptor

struct sockaddr *[inout]addr

A pointer to sockaddr structure filled in with the address of the peer (remote) socket. When addr is NULL, nothing is filled in; in this case, addrlen is not used, and should also be NULL.

socklen_t *[inout]addrlen

The caller must initialize it to contain the size (in bytes) of the structure pointed to by addr. On return it will contain the actual size of the peer address.

Returns

  • The socket id of the accepted socket on success, -1 if an error occurred.

Used with connection-based socket types (TCP). It extracts the first connection request on the queue of pending connections for the listening socket.


bind#

int bind (int sockid, const struct sockaddr * addr, socklen_t addrlen)

Bind a name to a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket id

const struct sockaddr *[in]addr

address structure ptr

socklen_t[in]addrlen

address structure size

Returns

  • 0 on success, -1 on failure.

Assigns the address to the socket, referred to by the socket ID, as specified by addr. It is normally necessary to assign a local address using bind() before a SOCK_STREAM socket may receive connections.


close#

int close (int sockid)

Close a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket id

Returns

  • 0 on success, -1 on failure.

Close a socket and remove from the socket handler storage.


connect#

int connect (int sockid, const struct sockaddr * addr, socklen_t addrlen)

Initiate a connection on a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket descriptor.

const struct sockaddr *[in]addr

If the socket sockid is of type SOCK_DGRAM, addr is the address to which datagrams are sent by default and the only address from which datagrams are received. If the socket is of type SOCK_STREAM, this call attempts to make a connection to the socket that is bound to the address specified by addr.

socklen_t[in]addrlen

length of the supplied sockaddr structure.

Returns

  • 0 on connection or binding success, -1 if an error occurred.

Connects the socket referred to by the sockid to the address specified by address.


getpeername#

int getpeername (int socket, struct sockaddr *restrict address, socklen_t *restrict address_len)

Get the address of the peer connected to the socket.

Parameters
TypeDirectionArgument NameDescription
int[in]socket

The socket file descriptor.

struct sockaddr *restrict[out]address

A pointer to a sockaddr structure where the peer's address will be stored.

socklen_t *restrict[inout]address_len

A pointer to a socklen_t variable that specifies the size of the 'address' structure.

This function retrieves the address of the peer connected to the specified socket. The peer's address is stored in the provided 'address' structure, and the length of the address is stored in 'address_len'.

Returns

  • 0 on success, -1 on failure and sets errno appropriately.


getsockname#

int getsockname (int socket, struct sockaddr *restrict address, socklen_t *restrict address_len)

Retrieves the local address of a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]socket

The socket descriptor.

struct sockaddr *restrict[out]address

A pointer to a struct sockaddr where the local address information will be stored.

socklen_t *restrict[inout]address_len

A pointer to a socklen_t variable that specifies the size of the address structure. Upon successful completion, it contains the actual size of the address data.

Returns

  • On success, returns zero. On failure, returns -1 and sets errno appropriately.

This function retrieves the local address associated with a socket. It populates the provided address structure with the local address information.


getsockopt#

int getsockopt (int sockid, int level, int optname, void * optval, socklen_t * optlen)

Get socket option.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket descriptor.

int[in]level

socket protocol level.

int[in]optname

Option name. Supported options:

void *[out]optval

option value structure pointer.

socklen_t *[in]optlen

size of the option value structure.

Returns

  • 0 on success, -1 if an error occurred.

The function gets socket option by optname, and copies option data to optval ptr.


listen#

int listen (int sockid, int backlog)

Listen for connections on a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket id

int[in]backlog

Argument defines the maximum length to which the queue of pending connections for sockid may grow. Not implemented for Wi-SUN, the connection queue size is always 1

Returns

  • 0 on success, -1 if an error occurred.

Marks the socket referred to by sockid as a passive socket, that is, as a socket that will be used to accept incoming connection requests using accept.


recv#

ssize_t recv (int sockid, void * buf, size_t len, int flags)

Receive a message from a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

descriptor of socket to receive the message from.

void *[out]buf

pointer to destination data buffer.

size_t[in]len

length of destination data buffer.

int[in]flags

flags to select type of message reception. Ignored in our implementation.

Returns

  • The number of bytes received on success, -1 if an error occurred.

Should be used for connection-oriented protocol (TCP)


recvfrom#

ssize_t recvfrom (int sockid, void * buf, size_t len, int flags, struct sockaddr * src_addr, socklen_t * addrlen)

Receive messages from a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

descriptor of socket to receive the message from.

void *[out]buf

pointer to destination data buffer.

size_t[in]len

length of destination data buffer.

int[in]flags

flags to select type of message reception. Ignored in our implementation.

struct sockaddr *[in]src_addr

pointer to a sockaddr structure in which the sending address is to be stored.

socklen_t *[in]addrlen

length of the supplied sockaddr structure.

Returns

  • The number of bytes received on success, -1 if an error occurred.

Receives data on a socket whether or not it is connection-oriented.


recvmsg#

ssize_t recvmsg (int socket, struct msghdr * message, int flags)

Receive a message from a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]socket

Specifies the socket file descriptor.

struct msghdr *[inout]message

Points to a msghdr structure, containing both the buffer to store the source address and the buffers for the incoming message.

int[in]flags

Specifies the type of message reception.

Returns

  • The number of bytes received on success, -1 if an error occurred.

This function is typically used with connectionless-mode sockets because it permits the application to retrieve the source address of received data.


send#

ssize_t send (int sockid, const void * buff, size_t len, int flags)

Send a message on a socket.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket descriptor.

const void *[in]buff

pointer to data buffer to send.

size_t[in]len

length of data buffer to send.

int[in]flags

flags to select send options. Ignored in our implementation.

Returns

  • The number of bytes sent on success, -1 if an error occurred.

Preferred with connection-oriented sockets (TCP).


sendmsg#

ssize_t sendmsg (int socket, const struct msghdr * message, int flags)

Send a message through a connection-mode or connectionless-mode socket.

Parameters
TypeDirectionArgument NameDescription
int[in]socket

Specifies the socket file descriptor.

const struct msghdr *[in]message

Points to a msghdr structure, containing both the destination address and the buffers for the outgoing message.

int[in]flags

Specifies the type of message transmission.

Returns

  • The number of bytes received on success, -1 if an error occurred.


sendto#

ssize_t sendto (int sockid, const void * buff, size_t len, int flags, const struct sockaddr * dest_addr, socklen_t addr_len)

Send a message to a given address.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket descriptor.

const void *[in]buff

pointer to data buffer to send.

size_t[in]len

length of data buffer to send.

int[in]flags

flags to select send options. Ignored in our implementation.

const struct sockaddr *[in]dest_addr

pointer to destination address buffer; Required for datagram sockets.

socklen_t[in]addr_len

length of destination address buffer.

Returns

  • The number of bytes sent on success, -1 if an error occurred.

Preferred in datagram mode (UDP).


setsockopt#

int setsockopt (int sockid, int level, int optname, const void * optval, socklen_t optlen)

Set socket option designated by optname at a given protocol level to the value pointed by optval.

Parameters
TypeDirectionArgument NameDescription
int[in]sockid

socket ID

int[in]level

protocol level at which the option resides. it could be:

int[in]optname

option name. it could be:

const void *[in]optval

Pointer to the socket option new value. The type of variable pointed by optval depends level and optname values.

socklen_t[in]optlen

Must be the size of the symbol pointed by optval.

Returns

  • 0 on success, -1 if an error occurred.

This function can set socket properties.


socket#

int socket (int domain, int type, int protocol)

Create an endpoint for communication and returns an Id that refers to that endpoint.

Parameters
TypeDirectionArgument NameDescription
int[in]domain

Specifies a communication domain. It selects the protocol family which will be used for communication. Must be set to AF_INET6 (IPv6 network socket)

int[in]type

The communication semantics It can be:

int[in]protocol

Specifies the particular protocol to be used. It can be:

Returns

  • The socket's id on success, (-1) on failure.


Macro Definition Documentation#

APP_LEVEL_SOCKET#

#define APP_LEVEL_SOCKET
Value:
SOL_APPLICATION

For backward compatibility.


IN6ADDR_ANY_INIT#

#define IN6ADDR_ANY_INIT
Value:
{ { 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0 } }

Initialization value for IPv6 wildcard address.


INET6_ADDRSTRLEN#

#define INET6_ADDRSTRLEN
Value:
46

Length of the string form for IPv6.


IPV6_ADDR_SIZE#

#define IPV6_ADDR_SIZE
Value:
16

Size of an IPv6 address.


SOCK_NONBLOCK#

#define SOCK_NONBLOCK
Value:
0X00010000

When bitwise ored with socket's type, it sets the O_NONBLOCK status flag on the opened socket file description.