Z-Wave SDK Version 8.0.1 - Release Notes (Mar 25, 2026)#
Simplicity SDK Version 2025.12.2
Z-Wave and Z-Wave Long Range SDK are designed to meet the demands of the future smart home and beyond, where increasing needs for more sensors and battery-operated devices require both long range and low power. Context-aware environments are the next evolution in the smart home market, and they require technologies that have been optimized specifically for these applications.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 8.0.1#
None.
Added in 8.0.0#
Addressing the increasing demands for low power in battery-operated devices, the Z-Wave stack is now implemented independently from the platform power state (e.g., energy modes: EM0, EM1, EM1P, EM2, EM3/EM4). This architectural improvement reduces overall stack power consumption during radio events by leveraging the EM1P power state during radio operations instead of EM1. Additionally, using
sl_power_managerAPIs from application code will no longer interfere with Z-Wave stack radio logic. For more details, refer to the Important Changes section.The Z-Wave Long Range TX output power algorithm is refactored. It now tracks independently all the Z-Wave Long Range end devices. It is backward-compatible with the previous algorithm.
The 9.6 kbps PHY is used only if an end device in the network is not able to operate at a higher modulation rate (40 kbps or 100 kbps).
API Changes#
Changed in 8.0.1#
None.
Changed in 8.0.0#
The
zpal_power_managermodule is removed from the Z-Wave Silicon Labs PAL. It is replaced by two entities:A new
zw_shutdown_managercomponent. This module is responsible for sending a never listening end device to the EM4 power state. Requirements can be added by the application to prevent that transition, similarly to thesl_power_managercomponent.In the
zpal_radioPAL layer, new APIszpal_radio_request_stay_awakeandzpal_radio_revoke_stay_awakehandle requests to maintain an RX radio state in the stack.
The Packet Trace Interface (PTI) enablement relies on the standard
sl_rail_util_pticomponent instead of specific Z-Wave stack APIs.
Bug Fixes#
Fixed in 8.0.1#
NLS Support will no longer be enabled by default. An optional component (zw_s2_nls_support) was introduced to enable Network Level Security (NLS) support advertisement in the KEX Report during S2 inclusion. This allows alpha testing of NLS while avoiding certification issues when the feature is not certified.
Fixed in 8.0.0#
Below are important bugs fixed in this release. For a complete list, refer to this section.
The previous Z-Wave Long Range TX output power algorithm had an issue in the low output power range. It would revert to transmitting at the maximum output power. The issue is addressed in the newer implementation.
The FL Device end device radio behavior was impacted negatively by the use of the
zpal_pm_stay_awake()API. It would prevent the Z-Wave stack from properly behaving and acknowledging beam events. With the power management refactoring, this is no longer a concern. The Z-Wave stack behaves independently from application power management decisions.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 8.0.1#
None.
Added in 8.0.0#
The Z-Wave stack is now independent from the power state of the platform, meaning that using sl_power_manager APIs will not interfere with Z-Wave stack logic. It improves the stack power consumption during radio events, leveraging the EM1P power state. Refer to Important Changes for additional information.
Note: This improvement has implications on the application. It is now responsible to keep the EFR32 host awake if required. The Z-Wave stack only handles the radio state.
Enhancements#
Added in 8.0.1#
None.
Added in 8.0.0#
The Z-Wave Long Range TX output power algorithm is refactored. It now tracks independently of all Z-Wave Long Range end devices. It is backward-compatible with the previous algorithm.
The 9.6 kbps PHY is used only if an end device in the network is not able to operate at a higher modulation rate (40 kbps or 100 kbps).
The function CC_Configuration_SetValue(), previously only declared without an implementation, has been implemented.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added in 8.0.1#
None.
Added in 8.0.0#
| New API Signature | Deprecated API replaced by this (if any) |
|---|---|
| CC_UserCredential_send_association_report | CC_UserCredential_AssociationReport_tx |
| ZW_DCDC_CONFIG1 | |
| ZW_EM4_PIN_RETENTION_MODE | SL_DEVICE_INIT_EMU_EM4_PIN_RETENTION_MODE |
| ZW_EM4_INITIAL_STATE | SL_DEVICE_INIT_EMU_EM4_STATE |
| ZW_EM23_VOLTAGE_SCALE | |
| ZW_EM4_RETAIN_LFXO | SL_DEVICE_INIT_EMU_EM4_RETAIN_LFXO |
| ZW_EM4_RETAIN_LFRCO | SL_DEVICE_INIT_EMU_EM4_RETAIN_LFRCO |
| ZW_EM4_RETAIN_ULFRCO | SL_DEVICE_INIT_EMU_EM4_RETAIN_ULFRCO |
| zw_shutdown_manager_add_lock |
|
| zw_shutdown_manager_take_temporary_lock |
|
| zw_shutdown_manager_release_lock |
|
| zw_shutdown_manager_init |
|
¹ The value of ZW_DCDC_CONFIG is currently not applied by the Z-Wave stack.
² The exact replacements for these Power Manager APIs depend on your use case:
For controlling the power state (i.e. EM state) of the ARM core, use the
sl_power_managerAPI.To maintain the Z-Wave radio in an active listening state during periods when the application itself is not transmitting, use the
zpal_radioAPI.To prevent the device from entering deep sleep mode, use the
zw_shutdown_managerAPI.
Note that the new lock behavior is significantly different from the previous Power Manager APIs.
For more details, refer to Important Changes and Migration Guide.
Modified APIs#
Modified in 8.0.1#
None.
Modified in 8.0.0#
| Old API | Modified API |
|---|---|
| zpal_tx_power_t | zpal_tx_power_decidbm_t |
| ZW_TX_POWER_10DBM | ZW_TX_POWER_100_DDBM |
| ZW_TX_POWER_14DBM | ZW_TX_POWER_140_DDBM |
| ZW_TX_POWER_20DBM | ZW_TX_POWER_200_DDBM |
| EZWAVECOMMANDSTATUS_GET_ROUTING_TABLE_LINE | EZWAVECOMMANDSTATUS_GET_NEIGHBOR_TABLE_LINE |
| EZWAVECOMMANDTYPE_GET_ROUTING_TABLE_LINE | EZWAVECOMMANDTYPE_GET_NEIGHBOR_TABLE_LINE |
| SUPPORT_GET_ROUTING_TABLE_LINE | SUPPORT_GET_NEIGHBOR_TABLE_LINE |
Removed APIs#
Removed in 8.0.1#
Removed API | Was Deprecated? |
|---|---|
cc_configuration_set_interface | No |
cc_configuration_set_default_configuration | No |
Removed in 8.0.0#
Removed API | Was Deprecated? |
|---|---|
zw_power_manager_is_active | No |
zw_power_manager_init | No |
zw_power_manager_lock | No |
zw_power_manager_relock | No |
zw_power_manager_lock_cancel | No |
zpal_get_max_timeout | No |
zpal_pm_lock_is_active | No |
zpal_pm_init | No |
zpal_pm_lock | No |
zpal_pm_relock | No |
zpal_pm_lock_cancel | No |
zpal_pm_halt | No |
zpal_pm_register_domain | No |
zpal_zw_pm_event_handler | No |
zpal_radio_debug_configure | No |
zpal_radio_is_debug_enabled | No |
EZWAVECOMMANDTYPE_ZW_GET_PTI_CONFIG | No |
EZWAVECOMMANDSTATUS_ZW_GET_PTI_CONFIG | No |
Deprecated APIs#
Deprecated in 8.0.1#
None.
Deprecated in 8.0.0#
Deprecated API | Planned Removal Date (if any) | Replacement API Name (if any) |
|---|---|---|
CC_UserCredential_send_association_report | TBD | CC_UserCredential_AssociationReport_tx |
Bug Fixes#
Fixed in 8.0.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1601943 | Fixed an issue when sometimes beam acknowledgement was not sent by the FL Device due to CSMA failure by disabling LBT for beam acknowledgement. | None | FL Devices, CSMA |
| 1581958 | Fixed an issue when Frequently Listening device stayed longer in RX due to beam from other network. | None | FL Devices |
| 1604659 | Fixed an issue where the Frequently Listening device did not wait for the end of the fragment to send the beam acknowledgement. | None | ZPAL radio, FL Devices |
| 1605316 | Fixed an end of fragment detection issue by reducing the grace period length. | None | FL Devices |
| 1605311 | Fixed an issue that prevented controllers from handling beam acknowledgement when only 1 fragment was remaining. | None | Z-Wave stack, Serial API controller |
| 1585554 | Restores the fragmented LR beam length to 3s (it was set to 2s from SDK version 7.20 onwards). The change had introduced a regression where FL Devices (configured for a 900ms wakeup period) would miss about 10% of the beams. | None | Z-Wave stack |
| 1569671 | Fixed an edge case when the FL device becomes unresponsive. | None | FL Devices |
| 1600768 | NLS Support was advertised in KEX Report for all end node firmwares since version 7.23.0, even when the feature was not certified. This could cause certification issues. Added optional component (zw_s2_nls_support) to allow users to choose whether to enable NLS support for alpha testing. | S2V2, end nodes | All Z-Wave applications |
| 1583202 | Fixed an issue when fragmented beam period exceeded 200 ms period. | None | FL Devices |
| 1577434 | Added a shutdown lock mechanism to prevent multiple calls to the shutdown manager. The lock is now checked before ANY release or add operations, ensuring proper state management during indicator control operations. | None | Never Listening devices |
| 1585383 | Fixed intermittent device resets before inclusion on Never Listening and Frequently Listening devices by adding command class ID checking. | None | Never Listening, FL Devices |
| 1590901 | Fixed LBT/CCA threshold values for 2CH regions (EU, US, ANZ, HK, IN, IL, RU, CN). | None | zpal_radio |
| 1595223 | Fixed incorrect Protocol Build Number reported in the Version Z-Wave Software Report message. | None | End Devices |
| 1581738 | Fixed an FL Device migration issue by adding automatic upgrade for RAIL PM initialization. | None | FL Devices |
| 1581963 | Resolved beam acknowledgement by fixing end-of-beam fragment detection. This improves the FL node response latency. Also, it fixed the PowerlevelCmdClassV1 CTT test. | None | FL Devices |
| 1556587 | Fixed endpoint handling in Multilevel Sensor Command Class: sensor types and scales are now correctly filtered per endpoint. Previously, the device incorrectly reported the same sensor capabilities across all endpoints (the properties of endpoint 0 were duplicated). New endpoint-aware functions (cc_multilevel_sensor_get_supported_sensors_by_endpoint and cc_multilevel_sensor_get_supported_scale_by_endpoint) are introduced while maintaining backward compatibility with existing code. | None | Multilevel Sensor Command Class |
Fixed in 8.0.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1542556 | Fixed an issue that prevented the modification of credential data via the CLI. All-zero PIN Code credentials (e.g. 0000) are now rejected by default. | None | ZAF / User Credential Command Class |
| 1525543 | Fixed lower limit of configuration ranges in CC Binary Switch duration, User Credential CC max credential slots, and minimum and maximum credential data length to allow values of 0. | None | ZAF / User Credential Command Class, Binary Switch Command Class |
| 1516742 | Fixed User Credential Association Reports not being advertised in the list of Lifeline notifications and not being sent to the required Lifeline destinations. | None | ZAF / User Credential Command Class |
| 1489288 | Fixed applications supporting the User Credential Command Class not reporting support for name encodings ASCII, Extended ASCII, and UTF-16. This applies changes from the 2025A specification. | None | ZAF / User Credential Command Class |
| 1488041 | A Credential Report with the status "Credential Unchanged" is now returned if no credentials are deleted after a bulk credential deletion request is received over the air. This applies changes from the 2025A specification. | None | ZAF / User Credential Command Class |
| 1480294 | Fixed the s_colorComponent structure to be compatible with the zaf_config_t. | None | ZAF / Color Switch Command Class |
| 1473325 | Slow refresh has been enabled by default in Central Scene V3 according to the specification. | None |
|
| 1432659 | Fixed an issue when too many reports are sent when multiple buttons are pressed at once. | None | All examples |
| 1556171 | Multilevel Sensor Command Class support has been extended to include all sensor types and scales defined by the specification. If auto-generating sources from .cc_config files fails, no error message is displayed. It is recommended to run the CC Configurator manually (see DevTools/cc_configurator/README). | None | Multilevel Sensor Command Class |
| 1490329 | User-defined configurations in SLC project files related to the Energy Management Unit had not been applied due to the Z-Wave stack initialization process overriding them with hard-coded values. These configurations are now configurable via the Z-Wave Core Component and applied correctly except for the DC/DC Converter Mode (ZW_DCDC_CONFIG), which is still hard-coded. | None | All examples |
| 1356409 | Fixed an issue where the Serial API controller would not acknowledge the "Initiate Shutdown" command. | SF case 00320844 | Serial API controller |
| 1298116 | The Serial API controller could mistake an Explorer Autoinclusion frame as an Application Frame, notifying the host with "junk" data. The packet is now properly handled. | SF case 00315326 | Serial API controller |
| 1390101 | Fixed an issue preventing the configuration of a TX output power above +14 dBm in the Serial API controller application. | None | ZPAL |
| 1516616 | Fixed an issue where the Z-Wave Long Range TX output power algorithm would transmit at maximum power while it was supposed to transmit at a negative TX power. | None | ZPAL radio |
| 1358615 | Addressed a behavior where a Frequently Listening device would not be able to acknowledge a beam when the zpal_pm_stay_awake() API was used. | SF case 00320854 | ZPAL |
| 378359 | Previously, KEX Fail messages were sent without being secure. They are now sent encrypted with the same level of encryption as the frame at that point of inclusion. The fix aligns with the behavior to the Z-Wave specification. | None | Z-Wave stack |
| 1325755 | Removed an unnecessary duplicate message during the S2 bootstrapping process when S2 Authenticated mode is used. | None | Z-Wave stack |
Chip Enablement#
None.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None.
Modified Examples#
Modified in 8.0.1#
None.
Modified in 8.0.0#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
zwave_soc_sensor_pir | Removed unused device init config: SL_DEVICE_INIT_LFXO_TIMEOUT | N/A |
|
| N/A |
All examples | The Energy Management Unit related configurations, previously set in the SLC project files, had been overridden by system_startup_core during the stack init phase. To maintain their visibility, they were moved to the configuration of the zw_core component in a new, hardware-specific header file. | N/A |
|
| N/A |
zwave_soc_sensor_pir, zwave_soc_multilevel_sensor | The Sensor PIR and Multilevel Sensor applications now support the S0 security scheme (Security Command Class V1). See Note below this table. | N/A |
|
| N/A |
Note: The S0 security scheme enablement is introduced regressions on the S0_InvalidNetworkKeySet_Rev01 and S0_SettingNewNetworkKey_Rev01 CTT tests. Currently, these are identified as test-related errors. Clarification is in progress with the Z-Wave Alliance and test house.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1568087 | The configuration value for DC/DC Converter Mode (ZW_DCDC_CONFIG) is not applied. | Currently not available. | All Z-Wave applications | |
| 1399709 | Reported S2 command class version remains 1 until certification covers S2v2. | Currently not available. | All Z-Wave applications | |
| 369430 | All S2 multicast frames are sent using verified delivery S2_TXOPTION_VERIFY_DELIVERY whether or not a response is expected. | Change source code depending on the frame sent. | ZAF | |
| 1067228 | Zniffer on BRD4204D does not detect LR wakeup beams. | Use different board for sniffing LR wakeup beams. | zwave_ncp_zniffer | |
| 1556296 | The never listening device type activity profile is modified during SmartStart inclusion. It results in improved power consumption when the device is not transmitting smart start frames but additional power consumption during the SmartStart communications (typically from 1.22 µA to 1.89 µA). | Never listening device type. | ||
| 1568316 | In regions that leverage fragmented beams (Japan, Korea, and Long Range), the acknowledgement from the Frequently Listening device can be sent at the end of the fragmented beam instead of when the first fragment is received. This results in an added delay for the end device to notify the beaming device. | Frequently Listening device type. | ||
| 1574930 | Wrong indexing in algorithm context led to wrong interpretation of network statistics and failure of the LR dynamic channel switch. | LR Devices | ||
| 1574455 | S2v2 alpha implementation allows for disabling NLS via NLS State Set command for experimenting with the alpha implementation. This is not allowed according to the Z-Wave specification and will be removed in the future GA implementation. | S2v2 alpha feature |
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
None.
Migration Guide#
Click here for the migration guide for deprecated, removed, and modified items.
Using This Release#
Installation and Use | Help and Feedback
Installation and Use#
To upgrade your existing software with this release, see instructions in the Migration Guide.
To run your first demo, see our Z-Wave Getting Started for End Devices.
To learn more about the software in this release, dive into our Z-Wave online documentation.
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note: Ask AI is experimental.
Get help from our developer community.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.