network-diagnostics API Callbacks
Functions |
|
| void | emberDiagnosticAnswerHandler ( EmberStatus status, const EmberIpv6Address *remoteAddress, const uint8_t *payload, uint16_t payloadLength) |
Application callback for
emberSendDiagnosticQuery()
and
emberSendDiagnosticGet()
.
|
|
| bool | emberBatteryLevelHandler (uint8_t *batteryLevel) |
|
Application callback for the stack to obtain the battery level to use in a response to a network diagnostic request. From the Thread spec: "The battery level is an 8-bit unsigned integer that indicates remaining battery energy in the Thread device as an integer percentage value 0-100 (0x00-0x64).".
|
|
| void | emberSetVendorTlvsReturn ( EmberStatus status, uint16_t length) |
Application callback for
emberSetVendorTlvs()
.
|
|
| void | emberManagementGetResponseHandler ( EmberCoapStatus status, EmberCoapCode code, EmberCoapReadOptions *options, uint8_t *payload, uint16_t payloadLength, EmberCoapResponseInfo *info) |
The response to a management get request previous sent via
emberSendManagementGetRequest()
.
|
|
Detailed Description
These callbacks were contributed by the network-diagnostics API.
Function Documentation
| bool emberBatteryLevelHandler | ( | uint8_t * |
batteryLevel
|
) |
- Parameters
-
batteryLevelThe battery level value to return to the stack.
This handler should return false if the battery level is not measured, unknown, or the device does not operate on battery power. If a valid battery level is being supplied, it must return true.
The application must define EMBER_APPLICATION_HAS_BATTERY_LEVEL_HANDLER in its CONFIGURATION_HEADER to use this.
This is an SOC-only API.
| void emberDiagnosticAnswerHandler | ( | EmberStatus |
status,
|
| const EmberIpv6Address * |
remoteAddress,
|
||
| const uint8_t * |
payload,
|
||
| uint16_t |
payloadLength
|
||
| ) |
- Parameters
-
statusStatus of the query result. remoteAddressThe remote address that sent the answer. payloadThe returned payload. payloadLengthThe returned payload length.
| void emberManagementGetResponseHandler | ( | EmberCoapStatus |
status,
|
| EmberCoapCode |
code,
|
||
| EmberCoapReadOptions * |
options,
|
||
| uint8_t * |
payload,
|
||
| uint16_t |
payloadLength,
|
||
| EmberCoapResponseInfo * |
info
|
||
| ) |
| void emberSetVendorTlvsReturn | ( | EmberStatus |
status,
|
| uint16_t |
length
|
||
| ) |
- Parameters
-
statusEMBER_SUCCESS if the supplied TLVs were valid and successfully installed, EMBER_BAD_ARGUMENT otherwise. See emberSetVendorTlvsfor validity requirements.lengthThe number of bytes in the supplied network data.