EmberZclCommandContext_t Struct Reference
#include <
zcl-core-types.h
>
Data Fields |
|
| EmberIpv6Address | remoteAddress |
| EmberCoapCode | code |
| const EmberCoapRequestInfo * | info |
| const uint8_t * | payload |
| uint16_t | payloadLength |
| EmberZclGroupId_t | groupId |
| EmberZclEndpointId_t | endpointId |
| const EmberZclClusterSpec_t * | clusterSpec |
| EmberZclCommandId_t | commandId |
This structure holds a command context.
Field Documentation
| const EmberZclClusterSpec_t * EmberZclCommandContext_t::clusterSpec |
A cluster specification of a command.
| EmberCoapCode EmberZclCommandContext_t::code |
CoAP code of a command.
| EmberZclCommandId_t EmberZclCommandContext_t::commandId |
A command identifier.
| EmberZclEndpointId_t EmberZclCommandContext_t::endpointId |
An endpoint identifier of a command.
| EmberZclGroupId_t EmberZclCommandContext_t::groupId |
A group identifier of a command.
| const EmberCoapRequestInfo * EmberZclCommandContext_t::info |
EZ-Mode needs access to the request info structure
| const uint8_t* EmberZclCommandContext_t::payload |
Payload of a command.
| uint16_t EmberZclCommandContext_t::payloadLength |
Payload length of a command.
| EmberIpv6Address EmberZclCommandContext_t::remoteAddress |
A remote address of a command.
The documentation for this struct was generated from the following file:
-
zcl-core-types.h