USB Device HID API
Description
USB Device HID API.
Data Structures |
|
| struct | sl_usbd_hid_callbacks_t |
|
HID callbacks.
|
|
Functions |
|
| sl_status_t | sl_usbd_hid_init (void) |
|
Initialize HID class.
|
|
| sl_status_t | sl_usbd_hid_create_instance (uint8_t subclass, uint8_t protocol, sl_usbd_hid_country_code_t country_code, uint16_t interval_in, uint16_t interval_out, bool ctrl_rd_en, sl_usbd_hid_callbacks_t *p_hid_callbacks, uint8_t *p_class_nbr) |
|
Add a new instance of the HID class.
|
|
| sl_status_t | sl_usbd_hid_add_to_configuration (uint8_t class_nbr, uint8_t config_nbr) |
|
Add the HID class instance to the USB device configuration (see Note #1).
|
|
| sl_status_t | sl_usbd_hid_is_enabled (uint8_t class_nbr, bool *p_enabled) |
|
Get the HID class enable state.
|
|
| sl_status_t | sl_usbd_hid_write_sync (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint16_t timeout, uint32_t *p_xfer_len) |
|
Send data to the host through the Interrupt IN endpoint.
|
|
| sl_status_t | sl_usbd_hid_read_sync (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint16_t timeout, uint32_t *p_xfer_len) |
|
Receive data from the host through the Interrupt OUT endpoint.
|
|
| sl_status_t | sl_usbd_hid_read_async (uint8_t class_nbr, void *p_buf, uint32_t buf_len, sl_usbd_hid_async_function_t async_fnct, void *p_async_arg) |
|
Receive data from the host through the Interrupt OUT endpoint.
|
|
| sl_status_t | sl_usbd_hid_write_async (uint8_t class_nbr, void *p_buf, uint32_t buf_len, sl_usbd_hid_async_function_t async_fnct, void *p_async_arg) |
|
Send data to the host through the Interrupt IN endpoint.
|
|
Macros |
|
| #define | SLI_USBD_HID_EXTERN extern |
| #define | SL_USBD_HID_SUBCLASS_NONE 0x00u |
| #define | SL_USBD_HID_SUBCLASS_BOOT 0x01u |
| #define | SL_USBD_HID_PROTOCOL_NONE 0x00u |
| #define | SL_USBD_HID_PROTOCOL_KBD 0x01u |
| #define | SL_USBD_HID_PROTOCOL_MOUSE 0x02u |
| #define | SL_USBD_HID_ITEM_LONG 0xFE |
| #define | SL_USBD_HID_ITEM_TYPE_MAIN 0x00 |
| #define | SL_USBD_HID_ITEM_TYPE_GLOBAL 0x04 |
| #define | SL_USBD_HID_ITEM_TYPE_LOCAL 0x08 |
| #define | SL_USBD_HID_ITEM_TYPE_RESERVED 0x0C |
| #define | SL_USBD_HID_MAIN_INPUT 0x80 |
| #define | SL_USBD_HID_MAIN_OUTPUT 0x90 |
| #define | SL_USBD_HID_MAIN_COLLECTION 0xA0 |
| #define | SL_USBD_HID_MAIN_FEATURE 0xB0 |
| #define | SL_USBD_HID_MAIN_ENDCOLLECTION 0xC0 |
| #define | SL_USBD_HID_MAIN_CONSTANT 0x01 |
| #define | SL_USBD_HID_MAIN_DATA 0x00 |
| #define | SL_USBD_HID_MAIN_VARIABLE 0x02 |
| #define | SL_USBD_HID_MAIN_ARRAY 0x00 |
| #define | SL_USBD_HID_MAIN_RELATIVE 0x04 |
| #define | SL_USBD_HID_MAIN_ABSOLUTE 0x00 |
| #define | SL_USBD_HID_MAIN_WRAP 0x08 |
| #define | SL_USBD_HID_MAIN_NOWRAP 0x00 |
| #define | SL_USBD_HID_MAIN_NONLINEAR 0x10 |
| #define | SL_USBD_HID_MAIN_LINEAR 0x00 |
| #define | SL_USBD_HID_MAIN_NOPREFERRED 0x20 |
| #define | SL_USBD_HID_MAIN_PREFERREDSTATE 0x00 |
| #define | SL_USBD_HID_MAIN_NULLSTATE 0x40 |
| #define | SL_USBD_HID_MAIN_NONULLPOSITION 0x00 |
| #define | SL_USBD_HID_MAIN_VOLATILE 0x80 |
| #define | SL_USBD_HID_MAIN_NONVOLATILE 0x00 |
| #define | SL_USBD_HID_MAIN_BUFFEREDBYTES 0x0100 |
| #define | SL_USBD_HID_MAIN_BITFIELD 0x0000 |
| #define | SL_USBD_HID_COLLECTION_PHYSICAL 0x00 |
| #define | SL_USBD_HID_COLLECTION_APPLICATION 0x01 |
| #define | SL_USBD_HID_COLLECTION_LOGICAL 0x02 |
| #define | SL_USBD_HID_COLLECTION_REPORT 0x03 |
| #define | SL_USBD_HID_COLLECTION_NAMEDARRAY 0x04 |
| #define | SL_USBD_HID_COLLECTION_USAGESWITCH 0x05 |
| #define | SL_USBD_HID_COLLECTION_USAGEMODIFIER 0x06 |
| #define | SL_USBD_HID_GLOBAL_USAGE_PAGE 0x04 |
| #define | SL_USBD_HID_GLOBAL_LOG_MIN 0x14 |
| #define | SL_USBD_HID_GLOBAL_LOG_MAX 0x24 |
| #define | SL_USBD_HID_GLOBAL_PHY_MIN 0x34 |
| #define | SL_USBD_HID_GLOBAL_PHY_MAX 0x44 |
| #define | SL_USBD_HID_GLOBAL_UNIT_EXPONENT 0x54 |
| #define | SL_USBD_HID_GLOBAL_UNIT 0x64 |
| #define | SL_USBD_HID_GLOBAL_REPORT_SIZE 0x74 |
| #define | SL_USBD_HID_GLOBAL_REPORT_ID 0x84 |
| #define | SL_USBD_HID_GLOBAL_REPORT_COUNT 0x94 |
| #define | SL_USBD_HID_GLOBAL_PUSH 0xA4 |
| #define | SL_USBD_HID_GLOBAL_POP 0xB4 |
| #define | SL_USBD_HID_LOCAL_USAGE 0x08 |
| #define | SL_USBD_HID_LOCAL_USAGE_MIN 0x18 |
| #define | SL_USBD_HID_LOCAL_USAGE_MAX 0x28 |
| #define | SL_USBD_HID_LOCAL_DESIGNATOR_INDEX 0x38 |
| #define | SL_USBD_HID_LOCAL_DESIGNATOR_MIN 0x48 |
| #define | SL_USBD_HID_LOCAL_DESIGNATOR_MAX 0x58 |
| #define | SL_USBD_HID_LOCAL_STRING_INDEX 0x78 |
| #define | SL_USBD_HID_LOCAL_STRING_MIN 0x88 |
| #define | SL_USBD_HID_LOCAL_STRING_MAX 0x98 |
| #define | SL_USBD_HID_LOCAL_DELIMITER 0xA8 |
| #define | SL_USBD_HID_BIAS_NOT_APPLICABLE 0 |
| #define | SL_USBD_HID_BIAS_RIGHT_HAND 1 |
| #define | SL_USBD_HID_BIAS_LEFT_HAND 2 |
| #define | SL_USBD_HID_BIAS_BOTH_HANDS 3 |
| #define | SL_USBD_HID_BIAS_EITHER_HAND 4 |
| #define | SL_USBD_HID_DESIGNATOR_NONE 0x00 |
| #define | SL_USBD_HID_DESIGNATOR_HAND 0x01 |
| #define | SL_USBD_HID_DESIGNATOR_EYEBALL 0x02 |
| #define | SL_USBD_HID_DESIGNATOR_EYEBROW 0x03 |
| #define | SL_USBD_HID_DESIGNATOR_EYELID 0x04 |
| #define | SL_USBD_HID_DESIGNATOR_EAR 0x05 |
| #define | SL_USBD_HID_DESIGNATOR_NOSE 0x06 |
| #define | SL_USBD_HID_DESIGNATOR_MOUTH 0x07 |
| #define | SL_USBD_HID_DESIGNATOR_UPPER_LIP 0x08 |
| #define | SL_USBD_HID_DESIGNATOR_LOWER_LIP 0x09 |
| #define | SL_USBD_HID_DESIGNATOR_JAW 0x0A |
| #define | SL_USBD_HID_DESIGNATOR_NECK 0x0B |
| #define | SL_USBD_HID_DESIGNATOR_UPPER_ARM 0x0C |
| #define | SL_USBD_HID_DESIGNATOR_ELBOW 0x0D |
| #define | SL_USBD_HID_DESIGNATOR_FOREARM 0x0E |
| #define | SL_USBD_HID_DESIGNATOR_WRIST 0x0F |
| #define | SL_USBD_HID_DESIGNATOR_PALM 0x10 |
| #define | SL_USBD_HID_DESIGNATOR_THUMB 0x11 |
| #define | SL_USBD_HID_DESIGNATOR_INDEX_FINGER 0x12 |
| #define | SL_USBD_HID_DESIGNATOR_MIDDLE_FINGER 0x13 |
| #define | SL_USBD_HID_DESIGNATOR_RING_FINGER 0x14 |
| #define | SL_USBD_HID_DESIGNATOR_LITTLE_FINGER 0x15 |
| #define | SL_USBD_HID_DESIGNATOR_HEAD 0x16 |
| #define | SL_USBD_HID_DESIGNATOR_SHOULDER 0x17 |
| #define | SL_USBD_HID_DESIGNATOR_HIP 0x18 |
| #define | SL_USBD_HID_DESIGNATOR_WAIST 0x19 |
| #define | SL_USBD_HID_DESIGNATOR_THIGH 0x1A |
| #define | SL_USBD_HID_DESIGNATOR_KNEE 0x1B |
| #define | SL_USBD_HID_DESIGNATOR_CALF 0x1C |
| #define | SL_USBD_HID_DESIGNATOR_ANKLE 0x1D |
| #define | SL_USBD_HID_DESIGNATOR_FOOT 0x1E |
| #define | SL_USBD_HID_DESIGNATOR_HEEL 0x1F |
| #define | SL_USBD_HID_DESIGNATOR_BALL_OF_FOOT 0x20 |
| #define | SL_USBD_HID_DESIGNATOR_BIG_TOE 0x21 |
| #define | SL_USBD_HID_DESIGNATOR_SECOND_TOE 0x22 |
| #define | SL_USBD_HID_DESIGNATOR_THIRD_TOE 0x23 |
| #define | SL_USBD_HID_DESIGNATOR_FOURTH_TOE 0x24 |
| #define | SL_USBD_HID_DESIGNATOR_LITTLE_TOE 0x25 |
| #define | SL_USBD_HID_DESIGNATOR_BROW 0x26 |
| #define | SL_USBD_HID_DESIGNATOR_CHEEK 0x27 |
| #define | SL_USBD_HID_QUALIFIER_NOT_APPLICABLE 0 |
| #define | SL_USBD_HID_QUALIFIER_RIGHT 1 |
| #define | SL_USBD_HID_QUALIFIER_LEFT 2 |
| #define | SL_USBD_HID_QUALIFIER_BOTH 3 |
| #define | SL_USBD_HID_QUALIFIER_EITHER 4 |
| #define | SL_USBD_HID_QUALIFIER_CENTER 5 |
| #define | SL_USBD_HID_USAGE_PAGE_UNDEFINED 0x00 |
| #define | SL_USBD_HID_USAGE_PAGE_GENERIC_DESKTOP_CONTROLS 0x01 |
| #define | SL_USBD_HID_USAGE_PAGE_SIMULATION_CONTROLS 0x02 |
| #define | SL_USBD_HID_USAGE_PAGE_VR_CONTROLS 0x03 |
| #define | SL_USBD_HID_USAGE_PAGE_SPORT_CONTROLS 0x04 |
| #define | SL_USBD_HID_USAGE_PAGE_GAME_CONTROLS 0x05 |
| #define | SL_USBD_HID_USAGE_PAGE_GENERIC_DEVICE_CONTROLS 0x06 |
| #define | SL_USBD_HID_USAGE_PAGE_KEYBOARD 0x07 |
| #define | SL_USBD_HID_USAGE_PAGE_LEDS 0x08 |
| #define | SL_USBD_HID_USAGE_PAGE_BUTTON 0x09 |
| #define | SL_USBD_HID_USAGE_PAGE_ORDINAL 0x0A |
| #define | SL_USBD_HID_USAGE_PAGE_TELEPHONY 0x0B |
| #define | SL_USBD_HID_USAGE_PAGE_CONSUMER 0x0C |
| #define | SL_USBD_HID_USAGE_PAGE_DIGITIZER 0x0D |
| #define | SL_USBD_HID_USAGE_PAGE_PID_PAGE 0x0F |
| #define | SL_USBD_HID_USAGE_PAGE_UNICODE 0x10 |
| #define | SL_USBD_HID_USAGE_PAGE_ALPHANUMERIC_DISPLAY 0x14 |
| #define | SL_USBD_HID_USAGE_PAGE_MEDICAL_INSTRUMENTS 0x40 |
| #define | SL_USBD_HID_USAGE_PAGE_MONITOR_0 0x80 |
| #define | SL_USBD_HID_USAGE_PAGE_MONITOR_1 0x81 |
| #define | SL_USBD_HID_USAGE_PAGE_MONITOR_2 0x82 |
| #define | SL_USBD_HID_USAGE_PAGE_MONITOR_3 0x83 |
| #define | SL_USBD_HID_USAGE_PAGE_POWER_0 0x84 |
| #define | SL_USBD_HID_USAGE_PAGE_POWER_1 0x85 |
| #define | SL_USBD_HID_USAGE_PAGE_POWER_2 0x86 |
| #define | SL_USBD_HID_USAGE_PAGE_POWER_3 0x87 |
| #define | SL_USBD_HID_USAGE_PAGE_BAR_CODE_SCANNER_PAGE 0x8C |
| #define | SL_USBD_HID_USAGE_PAGE_SCALE_PAGE 0x8D |
| #define | SL_USBD_HID_USAGE_PAGE_MSR_DEVICES 0x8E |
| #define | SL_USBD_HID_USAGE_PAGE_POINT_OF_SALE_PAGES 0x8F |
| #define | SL_USBD_HID_USAGE_PAGE_CAMERA_CONTROL_PAGE 0x90 |
| #define | SL_USBD_HID_USAGE_PAGE_ARCADE_PAGE 0x91 |
| #define | SL_USBD_HID_CP_POINTER 0x01 |
| #define | SL_USBD_HID_CA_MOUSE 0x02 |
| #define | SL_USBD_HID_CA_JOYSTICK 0x04 |
| #define | SL_USBD_HID_CA_GAME_PAD 0x05 |
| #define | SL_USBD_HID_CA_KEYBOARD 0x06 |
| #define | SL_USBD_HID_CA_KEYPAD 0x07 |
| #define | SL_USBD_HID_CA_MULTI_AXIS_CONTROLLER 0x08 |
| #define | SL_USBD_HID_DV_X 0x30 |
| #define | SL_USBD_HID_DV_Y 0x31 |
| #define | SL_USBD_HID_DV_Z 0x32 |
| #define | SL_USBD_HID_DV_WHEEL 0x38 |
| #define | SL_USBD_HID_CA_SYSTEM_CONTROL 0x80 |
Typedefs |
|
| typedef void(* | sl_usbd_hid_async_function_t ) (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint32_t xfer_len, void *p_callback_arg, sl_status_t status) |
|
Async comm callback.
|
|
Enumerations |
|
| enum |
sl_usbd_hid_country_code_t
{
SL_USBD_HID_COUNTRY_CODE_NOT_SUPPORTED = 0u , SL_USBD_HID_COUNTRY_CODE_ARABIC = 1u , SL_USBD_HID_COUNTRY_CODE_BELGIAN = 2u , SL_USBD_HID_COUNTRY_CODE_CANADIAN_BILINGUAL = 3u , SL_USBD_HID_COUNTRY_CODE_CANADIAN_FRENCH = 4u , SL_USBD_HID_COUNTRY_CODE_CZECH_REPUBLIC = 5u , SL_USBD_HID_COUNTRY_CODE_DANISH = 6u , SL_USBD_HID_COUNTRY_CODE_FINNISH = 7u , SL_USBD_HID_COUNTRY_CODE_FRENCH = 8u , SL_USBD_HID_COUNTRY_CODE_GERMAN = 9u , SL_USBD_HID_COUNTRY_CODE_GREEK = 10u , SL_USBD_HID_COUNTRY_CODE_HEBREW = 11u , SL_USBD_HID_COUNTRY_CODE_HUNGARY = 12u , SL_USBD_HID_COUNTRY_CODE_INTERNATIONAL = 13u , SL_USBD_HID_COUNTRY_CODE_ITALIAN = 14u , SL_USBD_HID_COUNTRY_CODE_JAPAN_KATAKANA = 15u , SL_USBD_HID_COUNTRY_CODE_KOREAN = 16u , SL_USBD_HID_COUNTRY_CODE_LATIN_AMERICAN = 17u , SL_USBD_HID_COUNTRY_CODE_NETHERLANDS_DUTCH = 18u , SL_USBD_HID_COUNTRY_CODE_NORWEGIAN = 19u , SL_USBD_HID_COUNTRY_CODE_PERSIAN_FARSI = 20u , SL_USBD_HID_COUNTRY_CODE_POLAND = 21u , SL_USBD_HID_COUNTRY_CODE_PORTUGUESE = 22u , SL_USBD_HID_COUNTRY_CODE_RUSSIA = 23u , SL_USBD_HID_COUNTRY_CODE_SLOVAKIA = 24u , SL_USBD_HID_COUNTRY_CODE_SPANISH = 25u , SL_USBD_HID_COUNTRY_CODE_SWEDISH = 26u , SL_USBD_HID_COUNTRY_CODE_SWISS_FRENCH = 27u , SL_USBD_HID_COUNTRY_CODE_SWISS_GERMAN = 28u , SL_USBD_HID_COUNTRY_CODE_SWITZERLAND = 29u , SL_USBD_HID_COUNTRY_CODE_TAIWAN = 30u , SL_USBD_HID_COUNTRY_CODE_TURKISH_Q = 31u , SL_USBD_HID_COUNTRY_CODE_UK = 32u , SL_USBD_HID_COUNTRY_CODE_US = 33u , SL_USBD_HID_COUNTRY_CODE_YUGOSLAVIA = 34u , SL_USBD_HID_COUNTRY_CODE_TURKISH_F = 35u } |
Function Documentation
◆ sl_usbd_hid_init()
| sl_status_t sl_usbd_hid_init | ( | void |
|
) |
Initialize HID class.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_hid_create_instance()
| sl_status_t sl_usbd_hid_create_instance | ( | uint8_t |
subclass,
|
| uint8_t |
protocol,
|
||
| sl_usbd_hid_country_code_t |
country_code,
|
||
| uint16_t |
interval_in,
|
||
| uint16_t |
interval_out,
|
||
| bool |
ctrl_rd_en,
|
||
| sl_usbd_hid_callbacks_t * |
p_hid_callbacks,
|
||
| uint8_t * |
p_class_nbr
|
||
| ) |
Add a new instance of the HID class.
- Parameters
-
subclassSubclass code. protocolprotocol code. country_codeCountry code id. interval_inPolling interval for input transfers, in milliseconds. It must be a power of 2. interval_outPolling interval for output transfers, in milliseconds. It must be a power of 2. Used only when read operations are not through control transfers. ctrl_rd_enEnable read operations through the control transfers. p_hid_callbacksPointer to HID descriptor and request callback structure. [Content MUST be persistent] p_class_nbrPointer to variable that will receive class instance number. The variable is set to class instance number if no errors are returned, otherwise it is set to SL_USBD_CLASS_NBR_NONE.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_hid_add_to_configuration()
| sl_status_t sl_usbd_hid_add_to_configuration | ( | uint8_t |
class_nbr,
|
| uint8_t |
config_nbr
|
||
| ) |
Add the HID class instance to the USB device configuration (see Note #1).
- Parameters
-
class_nbrClass instance number. config_nbrConfiguration index to add HID class instance to.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
-
(1) Called several times, it creates multiple instances and configurations. For instance, the following architecture could be created :
* FS * |-- Configuration 0 (HID class 0) * (HID class 1) * (HID class 2) * |-- Interface 0 * |-- Configuration 1 (HID class 0) * |-- Interface 0 *
-
(2) Configuration Descriptor corresponding to a HID device uses the following format :
* Configuration Descriptor * |-- Interface Descriptor (HID class) * |-- Endpoint Descriptor (Interrupt IN) * |-- Endpoint Descriptor (Interrupt OUT) - optional *
◆ sl_usbd_hid_is_enabled()
| sl_status_t sl_usbd_hid_is_enabled | ( | uint8_t |
class_nbr,
|
| bool * |
p_enabled
|
||
| ) |
Get the HID class enable state.
- Parameters
-
class_nbrClass instance number. p_enabledPointer to a variable that will receive HID class enable state. The variable is set to true if HID class is enabled, and is set to false if it is NOT enabled.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_hid_write_sync()
| sl_status_t sl_usbd_hid_write_sync | ( | uint8_t |
class_nbr,
|
| void * |
p_buf,
|
||
| uint32_t |
buf_len,
|
||
| uint16_t |
timeout,
|
||
| uint32_t * |
p_xfer_len
|
||
| ) |
Send data to the host through the Interrupt IN endpoint.
This function is blocking.
- Parameters
-
class_nbrClass instance number. p_bufPointer to the transmit buffer. If more than one input report exists, the first byte must represent the report id. buf_lenTransmit buffer length, in octets. timeoutTimeout in milliseconds. p_xfer_lenPointer to a variable that will receive transfer length. The variable is set to number of octets received, if no errors are returned, or is set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_hid_read_sync()
| sl_status_t sl_usbd_hid_read_sync | ( | uint8_t |
class_nbr,
|
| void * |
p_buf,
|
||
| uint32_t |
buf_len,
|
||
| uint16_t |
timeout,
|
||
| uint32_t * |
p_xfer_len
|
||
| ) |
Receive data from the host through the Interrupt OUT endpoint.
This function is blocking.
- Parameters
-
class_nbrClass instance number. p_bufPointer to the receive buffer. buf_lenReceive the buffer length, in octets. timeoutTimeout, in milliseconds. p_xfer_lenPointer to a variable that will receive transfer length. The variable is set to number of octets received, if no errors are returned, or is set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_hid_read_async()
| sl_status_t sl_usbd_hid_read_async | ( | uint8_t |
class_nbr,
|
| void * |
p_buf,
|
||
| uint32_t |
buf_len,
|
||
| sl_usbd_hid_async_function_t |
async_fnct,
|
||
| void * |
p_async_arg
|
||
| ) |
Receive data from the host through the Interrupt OUT endpoint.
This function is non-blocking and returns immediately after transfer preparation. Upon transfer completion, the provided callback is called to notify the application.
- Parameters
-
class_nbrClass instance number. p_bufPointer to receive buffer. buf_lenReceive buffer length, in octets. async_fnctReceive callback. p_async_argAdditional argument provided by application for receive callback.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_hid_write_async()
| sl_status_t sl_usbd_hid_write_async | ( | uint8_t |
class_nbr,
|
| void * |
p_buf,
|
||
| uint32_t |
buf_len,
|
||
| sl_usbd_hid_async_function_t |
async_fnct,
|
||
| void * |
p_async_arg
|
||
| ) |
Send data to the host through the Interrupt IN endpoint.
This function is non-blocking, and returns immediately after transfer preparation. Upon transfer completion, the provided callback is called to notify the application.
- Parameters
-
class_nbrClass instance number. p_bufPointer to transmit buffer. If more than one input report exists, the first byte must represent the report id. buf_lenTransmit buffer length, in octets. async_fnctTransmit callback. p_async_argAdditional argument provided by application for transmit callback.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
Macro Definition Documentation
◆ SL_USBD_HID_BIAS_NOT_APPLICABLE
| #define SL_USBD_HID_BIAS_NOT_APPLICABLE 0 |
HID PHYSICAL DESCRIPTOR DEFINES
Note(s) : (1) See 'Device Class Definition for Human Interface Devices Version 1.11', Section 6.2.3.
◆ SL_USBD_HID_USAGE_PAGE_UNDEFINED
| #define SL_USBD_HID_USAGE_PAGE_UNDEFINED 0x00 |
HID USAGE PAGES
Note(s) : (1) See 'Universal Serial Bus HID Usage Tables', Version 1.12, Section 3 for more details about Usage Pages.
(2) See 'Universal Serial Bus HID Usage Tables', Version 1.12, Section 4 for more details about Generic Desktop Page usages and controls.
Typedef Documentation
◆ sl_usbd_hid_async_function_t
| typedef void(* sl_usbd_hid_async_function_t) (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint32_t xfer_len, void *p_callback_arg, sl_status_t status) |
Async comm callback.
Enumeration Type Documentation
◆ sl_usbd_hid_country_code_t
HUMAN INTERFACE DEVICE COUNTRY CODES DEFINES
Note(s) : (1) See 'Device Class Definition for Human Interface Devices (HID), 6/27/01, Version 1.11', section 6.2.1 for more details about HID descriptor country code.
(a) The country code identifies which country the hardware is localized for. Most hardware is not localized and thus this value would be zero (0). However, keyboards may use the field to indicate the language of the key caps.