You are viewing documentation for version:
1.0
|
Version History
USB Device MSC API.
|
|
|
sl_status_t
|
sl_usbd_msc_init
(void)
|
|
|
Initialize internal structures and variables used by the Mass Storage Class Bulk Only Transport.
|
|
|
|
sl_status_t
|
sl_usbd_msc_create_instance
(uint8_t subclass, uint32_t msc_task_stack_size, osPriority_t msc_task_priority,
sl_usbd_msc_subclass_driver_t
*p_subclass_drv, void *p_subclass_arg, uint8_t *p_class_nbr)
|
|
|
Add a new instance of the Mass Storage Class.
|
|
|
|
sl_status_t
|
sl_usbd_msc_add_to_configuration
(uint8_t class_nbr, uint8_t config_nbr)
|
|
|
Add an existing MSC instance to the specified configuration.
|
|
|
|
sl_status_t
|
sl_usbd_msc_lun_add
(uint8_t class_nbr, void *p_lu_data, uint8_t *p_lu_nbr)
|
|
|
Add an MSC logical unit to the MSC interface.
|
|
|
|
sl_status_t
|
sl_usbd_msc_is_enabled
(uint8_t class_nbr, bool *p_enabled)
|
|
|
Get the MSC enable state of the device.
|
|
|
|
#define
|
SL_USBD_MSC_LU_NBR_INVALID
255u
|
|
|
|
#define
|
SL_USBD_MSC_SUBCLASS_CODE_RBC
0x01
|
|
|
|
#define
|
SL_USBD_MSC_SUBCLASS_CODE_SFF_8020i
0x02
|
|
|
|
#define
|
SL_USBD_MSC_SUBCLASS_CODE_MMC_2
0x02
|
|
|
|
#define
|
SL_USBD_MSC_SUBCLASS_CODE_QIC_157
0x03
|
|
|
|
#define
|
SL_USBD_MSC_SUBCLASS_CODE_UFI
0x04
|
|
|
|
#define
|
SL_USBD_MSC_SUBCLASS_CODE_SFF_8070i
0x05
|
|
|
|
#define
|
SL_USBD_MSC_SUBCLASS_CODE_SCSI
0x06
|
|
|
|
#define
|
SL_USBD_MSC_PROTOCOL_CODE_CTRL_BULK_INTR_CMD_INTR
0x00
|
|
|
|
#define
|
SL_USBD_MSC_PROTOCOL_CODE_CTRL_BULK_INTR
0x01
|
|
|
|
#define
|
SL_USBD_MSC_PROTOCOL_CODE_BULK_ONLY
0x50
|
◆
sl_usbd_msc_init()
|
sl_status_t sl_usbd_msc_init
|
(
|
void
|
|
)
|
|
Initialize internal structures and variables used by the Mass Storage Class Bulk Only Transport.
-
Returns
-
Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆
sl_usbd_msc_create_instance()
|
sl_status_t sl_usbd_msc_create_instance
|
(
|
uint8_t
|
subclass,
|
|
|
|
uint32_t
|
msc_task_stack_size,
|
|
|
|
osPriority_t
|
msc_task_priority,
|
|
|
|
sl_usbd_msc_subclass_driver_t
*
|
p_subclass_drv,
|
|
|
|
void *
|
p_subclass_arg,
|
|
|
|
uint8_t *
|
p_class_nbr
|
|
|
)
|
|
|
Add a new instance of the Mass Storage Class.
-
Parameters
-
subclass
|
MSC subclass code.
|
p_subclass_drv
|
Pointer to data structure of functions that implement the subclass driver.
|
msc_task_stack_size
|
The USB stack creates a task to handle the events of each MSC instance. This parameter specifies the stack size to be used for the newly created task for this instance.
|
msc_task_priority
|
The USB stack creates a task to handle the events of each MSC instance. This parameter specifies the CMSIS priority of that task.
|
p_subclass_arg
|
An argument that will be passed to the driver when driver functions are called.
|
p_class_nbr
|
Pointer to a variable that will receive the instance number for the created class instance, if no errors are returned. Otherwise, the variable is set to SL_USBD_CLASS_NBR_NONE.
|
-
Returns
-
Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆
sl_usbd_msc_add_to_configuration()
|
sl_status_t sl_usbd_msc_add_to_configuration
|
(
|
uint8_t
|
class_nbr,
|
|
|
|
uint8_t
|
config_nbr
|
|
|
)
|
|
|
Add an existing MSC instance to the specified configuration.
-
Parameters
-
class_nbr
|
MSC instance number.
|
config_nbr
|
Configuration index to which to add the existing MSC interface.
|
-
Returns
-
Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
-
Note
-
(1)
sl_usbd_msc_add_to_configuration()
adds an Interface descriptor and its associated Endpoint descriptor(s) to the Configuration descriptor. One call to
sl_usbd_msc_add_to_configuration()
builds the Configuration descriptor corresponding to an MSC device with the following format:
* Configuration Descriptor
* |-- Interface Descriptor (MSC)
* |-- Endpoint Descriptor (Bulk OUT)
* |-- Endpoint Descriptor (Bulk IN)
*
If
sl_usbd_msc_add_to_configuration()
is called several times from the application, it creates multiple instances and configurations. For example, the following architecture could be created for a high-speed device:
* High-speed
* |-- Configuration 0
* |-- Interface 0 (MSC 0)
* |-- Configuration 1
* |-- Interface 0 (MSC 0)
* |-- Interface 1 (MSC 1)
*
In this example, there are two instances of MSC: 'MSC 0' and 'MSC 1', and two possible configurations for the device: 'Configuration 0' and 'Configuration 1'. 'Configuration 1' is composed of two interfaces.
Each class instance has an association with one of the interfaces. If 'Configuration 1' is activated by the host, it allows the host to access two different functionalities offered by the device.
◆
sl_usbd_msc_lun_add()
|
sl_status_t sl_usbd_msc_lun_add
|
(
|
uint8_t
|
class_nbr,
|
|
|
|
void *
|
p_lu_data,
|
|
|
|
uint8_t *
|
p_lu_nbr
|
|
|
)
|
|
|
Add an MSC logical unit to the MSC interface.
-
Parameters
-
class_nbr
|
MSC instance number.
|
p_lu_data
|
Pointer to the logical unit data to store in LU data structure.
|
p_lu_nbr
|
Pointer to a variable that will receive Logical Unit Number.
|
-
Returns
-
Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆
sl_usbd_msc_is_enabled()
|
sl_status_t sl_usbd_msc_is_enabled
|
(
|
uint8_t
|
class_nbr,
|
|
|
|
bool *
|
p_enabled
|
|
|
)
|
|
|
Get the MSC enable state of the device.
-
Parameters
-
class_nbr
|
MSC instance number.
|
p_enabled
|
Pointer to a boolean variable that will receive enable state. The variable is set to true if MSC class is enabled. The variable is set to false if the MSC class is not enabled.
|
-
Returns
-
Returns SL_STATUS_OK on success or another SL_STATUS code on failure.