Network Stack#
The SiWN917 Network Stack modes are as shown below.
Offloaded Mode
Hosted Mode
By default, the TCP/IP Stack runs on the TA (Network Processor) which is the Offloaded mode. If you want to bypass it and use the TCP/IP stack residing on the host processor, which is the Hosted mode, you can refer to the LWIP TCP client example in the release.
Offloaded Mode#


Hosted Mode#