Applications - Memory Occupancy#
Below is the memory occupancy of the default examples with 3.3.1 release (M4 - Application processor). The following memory occupancy may vary from release to release for a common flash device (8 MB).
Example Name | Features | Flash | RAM |
|---|---|---|---|
wifi_station_ble_provisioning_aws | Wi-Fi, Cloud, SSL, Certificates | 66 KB | 129 KB |
wifi_http_otaf | Wi-Fi, HTTP, TCP/IP | 40 KB | 96 KB |
wifi_powersave_standby_associated_soc | Wi-Fi, Power-save | 44 KB | 102 KB |
wifi_station_ble_throughput_app | Wi-Fi, BLE, TCP/IP | 49 KB | 100 KB |
Note: The leftover RAM will be allotted to ‘.heap’ variable.