Software Overview#
This section covers the software drivers required for the programmer.
The generic flash programmer executes the flashing operation via the Network Wireless Processor (NWP) boot loader.
| Description | Common Flash |
|---|---|
| Flash Memory | A single flash memory is shared between M4 (Host MCU) and NWP, and they access this flash memory over dedicated QSPI controllers. |
| Memory Access | An arbiter placed between the QSPIs and memory helps in arbitration for flash access. |
| Erase Operation | Uses the bootloader-based erase chip operation |
The flash memory is shared between the M4 and NWP. Only the NWP can perform low-level operations on the flash memory, and the M4 can only support flash read operations. For low-level operations such as erase and write operations, the M4 can request the NWP bootloader to do the operations.
The steps required for flash programming are as follows.
| Programming Stage | Description | APIs |
|---|---|---|
| Initialization | Device description needs to be provided in this stage. | In FlashDev.c file, we provided the device details in the "struct FlashDevice_t" |
| Program | Program the flash. | In FlashPrg.c file, we used the following two SiWx917 APIs in the ProgramPage() API.
|
| Erase | Erases the entire flash. | In FlashPrg.c, we used the following SiWx917 API in the EraseChip() API
|
Note: The SiWx917 APIs are explained in detail in Section SiWx917 Generic Flash APIs.