Analog Peripherals Debugging and Error Handling (SiWx91x Devices)#
This section provides best practices for debugging and error handling when working with analog peripherals on SiWx917 devices. It covers common issues, diagnostic techniques, error recovery patterns, and callback-based fault detection for analog-to-digital converter (ADC) and digital-to-analog converter (DAC) peripherals.
Common Debugging Tips#
Using a Logic Analyzer#
A logic analyzer is an essential tool for verifying timing and signal integrity in ADC and DAC operations. Use it to inspect:
Clock signals. Verify that sampling clocks operate at the expected frequencies.
Control signals. Check enable, trigger, and DMA control signals.
Interrupt timing. Measure callback response times for data-ready events.
FIFO activity. Monitor FIFO fill levels and detect underflow or overflow conditions.
ADC Debugging Strategies#
Signal Integrity#
Ensure that the analog input signal remains within the 0 V to VREF range.
Verify reference voltage stability and analog ground connections.
Confirm that analog input pins are not shared with digital I/O functions.
Configuration Validation#
Verify that ADC channel mappings match physical pin assignments.
Check sampling rates and FIFO thresholds for the intended use case.
Confirm that the input mode (single-ended or differential) matches the hardware design.
Data Analysis#
Compare digital output values with expected analog input levels.
Verify conversion timing consistency across repeated samples.
Use known reference voltages to validate accuracy.
DAC Debugging Strategies#
Output Verification#
Measure DAC output using an oscilloscope to confirm expected voltage levels.
Verify load impedance and avoid heavy loads below 1 kΩ.
Confirm that sample rate and update frequency match the configuration.
Data Path Validation#
Confirm input data format (12-bit unsigned).
Verify correct scaling to match expected voltage output range.
Ensure FIFO ordering matches the intended waveform sequence.
Error Code Handling#
Analog peripheral APIs return status codes of type sl_status_t to indicate success or failure. Consistent handling of these codes ensures reliability and smooth recovery from runtime faults.
Error Code Reference Table#
Analog peripheral driver APIs return standardized status codes (sl_status_t) that help identify issues and guide recovery actions.
Always check for SL_STATUS_OK after each API call to ensure successful operation.
Error Code | Description | Recommended Recovery Action |
|---|---|---|
| Operation completed successfully. | Continue normal operation. |
| Invalid configuration or argument. | Verify and correct parameters (such as channel, VREF, and sample rate). |
| Peripheral not initialized. | Call initialization function before performing operations. |
| Value out of acceptable range. | Check input values against valid ranges (such as voltage or channel). |
| Invalid count or size parameter. | Verify buffer sizes and sample counts. |
| General failure detected. | Reset and reinitialize the peripheral. |
Interrupt Error Handling#
The SiWx917 ADC peripherals generate interrupts to signal events that require software handling.
Event Type | Description | Recommended Action |
|---|---|---|
| Internal DMA transfer event triggered. | Handle DMA completion, verify data integrity, and prepare the next transfer. |
| ADC static mode conversion completed. | Read conversion result and clear the event flag. |
Common Error Codes and Recovery Strategies#
ADC Error Codes#
SL_STATUS_INVALID_PARAMETER
Occurs when invalid arguments are passed to initialization or configuration API functions.
if (status == SL_STATUS_INVALID_PARAMETER) { printf("ADC initialization failed: Invalid parameters\n"); // Validate channel index, VREF, and sampling rate }
SL_STATUS_NOT_READY
Indicates that ADC is not fully initialized or configured.
if (status == SL_STATUS_NOT_READY) { printf("ADC not ready – reinitializing...\n"); sl_si91x_adc_init(adc_channel_config, adc_config, vref_value); }
SL_STATUS_BUSY
The ADC is performing another conversion or DMA transaction.
if (status == SL_STATUS_BUSY) { printf("ADC busy – waiting for completion\n"); sl_sleeptimer_delay_millisecond(10); }
DAC Error Codes#
SL_STATUS_INVALID_CONFIGURATION
Occurs when configuration parameters are invalid.
if (status == SL_STATUS_INVALID_CONFIGURATION) { printf("Invalid DAC configuration\n"); // Check sample rate, FIFO settings, and pin mapping }
SL_STATUS_FAIL
Indicates that the DAC encountered an error during a write or update operation.
if (status == SL_STATUS_FAIL) { printf("DAC write failed\n"); // Re-verify initialization and data format }
Error Recovery Patterns#
Implementing retry-based recovery improves robustness in the presence of transient failures.
sl_status_t adc_operation_with_recovery(void) { sl_status_t status; int retries = 0; const int max_retries = 3; do { status = sl_si91x_adc_start(adc_config); if (status == SL_STATUS_OK) break; switch (status) { case SL_STATUS_NOT_READY: sl_si91x_adc_deinit(adc_config); sl_si91x_adc_init(adc_channel_config, adc_config, vref_value); break; case SL_STATUS_BUSY: sl_sleeptimer_delay_millisecond(10); break; default: printf("Unexpected ADC error: 0x%lx\n", status); break; } retries++; } while (retries < max_retries); return status; }
Callback-Based Error Detection#
Callbacks provide an efficient mechanism for asynchronous event monitoring and error reporting.
ADC Callback Example#
static void adc_callback_handler(uint8_t channel_no, uint8_t event) { switch (event) { case SL_ADC_DATA_READY: sl_si91x_adc_read_data(adc_config, &channel_id, &adc_data); break; case SL_ADC_STATIC_MODE_CALLBACK: printf("ADC static mode conversion complete\n"); break; default: printf("Unexpected ADC event: %d\n", event); break; } }
DAC Callback Example#
static void dac_callback_handler(uint8_t event) { switch (event) { case SL_DAC_FIFO_EMPTY: printf("DAC FIFO empty – refilling buffer\n"); sl_si91x_dac_write_data(next_samples, sample_count); break; default: printf("Unexpected DAC event: %d\n", event); break; } }
Troubleshooting Common Issues#
ADC Troubleshooting#
Problem | Cause | Solution |
|---|---|---|
Inconsistent readings | Unstable VREF or poor grounding | Stabilize reference and ground; add bypass capacitors. |
Conversion timeout | Power state or clock misconfiguration | Ensure the ADC clock and power state support active operation. |
Incorrect readings | Input voltage out of range | Verify scaling and VREF calibration. |
DAC Troubleshooting#
Problem | Cause | Solution |
|---|---|---|
Incorrect output voltage | VREF or scaling mismatch | Reconfigure reference voltage and verify data format. |
FIFO underrun | Insufficient buffer refill | Use callbacks to maintain FIFO fill levels. |
Distorted output | Incorrect sample rate or load | Adjust sample frequency and verify proper output impedance. |