Timer Developer Guide Appendix#
This appendix provides reference material, examples, and supporting information for working with timers, clocks, and power management in embedded systems. It includes glossary terms, acronyms, extended examples, reference tables, troubleshooting guidance, best practices, and related resources.
Glossary#
The glossary defines key terms related to timers, power management, and clock systems. Use this section to clarify technical concepts when configuring or debugging hardware timers.
Timer-Specific Terms#
Counter: A digital circuit that increments or decrements on each clock pulse. Counters measure time intervals or count events.
Prescaler: A clock divider that reduces the input clock frequency to a lower frequency for the timer counter. Prescalers extend timing periods.
Compare Match: An event that occurs when a timer counter value equals a predefined compare value. Compare match events often trigger interrupts or toggle outputs.
Capture: The process of storing the current timer counter value when an external event occurs. Capture enables precise timing measurements.
Pulse Width Modulation (PWM): A technique for generating variable-width pulses to control power delivered to electrical devices.
Duty Cycle: The percentage of time a PWM signal remains in the "on" state relative to the total period.
Jitter: Variations in timing between consecutive events. Jitter often results from clock instability or system interrupts.
Latency: The delay between when an event occurs and when the system responds.
Resolution: The smallest time increment that a timer can measure or generate.
Overflow: A condition where a timer counter reaches its maximum value and wraps back to zero.
Power Management Terms#
Power management terms describe operating states and subsystems that affect energy consumption.
Power State (PS): Different operating modes of the system, each with specific power consumption and functionality levels.
PS4 (High Power): Full operational mode with all peripherals active. This mode consumes the most power.
PS2 (Ultra-Low-Power Mode, ULP Mode): A mode with limited functionality but significantly reduced power consumption.
PS1 (Sleep Mode): A deep sleep mode where most systems suspend, but some wake sources remain active.
PS0 (Deep Sleep): The lowest power mode, with minimal power consumption and most systems suspended.
Wake Source: An event or condition that causes the system to transition from a low-power state to a higher-power state.
Ultra-Low-Power Subsystem (ULPSS): A specialized subsystem that stays active in low-power modes to perform essential functions.
Clock and Timing Terms#
These terms define sources and circuits that provide timing signals.
Clock Source: The origin of timing signals for a timer. Clock sources can include internal oscillators, external crystals, or derived clocks.
Interface Phase-Locked Loop (PLL): A circuit that generates high-frequency clock signals from lower-frequency inputs.
Resistor-Capacitor (RC) Oscillator: An oscillator based on resistors and capacitors. RC oscillators provide a clock reference but are less accurate than crystal oscillators.
Crystal Oscillator (XTAL): A high-precision oscillator that provides a stable and accurate clock reference.
Clock Divider: A circuit that divides the input clock frequency by a programmable factor.
Acronyms#
This table lists acronyms used throughout the guide and their definitions.
Acronym | Full Name | Description |
|---|---|---|
CT | Configurable Timer | High-performance timer with advanced PWM and capture features |
SYSRTC | System Real-Time Clock | Low-power timer for timekeeping across all power states |
ULP | Ultra-Low Power | A power-efficient mode and timer type |
WDT | Watchdog Timer | Reliability timer for fault detection and recovery |
PWM | Pulse Width Modulation | Technique for generating variable-width electrical pulses |
ICU | Input Capture Unit | Hardware unit for capturing external event timing |
OCU | Output Compare Unit | Hardware unit for generating precise output timing |
WFG | Waveform Generator | Hardware that generates complex waveform patterns |
DMA | Direct Memory Access | High-speed data transfer without CPU involvement |
GPIO | General Purpose Input/Output | Configurable digital pins for external connections |
RTOS | Real-Time Operating System | Operating system designed for real-time applications |
IoT | Internet of Things | Network of interconnected devices and sensors |
PLL | Phase-Locked Loop | Circuit that generates stable clock frequencies |
RC | Resistor-Capacitor | Type of oscillator circuit |
XTAL | Crystal | High-precision timing reference |
SOC | System on Chip | Integrated circuit with multiple system components |
Extended Examples#
This section demonstrates how to configure timers for real-world use cases. Each example includes requirements and implementation details.
Example 1: Motor Control System with Configurable Timer#
Scenario: A three-phase motor control system requires synchronized PWM signals with precise timing.
Requirements:
Generate three PWM outputs with 120° phase separation
Support a frequency range of 1 Hz to 1 kHz
Provide duty cycle control from 0% to 100%
Enable synchronized start and stop
Implementation:
// CT configuration for three-phase motor control void configure_motor_control_timer(void) { // Configure Counter0 for base timing CT_Config_t ctConfig = { .counter = CT_COUNTER_0, .mode = CT_MODE_UP, .clockSource = CT_CLOCK_SOURCE_INTERFACE_PLL, .prescaler = 160, // 160 MHz / 160 = 1 MHz .period = 999 // 1 MHz / 1000 = 1 kHz base frequency }; CT_Init(&ctConfig); // Configure three PWM channels with 120° phase separation // Channel 0: 0° phase CT_OCU_Config_t ocu0 = { .channel = 0, .mode = CT_OCU_MODE_PWM, .compareValue = 499, // 50% duty cycle .polarity = CT_OCU_POLARITY_HIGH }; CT_OCU_Init(&ocu0); // Channel 1: 120° phase (333 counts delay) CT_OCU_Config_t ocu1 = { .channel = 1, .mode = CT_OCU_MODE_PWM, .compareValue = 499, .polarity = CT_OCU_POLARITY_HIGH }; CT_OCU_Init(&ocu1); CT_SetCompareValue(CT_COUNTER_0, 1, 333); // Phase delay // Channel 2: 240° phase (666 counts delay) CT_OCU_Config_t ocu2 = { .channel = 2, .mode = CT_OCU_MODE_PWM, .compareValue = 499, .polarity = CT_OCU_POLARITY_HIGH }; CT_OCU_Init(&ocu2); CT_SetCompareValue(CT_COUNTER_0, 2, 666); // Phase delay // Start the timer CT_Start(CT_COUNTER_0); }
Example 2: Low-Power Internet of Things (IoT) Device with System Real-Time Clock (SYSRTC)#
Scenario: A battery-powered IoT sensor needs to wake periodically to collect and transmit data.
Requirements:
Wake every 5 minutes to collect sensor data
Wake every hour to transmit data
Maintain accurate time across all power states
Minimize power consumption
Implementation:
// SYSRTC configuration for IoT device timing void configure_iot_timing(void) { // Initialize SYSRTC with 32 kHz clock SYSRTC_Config_t config = { .clockSource = SYSRTC_CLOCK_SOURCE_32KHZ_RC, .prescaler = 1 // No additional division }; SYSRTC_Init(&config); // Configure Group 0 for sensor sampling (5-minute intervals) SYSRTC_GroupConfig_t group0 = { .group = 0, .compare0Value = 5 * 60 * 32768, // 5 minutes in 32 kHz ticks .compare0Mode = SYSRTC_COMPARE_MODE_PERIODIC, .compare0Interrupt = true }; SYSRTC_ConfigureGroup(&group0); // Configure Group 1 for data transmission (hourly) SYSRTC_GroupConfig_t group1 = { .group = 1, .compare0Value = 60 * 60 * 32768, // 1 hour in 32 kHz ticks .compare0Mode = SYSRTC_COMPARE_MODE_PERIODIC, .compare0Interrupt = true }; SYSRTC_ConfigureGroup(&group1); // Enable interrupts SYSRTC_EnableInterrupt(0, SYSRTC_INT_COMPARE0); SYSRTC_EnableInterrupt(1, SYSRTC_INT_COMPARE0); // Start SYSRTC SYSRTC_Start(); } // Interrupt handlers void SYSRTC_Group0_Compare0_IRQHandler(void) { // Collect sensor data collect_sensor_data(); // Clear interrupt flag SYSRTC_ClearInterrupt(0, SYSRTC_INT_COMPARE0); } void SYSRTC_Group1_Compare0_IRQHandler(void) { // Transmit collected data transmit_data(); // Clear interrupt flag SYSRTC_ClearInterrupt(1, SYSRTC_INT_COMPARE0); }
Example 3: Ultra-Low-Power (ULP) Timer for Sleep Mode Wake Scheduling#
Scenario: A wearable device must schedule precise wake events while maintaining accurate timing in sleep modes.
Requirements:
Wake every 100 ms for sensor sampling during light sleep
Wake every 1 second for system maintenance
Maintain microsecond accuracy
Operate in Ultra-Low-Power (PS2) mode
Implementation:
// ULP Timer configuration for sleep mode timing void configure_ulp_wake_timing(void) { // Configure ULP Timer 0 for 100 ms sensor sampling ULP_TIMER_Config_t timer0_config = { .instance = ULP_TIMER_0, .clockSource = ULP_TIMER_CLOCK_SOURCE_32KHZ_RC, .resolution = ULP_TIMER_RESOLUTION_1US, .mode = ULP_TIMER_MODE_PERIODIC, .period = 100000 // 100 ms in microseconds }; ULP_TIMER_Init(&timer0_config); // Configure ULP Timer 1 for 1 second system maintenance ULP_TIMER_Config_t timer1_config = { .instance = ULP_TIMER_1, .clockSource = ULP_TIMER_CLOCK_SOURCE_32KHZ_RC, .resolution = ULP_TIMER_RESOLUTION_1US, .mode = ULP_TIMER_MODE_PERIODIC, .period = 1000000 // 1 second in microseconds }; ULP_TIMER_Init(&timer1_config); // Enable interrupts ULP_TIMER_EnableInterrupt(ULP_TIMER_0, ULP_TIMER_INT_PERIODIC); ULP_TIMER_EnableInterrupt(ULP_TIMER_1, ULP_TIMER_INT_PERIODIC); // Start timers ULP_TIMER_Start(ULP_TIMER_0); ULP_TIMER_Start(ULP_TIMER_1); } // Interrupt handlers void ULP_TIMER_0_IRQHandler(void) { // Sample sensors sample_sensors(); // Clear interrupt ULP_TIMER_ClearInterrupt(ULP_TIMER_0, ULP_TIMER_INT_PERIODIC); } void ULP_TIMER_1_IRQHandler(void) { // Perform system maintenance system_maintenance(); // Clear interrupt ULP_TIMER_ClearInterrupt(ULP_TIMER_1, ULP_TIMER_INT_PERIODIC); }
Reference Tables#
Reference tables provide quick comparisons and specifications for timers, power consumption, and clock sources.
Timer Feature Comparison#
Feature | CT | SYSRTC | ULP Timer | WDT |
|---|---|---|---|---|
Counter Width | 16-bit × 2 | 32-bit shared | 32-bit × 4 | Hardware |
Clock Range | 40-160 MHz | 32 kHz | 32 kHz–32 MHz | Internal |
PWM Channels | 8 | 4 | 0 | 0 |
Capture Channels | 8 | 2 | 0 | 0 |
DMA Support | Yes | No | No | No |
Power States | PS4 only | All | PS4, PS2, PS1* | All |
Typical Use | High-performance | Timekeeping | Sleep timing | Reliability |
*PS1: Wake source only
Power Consumption Estimates#
Timer Type | PS4 (mA) | PS2 (µA) | PS1 (µA) | PS0 (µA) |
|---|---|---|---|---|
CT | 2–5 | N/A | N/A | N/A |
SYSRTC | 0.1–0.5 | 0.05–0.2 | 0.02–0.1 | 0.01–0.05 |
ULP Timer | 0.05–0.2 | 0.02–0.1 | 0.01–0.05 | N/A |
WDT | 0.01–0.05 | 0.01–0.05 | 0.01–0.05 | 0.01–0.05 |
Note: Actual values vary based on configuration and system conditions.
Clock Source Characteristics#
Source | Frequency | Accuracy | Power | Stability |
|---|---|---|---|---|
Interface PLL | 40–160 MHz | ±0.1% | High | Excellent |
32 kHz RC | 32 kHz | ±2% | Low | Good |
32 kHz XTAL | 32 kHz | ±0.01% | Low | Excellent |
REF 32 MHz | 32 MHz | ±0.5% | Medium | Good |
SOC Clock | Variable | ±0.1% | Medium | Excellent |
Troubleshooting Guide#
The troubleshooting guide helps diagnose common issues with timers and provides practical solutions.
Common Issues and Solutions#
Timer Not Starting#
Symptoms: Timer counter remains at 0 and does not generate interrupts.
Possible Causes:
Clock source not enabled
Incorrect prescaler configuration
Timer not enabled after configuration
Solutions:
Verify the clock source is active
Check prescaler calculations
Ensure the timer is started after configuration
Incorrect Timing#
Symptoms: Timer periods appear longer or shorter than expected.
Possible Causes:
Wrong clock source selection
Incorrect prescaler value
Clock frequency mismatch
Solutions:
Verify clock source frequency
Recalculate prescaler values
Check clock configuration
Interrupts Not Firing#
Symptoms: Timer runs but does not generate interrupts.
Possible Causes:
Interrupt not enabled
Interrupt priority set too low
Nested Vectored Interrupt Controller (NVIC) not configured
Solutions:
Enable timer interrupts
Set appropriate interrupt priority
Configure NVIC for timer interrupts
Power State Issues#
Symptoms: Timer stops in low-power modes.
Possible Causes:
Timer incompatible with selected power state
Clock source suspended
Interrupt routing disabled
Solutions:
Check power state compatibility
Use a timer supported in the required mode
Verify clock and interrupt configuration
Debugging Techniques#
Clock Verification: Use an oscilloscope or logic analyzer to check clock signals.
Register Inspection: Monitor timer registers during operation.
Interrupt Monitoring: Verify interrupt generation and handling.
Power State Testing: Test across all supported power states.
Timing Validation: Use an external timing reference to confirm accuracy.
Best Practices#
Follow these best practices for efficient and reliable timer use.
Timer Selection#
Use the Configurable Timer (CT) for high-performance applications requiring precise timing.
Use the System Real-Time Clock (SYSRTC) for continuous timekeeping across power states.
Select the Ultra-Low-Power Timer for sleep mode timing.
Use the Watchdog Timer (WDT) to improve system reliability.
Configuration#
Verify clock source availability before configuring timers.
Select appropriate prescaler values for required resolution.
Enable interrupts only when necessary to minimize power consumption.
Use Direct Memory Access (DMA) with CT for high-frequency operations.
Power Management#
Group timer operations to reduce power state transitions.
Use the lowest-power timer that meets requirements.
Disable unused timer features to reduce power consumption.
Schedule wake events efficiently to minimize active time.
Performance Optimization#
Use DMA for high-frequency data operations.
Minimize time spent in interrupt service routines.
Group related timer operations for efficiency.
Prefer hardware features over software-based implementations.
Related Resources
Refer to these resources for additional guidance:
Timer API Reference: Function documentation
Power Manager Guide: Power state management and transitions
Clock Configuration Guide: System clock setup and management
Interrupt Guide: Interrupt handling and configuration
GPIO Guide: Pin configuration and routing
DMA Guide: High-performance data transfer
Application Notes: Real-world implementation examples
Development Tools: Debugging and validation utilities