BLE Country Region#
Currently, users are restricted to configuring the same region for both BLE and Wi-Fi. This new enhancement provides the flexibility to set the BLE region independently before connecting to an Access Point (AP). Once the connection to the AP is successfully established, the BLE region will automatically adjust to match the region supported by the connected AP
Note: This configuration is supported exclusively on the SiW917Y module.
Follow these steps to update the BLE country region:
Compile and insert the driver as outlined in the Compilation Steps and Installing the Driver sections.
Navigate to the release folder.
Run the following command to request the
BLE_COUNTRY_REGION_UPDATEcommand:
Set BLE Country Region Command#
./bt_util ble_country_region <country_region>Supported Country Region Codes:
Region  | Value  | 
|---|---|
FCC  | 0  | 
ETSI  | 1  | 
TELEC  | 2  | 
WORLDWIDE  | 3  | 
KCC  | 4  | 
WORLDSAFE  | 5 (Applicable only for the SiW917Y module)  | 
Example:
#./bt_util ble_country_region 2Users can expect the similar console output
Set country region 
***** Received Country region From LMAC is = 2 *****Get BLE Country Region Command#
./bt_util ble_country_region get_ble_countryUsers can expect the similar console output
Read country region 
***** Received Country region From LMAC is = 2 *****