Developing with SiWT917 in RCP Mode#
The SiWT917, in Radio Co-processor (RCP) mode, offers low-level Wi-Fi and Bluetooth Low Energy for systems that have a higher-end 32/64-bit applications processor running a Linux-based operating system. The SiWT917 interfaces to a processor using SDIO host interfaces, with the networking and wireless stacks/profiles running on the host processor. SiWT917 provides multiple operating modes including Wi-Fi Client, Wi-Fi Access Point, Wi-Fi Client + Access Point, Wi-Fi + Bluetooth Low Energy (BLE), and BLE-only mode.
To get started, download the latest SiWT917 Open Source Driver and see the Getting Started Guide.