Wi-Fi performance profile.

Public Attributes#

Performance profile.

uint8_t

Set DTIM alignment required. si91x_dtim_alignment_types.

uint8_t

Default value to be used is 0.

uint16_t

Listen interval.

sl_wifi_twt_request_t

twt request.

Public Attribute Documentation#

profile#

sl_performance_profile_t sl_wifi_performance_profile_t::profile

Performance profile.


Definition at line 934 of file components/si91x/inc/sl_wifi_device.h

dtim_aligned_type#

uint8_t sl_wifi_performance_profile_t::dtim_aligned_type

Set DTIM alignment required. si91x_dtim_alignment_types.


Definition at line 935 of file components/si91x/inc/sl_wifi_device.h

num_of_dtim_skip#

uint8_t sl_wifi_performance_profile_t::num_of_dtim_skip

Default value to be used is 0.


Definition at line 936 of file components/si91x/inc/sl_wifi_device.h

listen_interval#

uint16_t sl_wifi_performance_profile_t::listen_interval

Listen interval.


Definition at line 937 of file components/si91x/inc/sl_wifi_device.h

twt_request#

sl_wifi_twt_request_t sl_wifi_performance_profile_t::twt_request

twt request.


Definition at line 938 of file components/si91x/inc/sl_wifi_device.h