You are viewing documentation for version:3.0.10Update Enums#In your existing application, replace each WiSeConnectâ„¢ SDK v2.x enum value with the equivalent v3.x enum value. Refer to the table below for the mapping of v2.x to v3.x enums.v2.x events are listed in alphabetical order of enum name.v2.x Enumv3.x EnumRSI_WLAN_ACCESS_POINT_MODESL_SI91X_ACCESS_POINT_MODERSI_WLAN_CLIENT_MODESL_SI91X_CLIENT_MODERSI_WLAN_CONCURRENT_MODESL_SI91X_CONCURRENT_MODERSI_WLAN_ENTERPRISE_CLIENT_MODESL_SI91X_ENTERPRISE_CLIENT_MODERSI_WLAN_TRANSMIT_TEST_MODESL_SI91X_TRANSMIT_TEST_MODE